Editors' Notes—Volume 40, Number 4, 2006 At the close of two-score years in print, we look
back…heck, we can all look
back at
every issue* that ever rolled off the presses, just as they
appeared at the time—including Volume 1, Number 1 (1967)—thanks to
scanning and the miracle of PDF. Moreover, a more portable physical
embodiment of the totality of
Analog Dialogue’s 40-year substance through 2006, a CD version, will soon be available,
replacing the four bulging binders that are currently needed to
contain the paper-and-ink version. When it arrives, we will recommend the CD to our
fans, to history lovers and reference librarians and their clientele
everywhere, as a private refuge from the crowded, noisy,
crime-ridden, sometimes dangerous highways and byways of the
Internet.
Dan
Sheingold [dan.sheingold@analog.com]
NEW WEB
FEATURES FOR 2007 As our screens got bigger and
our eyes get weaker, we chose to stop catering to the small-screen
crowd at the expense of the overwhelming percentage of readers who
are using screen resolutions of 1024 × 768 or higher. Please let us
know if you like the new on-line format†—or
think we should revert to the original. We also added a new feature,
the Back Burner, which is sure to become one of your favorite
spots. It will include teasers, design and test tips, tutorials, and
other information of interest to designers. Please let us know of
any topics that you would like to have covered in future issues.
IN THIS
ISSUE Mechanical buttons, switches, and jog wheels have
long been used as interfaces between users and machines, but their
many drawbacks have led designers to look for more reliable
solutions. Capacitive sensors, which can be used in place of
buttons, can also add versatility. Available ICs can measure the
capacitance of up to 14 sensors, compensate for environmental
changes, and provide a digital output. The picture quality available from cell phone
cameras is constantly improving. Autofocus is standard in many
high-resolution cameras, and optical zoom, shutter control, and
image stabilization are becoming common. These features require the
lens to move rapidly. Lens drivers power the motors that move the
lens in response to digital signals. New isolation capabilities—including integrated,
isolated power and truly bidirectional isolation channels—are
greatly simplifying the design of isolated systems. Fueled by a
shift from LED-based optocouplers to chip-scale microtransformer
technology that is compatible with standard CMOS processes, they fit
more functionality into a single package. As always, your comments are welcome.
Scott
Wayne [scott.wayne@analog.com]
*See
http://www.analog.com/library/analogDialogue/archives.html
†Take
a look at
http://www.analog.com/analogdialogue Copyright 1995- Analog Devices, Inc. All rights reserved. |