Tutorial: Improve Sensor Performance and SNR in Pulse Oximeter Designs

Jun 21 2010

Figure 1

   

Abstract

This tutorial discusses the different types of pulse oximeters including optical and reflective techniques and the design considerations taken when building high-end portable bedside monitors or mid and low-end battery-powered models. The discussion covers light absorption, sensor calibration, and details specifics within the transmit path leading to in-depth discovery of photodiode, interface, signal conversion, and data conversion characteristics. A functional block diagram and part recommendations are also included.

Overview

Pulse oximeters noninvasively measure or continuously monitor oxygen saturation in arterial blood to ensure that there is sufficient oxygenation. Typical applications include people with respiratory problems who are under anesthesia, neonates, and critically ill patients.

In a pulse oximetry system, a clip with optical electronics is usually attached to a finger, toe, or ear so that light can be transmitted through the skin from one side of the clip and received on the other side with a photodiode. Good arterial blood flow is required to measure oxygen saturation. Most applications use transmissive optical techniques, but there are some applications that use reflective techniques.

Oximeter Types

Available in different shapes and sizes, pulse oximeters fall within three main categories.

At the high end are portable bedside patient monitors, which have a removable cable that includes a clip containing the optics used to measure oxygen saturation. These models are either dedicated to pulse oximetry or they monitor multiple vital parameters such as pulse, blood pressure, respiratory rate, and temperature. These high-end models demand high performance, with a low-noise signal path being the most important design parameter. Power is a secondary consideration, since the monitor is line powered most of the time and only runs off of battery power when the patient is mobile. Size is not a driving factor in these designs.

Mid-range handheld pulse oximeter.

Mid-range handheld pulse oximeter.

Mid-range models are typically battery-powered handheld units with a removable cable. Performance is still important, but it needs to be balanced with size and power constraints. While handheld units run off of batteries all of the time, they have the space to include decently sized batteries.

Low-end fingertip pulse oximeter.

Low-end fingertip pulse oximeter.

At the low end are fingertip models, which combine the base unit and cable into a clip that is large enough to cover a finger and house the electronics and batteries. The small size means that performance may need to be sacrificed to preserve the small form factor and achieve the desired battery life.

Functional block diagram of a pulse oximeter.

Functional block diagram of a pulse oximeter.

Principle of Operation

Operation is based on the light-absorption characteristics of hemoglobin in the blood. Oxygenated hemoglobin absorbs more infrared light than red light, and deoxygenated hemoglobin absorbs more red light than infrared light. Thus, red and infrared LEDs in the oximeter alternately transmit light, and a photodiode receives the light that is not absorbed. The ratio of the red and infrared light received by the photodiode is used to calculate the percentage of oxygen in the blood. Based on the pulsatile nature of arterial blood flow, the pulse rate and strength are also determined and displayed during the measurement cycle.

Sensor Cable Calibration

Pulse oximeter sensor cables are removable and often disposable. The performance of the LEDs and the photodiode in the cable can vary due to either manufacturing tolerances or alternate versions of the sensor. The performance of the pulse oximeter can be improved by incorporating nonvolatile memory such as EPROM or EEPROM into the sensor cable to store calibration coefficients. This calibration data is used by the base unit to optimize the performance of the particular optical components in the sensor.

Because the electromechanical connector for the sensor cable typically has limited pins, system designers must add this calibration functionality with minimal interconnect. The simplest and most robust method to do this is to add a 1-Wire memory device to the cable connector. The 1-Wire protocol is a proven serial interface that uses only one connector pin to add calibration and other functionality to pin-limited designs.

Additionally, since each 1-Wire product is designed with high ESD protection built in, designers do not need to use external protection diodes.

An added benefit of 1-Wire memory devices is that they can be used to pass updates or new algorithms to the base unit, thereby providing a vehicle for in-field upgrades. They can also enable aftermarket control by allowing only approved sensor cables to be used. A unique 64-bit serial identification number is inscribed in each 1-Wire device. By writing to a lockout bit in the memory device, manufacturers are able to control how many times the sensor can be used before replacement is required. Replacement is driven by safety concerns and, more specifically, by patient contamination issues.

Pulse Oximeter Solutions

Transmit Path: Driving the LEDs

The red and infrared LEDs are driven alternately with a precise current; a quiet time occupies the interval between each alternating pulse. The repetition rate is not fast, usually well under 10kHz. The duty cycle is also low to keep overall power down and to allow ambient-light measurement while both LEDs are off. Most of the time the LEDs are at the end of a cable, so system designers prefer to drive the LEDs with current from the base unit. This approach reduces current errors and requires fewer lines in the cable, which, in turn, reduces cost and weight. The current used to drive the LEDs must have minimal noise because any noise in the bandwidth of interest will degrade the signal-to-noise ratio (SNR) of the system and decrease its ability to measure low oxygen-saturation levels in critically ill patients.

Off-the-shelf LED drivers are not typically used in this application for several reasons. It is difficult to accurately and precisely program the LED current with the required resolution, since the backlighting applications for which they are designed do not require high resolution. Also, if a switching topology is used for the LED driver, then the current noise will be too high. It is possible that an LED driver with a linear topology could be used, but this approach is not ideal due to the lack of resolution in programming the current.

The LEDs can be driven independently with a line from the base unit for each LED along with a shared ground. Alternatively, to save connector pins and lines, the LEDs can be driven in a back-to-back or antiparallel configuration. Figure 1 shows a method for driving the two LEDs in the cable using two digital-to-analog converters (DACs) to independently set the currents in the LEDs. The advantage of using two DACs is that they can be heavily filtered to reduce the noise because their output is relatively static. LED modulation is performed after the filtering of the DACs in this topology.

Figure 1. Simplified red and infrared LED bias and control circuit.

Figure 1. Simplified red and infrared LED bias and control circuit.

In all topologies, the operational amplifier used in the force-sense (FS) configuration needs to have low voltage noise and high enough bandwidth to modulate the LEDs. A single DAC can be used to reduce cost, but the performance may suffer if the noise increases. The peak current through each LED varies according to the characteristics of each LED and photodiode, and with the duration of each pulse. In practice, the peak current ranges from tens of mA to hundreds of mA across all oximeters, though individual meters will use a narrower range of currents.

Receive Path: Photodiode Interface, Signal Conditioning, and Data Conversion

A photodiode receives both ambient and modulated light from the red and infrared LEDs, and then generates a current that will be measured over time to determine oxygen saturation. The photodiode current is most often converted to a voltage using an operational amplifier in a transimpedance configuration, also called a transimpedance amplifier (TIA). The light received by the photodiode largely comprises ambient light that is not useful for determining oxygen saturation or pulse. The small amount of red or infrared light not absorbed by the tissue, venous blood, or arterial blood is the signal of interest and is buried in the ambient light.

Figure 2 presents a simplified circuit for converting the photodiode current to a voltage, for signal conditioning, and for analog-to-digital conversion. This circuit converts both the red and infrared signals together and then processes them in the digital domain. Alternate topologies exist where the red and infrared light are separated in the analog domain using synchronous demodulation. This technique allows the use of slow but high-resolution analog-to-digital converters (ADCs); however, it is poor at detecting motion artifacts.

Figure 2. Simplified photodiode receive path circuit.

Figure 2. Simplified photodiode receive path circuit.

The key specifications for the TIA are extremely low input current, input current noise, and input voltage noise, as well as high-voltage operation. These characteristics are necessary to maximize the SNR so that the small currents of interest can be measured amid the large ambient currents. High-voltage operation means that a larger feedback resistor can be used to easily amplify the ambient and received LED current before removing the ambient portion with a highpass filter. The remaining small signal of interest is then amplified to maximize the ADC's dynamic range. This gain stage should be programmable to compensate for changing environmental factors and the aging of optical components.

The key specifications for the ADC are high SNR and sample rate. The sample rate should be fast enough to capture the modulated signal and perform the required digital processing, which is different for each manufacturer.

Display and Backlighting

If a bedside pulse oximeter is part of a multiparameter patient monitor, it does not require its own display because it uses the large color display incorporated in the patient monitor. Bedside monitors dedicated to pulse oximetry will usually have a medium-sized color display, or they can incorporate a touch-sensitive display to enhance the user interface and reduce the number of dedicated buttons. Handheld models have either a simple LED or LCD segment display or a more advanced dotmatrix LCD display. Fingertip units have the space and power only for a small and simple LED or LCD display. Simple displays can be driven by the display drivers found in many microcontrollers; dot-matrix or more advanced displays will require dedicated circuitry or a turnkey display solution. Backlighting is not required for LED displays; a few white LEDs can be used to backlight small LCD displays.

Data Interface

Most handheld and bedside models have the ability to interface with a computer. This data transfer is usually performed by a health-care provider or technician and not by the patient. Traditionally, the data interface has used RS-232, and the format has been proprietary to the manufacturer. Pulse oximeters are now migrating toward USB or wireless (Bluetooth®, Wi-Fi®) interfaces, and in the future oximeters will be able to securely transfer data to any device with these standard interfaces.

Audible Alarms

Audible alarms range from simple buzzers to speakers outputting multiple tones, levels, and patterns. A simple buzzer can be driven by one or two microcontroller port pins with pulse-width modulation (PWM) capability. More advanced audible alarms can be achieved by adding an audio DAC along with a speaker amplifier.

Power and Battery Management

A pulse oximeter needs to generate multiple power-supply rails. Separate analog (3V) and often multiple digital (3V, 1.8V) supplies are required if there are low-voltage cores requiring their own supply. A separate clean supply for powering the LEDs (5V) is usually required due to the power, headroom, and noise considerations. A high voltage (+30V or -30V) is sometimes required for the TIA connected to the photodiode to increase the SNR and, in some cases, for the display.

Fingertip models use two primary alkaline batteries in the AAA form factor while handheld models use either two primary AA alkaline or rechargeable batteries. Both models require a combination of step-up switching regulators, low-dropout linear regulators (LDOs), and sometimes an inverting switching regulator. Bedside monitors are mainly line powered but will use lithium-ion (Li+) or nickel-metal-hydride (NiMH) rechargeable backup batteries. A regulated 5V DC voltage is usually supplied, so the power-supply design is different than the fingertip and handheld models. Battery charging and fuel gauges are needed for the models with rechargeable batteries, as well as authentication for safety and after-market control if the batteries are removable.

Electrostatic Discharge

Electrostatic discharge (ESD) is a concern where the sensor cable plugs in. This potential problem can be addressed with dedicated ESD line protectors, as well as careful design and layout of the board. The use of ESD-protected interfaces allows designers to avoid the space and cost associated with discrete protection components. ESD is also possible at the data port and printer port, if the oximeter is equipped with one. Air discharge may also need to be addressed for the buttons and display through small openings in the casing, but this depends on the individual oximeter design.



Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

MAX7032
PRODUCTION

Low-Cost, Crystal-Based, Programmable, ASK/FSK Transceiver with Fractional-N PLL

MAX2830
PRODUCTION

2.4GHz to 2.5GHz 802.11g/b RF Transceiver with PA and Rx/Tx/Diversity Switch

MAX2829
PRODUCTION

Single-/Dual-Band 802.11a/b/g World-Band Transceiver ICs

MAX9718 PRODUCTION

Low-Cost, Mono/Stereo, 1.4W Differential Audio Power Amplifiers

MAX9618 PRODUCTION

Single/Dual SC70, Zero-Drift, High-Efficiency, 1.5MHz Op Amps with RRIO

MAX9945 PRODUCTION

38V, Low-Noise, MOS-Input, Low-Power Op Amp

MAX9939 PRODUCTION

SPI-Programmable Gain Amplifier (PGA) with Input VOS Trim and Output Op Amp

MAX4252 PRODUCTION

UCSP, Single-Supply, Low-Noise, Low-Distortion, Rail-to-Rail Op Amps

MAX5812 PRODUCTION

12-Bit Low-Power, 2-Wire, Serial Voltage-Output DAC

MAX5535 PRODUCTION

Dual, Ultra-Low-Power, 12-Bit, Voltage-Output DACs

MAX5137 PRODUCTION

Pin-/Software-Compatible, 16-/12-Bit, Voltage-Output DACs

MAX1393 Obsolete

1.5V to 3.6V, 312.5ksps, 1-Channel True-Differential/2-Channel Single-Ended, 12-Bit, SAR ADCs

MAX1168 PRODUCTION

Multichannel, 16-Bit, 200ksps Analog-to-Digital Converters

MAX1396 Obsolete

1.5V to 3.6V, 312.5ksps, 1-Channel True-Differential/2-Channel Single-Ended, 12-Bit, SAR ADCs

MAX1162 PRODUCTION

16-Bit, +5V, 200ksps ADC with 10µA Shutdown

MAX1167 PRODUCTION

Multichannel, 16-Bit, 200ksps Analog-to-Digital Converters

MAX6029 PRODUCTION

Ultra-Low-Power Precision Series Voltage Reference

MAX6173 PRODUCTION

High-Precision Voltage References with Temperature Sensor

MAX6033 PRODUCTION

High-Precision, Low-Dropout SOT23 Series Voltage Reference

MAX9850 PRODUCTION

Stereo Audio DAC with DirectDrive® Headphone Amplifier

DS2460 PRODUCTION

SHA-1 Coprocessor with EEPROM

DS28E05 PRODUCTION

1-Wire EEPROM

DS2502

1Kb Add-Only Memory

DS2431 PRODUCTION

1024-Bit 1-Wire EEPROM

MAXQ622 PRODUCTION

16-Bit Microcontrollers with Infrared Module and Optional USB

MAXQ2010 Obsolete

16-Bit Mixed-Signal Microcontroller with LCD Interface

MAXQ2000 NOT RECOMMENDED FOR NEW DESIGNS

Low-Power LCD Microcontroller

MAXQ8913 Obsolete

16-Bit, Mixed-Signal Microcontroller with Op Amps, ADC, and DACs for All-in-One Servo Loop Control

MAXQ610 PRODUCTION

16-Bit Microcontroller with Infrared Module

DS28E01-100 PRODUCTION

1Kb Protected 1-Wire EEPROM with SHA-1 Engine

DS28E02 PRODUCTION

1-Wire SHA-1 Authenticated 1Kb EEPROM with 1.8V Operation

MAX8530 LAST TIME BUY

Dual Low-Dropout Linear Regulator with Reset or Low-Noise Output in UCSP or QFN

MAX15029 PRODUCTION

1.425V to 3.6V Input, 500mA Low-Dropout Regulators with BIAS Input

MAX6950 PRODUCTION

Serially Interfaced, +2.7V to +5.5V, 5- and 8-Digit LED Display Drivers

MAX17043 PRODUCTION

1-Cell/2-Cell Fuel Gauge with ModelGauge and Low-Battery Alert

MAX8814 PRODUCTION

28V Linear Li+ Battery Charger with Smart Autoboot Assistant

DS2780 PRODUCTION

Stand-Alone Fuel Gauge IC

DS2756 PRODUCTION

High-Accuracy Battery Fuel Gauge with Programmable Suspend Mode

MAX8808X PRODUCTION

1A Linear Li+ Battery Chargers with Integrated Pass FET and Thermal Regulation in 2mm x 2mm TDFN

DS2784 PRODUCTION

1-Cell Fuel Gauge with FuelPack, Protector, and SHA-1 Authentication

MAX1916 PRODUCTION

Low-Dropout, Constant-Current Triple White LED Bias Supply

MAX16826 PRODUCTION

Programmable, Four-String HB LED Driver with Output-Voltage Optimization and Fault Detection

MAX16814 PRODUCTION

Integrated, 4-Channel, High-Brightness LED Driver with High-Voltage DC-DC Controller

MAX16838 PRODUCTION

Integrated, 2-Channel, High-Brightness LED Driver with High-Voltage Boost and SEPIC Controller

MAX16033 PRODUCTION

Low-Power Battery-Backup Circuits in Small µDFN Packages

MAX6720 PRODUCTION

Dual/Triple Ultra-Low-Voltage SOT23 µP Supervisory Circuits

MAX6746 PRODUCTION

µP Reset Circuits with Capacitor-Adjustable Reset/Watchdog Timeout Delay

MAX6381 PRODUCTION

SC70/µDFN, Single/Dual Low-Voltage, Low-Power µP Reset Circuits

MAX16054 PRODUCTION

On/Off Controller with Debounce and ±15kV ESD Protection

MAX6495 PRODUCTION

72V, Overvoltage-Protection Switches/Limiter Controllers with an External MOSFET

MAX8667 Obsolete

1.5MHz Dual Step-Down DC-DC Converters with Dual LDOs and Individual Enables

MAX8570 PRODUCTION

High-Efficiency LCD Boost with True Shutdown

MAX8569 PRODUCTION

200mA Step-Up Converters in 6-Pin SOT23 and TDFN

MAX11800 NOT RECOMMENDED FOR NEW DESIGNS

Low-Power, Ultra-Small Resistive Touch-Screen Controllers with I²C/SPI Interface

MAX7310 PRODUCTION

2-Wire-Interfaced 8-Bit I/O Port Expander with Reset

DS2480B

Serial to 1-Wire Line Driver

DS2482-100 PRODUCTION

Single-Channel 1-Wire Master

MAX9940 PRODUCTION

Signal-Line Overvoltage Protector for Low-Voltage Devices

MAX3208E PRODUCTION

Dual, Quad, and Hex High-Speed Differential ESD-Protection ICs

MAX3207E PRODUCTION

Dual, Quad, and Hex High-Speed Differential ESD-Protection ICs

MAX2831 PRODUCTION

2.4GHz to 2.5GHz, 802.11g RF Transceivers with Integrated PA

Product Categories
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project