LTM4641 TechClip - Paralleled Outputs

2017年09月18日

The LTM4641 can support a load up to 40A by combining the outputs of four devices. Using two LTM4641 µModule regulators in parallel, we demonstrate how well the output currents match even under a load transient.

LTM4641 TechClip - Paralleled Outputs

2017年09月18日
The LTM4641 can support a load up to 40A by combining the outputs of four devices. Using two LTM4641 µModule regulators in parallel, we demonstrate how well the output currents match even under a load transient.
Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成