LTspice: Stepping Parameters

2017年09月18日

This video provides an overview of how to use the .STEP command to perform repeated analysis of a circuit in LTspice.

In any LTspice simulation, varying a parameter in a device or model is just as important as plotting voltages or currents, as it allows you to compare performance and develop your circuit intuition.

There are two ways to examine a circuit by changing the value of a parameter: You can either manually enter each value then re-simulate the circuit, or you can use the .STEP command to sweep across a range of values in a single simulation run and produce a side-by-side comparison.

LTspice: Stepping Parameters

2017年09月18日

This video provides an overview of how to use the .STEP command to perform repeated analysis of a circuit in LTspice.

In any LTspice simulation, varying a parameter in a device or model is just as important as plotting voltages or currents, as it allows you to compare performance and develop your circuit intuition.

There are two ways to examine a circuit by changing the value of a parameter: You can either manually enter each value then re-simulate the circuit, or you can use the .STEP command to sweep across a range of values in a single simulation run and produce a side-by-side comparison.

Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成