How to Save Power in Your Next Portable Project Using the MAX32660 Deep Sleep Feature

2022年10月04日

Thomas discusses the power-saving features of the MAX32660, including its "deep sleep" mode of operation. He then demonstrates how this is used to save power in a temperature-sensing application.

Learn more:

How to Save Power in Your Next Portable Project Using the MAX32660 Deep Sleep Feature

2022年10月04日
Thomas discusses the power-saving features of the MAX32660, including its "deep sleep" mode of operation. He then demonstrates how this is used to save power in a temperature-sensing application.

Learn more:
Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成