How to Design a Complex Switching Regulator as Simple as a Linear Regulator - MicroModules

2017年09月18日

There is an alternative solution when deciding between a step-down switching regulator and a linear regulator. Switching regulators dissipate less heat than linear regulators especially when the input voltage is much higher than the output voltage or the output load current is relative high. On the other hand, linear regulators are very simple and don’t require inductors. What if there was a switching regulator circuit could be simplified and fitted inside a surface-mount package and the complete solution became as simple as a regulator’s circuit? No inductors, no MOSFETs, no difficult calculations for compensation circuitry. On paper, it is a simple square box with a few resistors and capacitors. On a PCB, it is also a simple square box with a few resistors and capacitors.

ADI's DC/DC µModule® regulators are complete switching regulator systems that are housed in compact surface-mount LGA (land grid array) package. All the complexity is addressed inside the package. What a designer needs to do is to simply choose a resistor to set the output voltage. This innovative regulator solution, allows system designers to save precious engineering time by minimizing the task of devising point-of-load regulators and obtain a complete solution that is encapsulated in a package resembling a surface-mount IC.

How to Design a Complex Switching Regulator as Simple as a Linear Regulator - MicroModules

2017年09月18日
There is an alternative solution when deciding between a step-down switching regulator and a linear regulator. Switching regulators dissipate less heat than linear regulators especially when the input voltage is much higher than the output voltage or the output load current is relative high. On the other hand, linear regulators are very simple and don’t require inductors. What if there was a switching regulator circuit could be simplified and fitted inside a surface-mount package and the complete solution became as simple as a regulator’s circuit? No inductors, no MOSFETs, no difficult calculations for compensation circuitry. On paper, it is a simple square box with a few resistors and capacitors. On a PCB, it is also a simple square box with a few resistors and capacitors.

ADI's DC/DC µModule® regulators are complete switching regulator systems that are housed in compact surface-mount LGA (land grid array) package. All the complexity is addressed inside the package. What a designer needs to do is to simply choose a resistor to set the output voltage. This innovative regulator solution, allows system designers to save precious engineering time by minimizing the task of devising point-of-load regulators and obtain a complete solution that is encapsulated in a package resembling a surface-mount IC.
Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成