LEDは普及が進むと同時に、より強力なものとなってきています。車両、広告掲示板、産業用照明をはじめとする多くのアプリケーションで1A、2A、3Aならびにそれ以上の高電流LEDストリングが使用されますが、これらのLEDストリングはDC/DCコンバータによって正確かつ効率的にドライブされる必要があります。多くの場合、LEDストリングと入力源の両方の電圧が変化するので、昇圧および降圧トポロジーが必要です。この場合、高効率で小型の4スイッチ同期整流式昇降圧コントローラが最良のソリューションとなります。 LT3791は、最大60Vの入力電圧から最大60Vの出力電圧を供給してLEDストリングをドライブする昇降圧コントローラICです。このデバイスは98%を超える効率で100Wを超えるLEDをドライブできます。入力電圧と出力電圧の関係が変化するのに伴い、降圧領域から昇降圧領域、さらに昇圧領域へとスムーズに移行します。LTCの最高性能のPWM調光により、正確かつスムーズなLED輝度制御を行います。LEDストリングの短絡状態と開放状態に対する保護機能と診断機能を備えているため、堅牢で有用性の高い昇圧/降圧LEDドライバとなっています。
LT3791は定電流DCレギュレータとしても、定電圧DCレギュレータとしても動作可能なので、短絡保護機能を備えた最大60Vの優れた高電力昇降圧電圧レギュレータとしても使用できます。特殊な密閉型鉛蓄電池チャージャには定電流と定電圧の両方が必要で、LT3791は充電電圧からフロート電圧への切り替えに使用できる独自の1/10チャージャ電流検出機能を備えているので、高電力の密閉型鉛蓄電池(SLA)を充電できます。