Tips for Writing Bulletproof Real-Time Clock Control Code

Mar 28 2014

Figure 1

   

Abstract

With the use of proper device initialization and code sequencing, accurate timekeeping and clock alarm operations become a more manageable task.

Introduction

When we read a clock, as we have all done since childhood, our eyes 'take a snapshot' of the present displayed values. Someone has already gone through the effort to reorient that display for your readability. When the microprocessor needs to access the real-time clock, the 'snapshot' of the latest register values must be reoriented into a sequence of time counts that we are more familiar with.

With the use of proper device initialization and code sequencing, accurate timekeeping and clock alarm operations become a more manageable task.

Device Initialization

Upon the first power application to a new clock component, the sequence of required I/O instructions may vary, based upon that specific component. Refer to the device specification for register structuring. As a general guideline, and assuming power is stable and the I/O port is operational, it is recommended to:

  1. Enable writing to the chip (if a software write-protection option exists)
  2. Enable the 32kHz RTC oscillator (if not auto-started)
  3. Define the hardware interrupt output configuration(s) (as applicable)
  4. Load initial counter values

Enable Writing to the RTC: This unique function was added to some component designs (for example, the DS1305) to prevent inadvertent clock changes. Refer to the product specification for the write-protect (WP) bit explanation.

Enable RTC Oscillator: On some legacy designs (such as DS12887, DS1307), the RTC oscillator does not auto-start at first power-up. This operational feature was intended to prevent battery consumption during transit/storage, and must be enabled through I/O. Designs with an active-low EOSC bit in the Control register include a built-in oscillator auto-start function, executed upon the first power application. In some other designs like DS1685, it may also be necessary to identify the crystal load capacitance setting for proper oscillator operation.

Check 'OSF': Some RTC components contain an oscillator stop flag (OSF), allowing the user to monitor oscillator operation via periodic I/O. Upon initial power application, OSF will be set. After enabling the oscillator, clear OSF, and then periodically verify that the OSF bit remains Logic 0.

OSF may become Logic 1 based upon any of these conditions:

  1. Initial application of power
  2. Voltages on VCC and VBAT are insufficient to maintain oscillator operation
  3. %-overbar_pre%EOSC%-overbar_post% bit was set to 1, stopping the oscillator
  4. External influences upon the crystal (leakage, coupling, etc.)

Define Interrupt Output(s): Depending upon the specific component and the desired application, definition of the output functions should now be executed to prevent unintended signals from being sent to the microprocessor. Component programming options for real-time alarm(s), watchdog interrupt, square-wave output frequency, etc., should be selected to establish the desired pin/signal conditioning.

In devices with real-time alarms, every alarm register should initially be written to 00h (if binary-coded decimal (BCD)) or FFh (if binary) to prevent any inadvertent matching/interrupt generation. The alarm registers are not factory-initialized, and the associated alarm flags can appear at any time the alarm register contents match the real-time count.

Load Initial Counter (Time) Values: Again referring to the product's specification and register map, the order of counter loading or reading should be executed from least significant count to the most significant count. Figure 1 illustrates the counter orientation and carry functions for a typical BCD-formatted real-time clock component.

Figure 1. RTC counter chain.

Figure 1. RTC counter chain.

Whenever writing to the RTC, any write to the least significant counter byte resets the internal 1Hz chain, allowing the user one full second before any timekeeping counter bits subsequently increment. This 1Hz reset action, as well as synchronization techniques, are explained in further detail in the Time Synchronization section.

To facilitate ease of use, the registers are oriented in ascending weight and address order for your programming convenience.

BCD Format Binary (Seconds)
Hundredths of a Second (if so equipped) 00h -> FFh = 0 -> 255.
Seconds 00h -> FFh = 256. -> 65535.
Minutes 00h -> FFh = 65536. -> 16777215.
Hours 00h -> FFh = 16777216. -> 4294967295.
Day of Week
Date
Month
Year
Century (if so equipped)

Time Synchronization

To some users, the simple act of setting the clock (writing to the RTC) may accomplish the timekeeping accuracy goals for the real-time clock in that application. Depending upon the care taken when initializing our device, an initial clock-set error of a few seconds may be considered acceptable when weighed against the execution of the other tasks controlled by that application.

In other applications, it may be desired to synchronize the real-time clock with a known time standard, like WWV1. As previously mentioned, writing to the least significant counter byte resets the 1Hz countdown chain. Figure 2 illustrates how to reset the 1Hz countdown chain using an I2C Write sequence to the SECONDS register of a DS1340. The slave address byte (D0h), register address (00h), and 'updated Seconds value' (03h), are being transmitted to the component. Two representative examples of an asynchronous 1Hz square-wave output are shown to illustrate the resulting adjustment.

Figure 2. I/O-initiated clock synchronization (I2C format shown).

Figure 2. I/O-initiated clock synchronization (I2C format shown).

On the slave's acknowledgement of the data byte (27th rising edge of SCL), the slave simultaneously 1) pulls SDA low to ACK receipt of the data byte, 2) the 1Hz countdown chain is reset, and 3) the new Seconds value (03h in the Figure 2 example) is transferred into the Seconds register.

On the first 1Hz SQW waveform, the 1Hz signal was Logic 1 when the ACK occurred. SQW is immediately pulled low. Precisely 0.5 seconds after the ACK, the SQW output transitions high. Precisely 1.0 second after the ACK, SQW is pulled low, indicating 1 second has elapsed since the write completed. Reading the Seconds register now results in a content of 04h.

On the second 1Hz SQW diagram, the 1Hz signal was Logic 0 when the ACK occurred, so the SQW signal remains low until precisely 0.5 seconds after the ACK, where the 1Hz output will transition high. Precisely 1.0 second after the ACK, SQW is again pulled low, indicating 1 second has elapsed since the write completed. Reading the Seconds register now results in a content of 04h.

For products with 3-wire or SPI I/O, the equivalent trigger to the 27th SCL rising edge in Figure 2 is the next-occurring transition of either SCLK or Chip-Enable (CE or %-overbar_pre%CS%-overbar_post%, whichever input pin naming convention was used).

For products with Phantom I/O, the equivalent trigger to the 27th SCL rising edge in Figure 2 is the termination of the 72nd write cycle in the serial data packet (including the 64-cycle pattern recognition).

For products with Byte-Wide I/O, the equivalent trigger to the 27th SCL rising edge in Figure 2 would be the termination of a write cycle to the Seconds register.

Using Time-of-Day Alarms

On devices with one or more real-time alarm circuits, the user can request either periodic or non-periodic interrupt events to occur at some predetermined time. Alarms can be set up to 30 days in advance of the desired event.

Programming of the alarms suggests use of a few simple rules:

  1. Initialize all alarm registers to a known state one time (alarms are not POR-reset)
  2. Never change Real-Time Clock register settings when an alarm circuit is enabled
  3. Never change Alarm register settings when that alarm circuit is enabled
  4. Clear the associated Alarm Flag before enabling that alarm (or you may create a premature interrupt)

The most common periodic interrupt is a 'daily alarm', set to activate at 5:30AM, fully independent of the calendar content. To ignore the DAY/DATE register, we will utilize an alarm mask.

Control = 04h			;oscillator on, define %-overbar_pre%INT%-overbar_post%/SQW output function, alarms off
Alarm1 SECONDS = 00h		;0 seconds
Alarm1 MINUTES = 30h		;30 minutes
Alarm1 HOURS = 45h		;5AM in 12hr Mode
Alarm1 DAY/DATE = 80h		;alarm mask set to match on 'Hours, Minutes & Seconds'
Status = 00h			;clear both alarm flags
Control = 05h			;now enable Alarm1 (A1IE=1)

At the next occurrence of 5:30AM, the %-overbar_pre%INT%-overbar_post%/SQW pin will assert.

To clear the interrupt, leaving the alarm enabled for the following morning at the same time, clear the associated Alarm Flag (A1F).

To clear the interrupt and disable any future alarms, clear the associated Alarm Enable (A1IE).

When the associated alarm is disabled, those alarm registers can be used for general-purpose data storage.

Conclusion

Component initialization procedures, when properly sequenced, should include definitions for all of the RTC's hardware functionality required for stable system operation. If desired, the real-time clock can also be synchronized to an external time base, and a procedure for that synchronization has been outlined. Additionally, optional use of real-time clock alarms has been included, focusing upon the order of execution of I/O instructions.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Products

DS1629
PRODUCTION

Digital Thermometer and Real-Time Clock/Calendar

DS1677
Obsolete

Portable System Controller

DS1511
PRODUCTION

Y2K-Compliant Watchdog Real-Time Clocks

DS3232 PRODUCTION

Extremely Accurate I²C RTC with Integrated Crystal and SRAM

DS1682 PRODUCTION

Total-Elapsed-Time Recorder with Alarm

DS1672 PRODUCTION

I²C 32-Bit Binary Counter RTC

DS1392 PRODUCTION

Low-Voltage SPI/3-Wire RTCs with Trickle Charger

DS17885 PRODUCTION

3V/5V Real-Time Clocks

DS1302 PRODUCTION

Trickle-Charge Timekeeping Chip

DS17285 PRODUCTION

3V/5V Real-Time Clocks

DS12885 PRODUCTION

Real-Time Clocks

DS1642 Obsolete

Nonvolatile Timekeeping RAM

DS1341 PRODUCTION

Low-Current I²C RTCs for High-ESR Crystals

DS12C887 PRODUCTION

Real-Time Clocks

DS1500 Obsolete

Y2K-Compliant Watchdog RTC with NV Control

DS3231 PRODUCTION

Extremely Accurate I²C-Integrated RTC/TCXO/Crystal

DS1315 PRODUCTION

Phantom Time Chip

DS1744 PRODUCTION

Y2K-Compliant, Nonvolatile Timekeeping RAMs

DS1371 PRODUCTION

I²C, 32-Bit Binary Counter Watchdog Clock

DS12C887A

Real-Time Clocks

DS1339 PRODUCTION

I²C Serial Real-Time Clock

DS12887A

Real-Time Clocks

DS1685 PRODUCTION

3V/5V Real-Time Clock

DS1394 PRODUCTION

Low-Voltage SPI/3-Wire RTCs with Trickle Charger

DS1553 Obsolete

64kB, Nonvolatile, Year-2000-Compliant Timekeeping RAM

DS3234 PRODUCTION

Extremely Accurate SPI Bus RTC with Integrated Crystal and SRAM

DS3232M PRODUCTION

±5ppm, I²C Real-Time Clock with SRAM

DS3231M PRODUCTION

±5ppm, I2C Real-Time Clock

DS17287 PRODUCTION

3V/5V Real-Time Clocks

DS1743 Obsolete

Y2K-Compliant, Nonvolatile Timekeeping RAMs

DS17887 PRODUCTION

3V/5V Real-Time Clocks

DS1644 Obsolete

Nonvolatile Timekeeping RAM

DS1344 PRODUCTION

Low-Current SPI/3-Wire RTCs

DS1338 PRODUCTION

I²C RTC with 56-Byte NV RAM

DS12887 PRODUCTION

Real-Time Clocks

DS1746 PRODUCTION

Y2K-Compliant, Nonvolatile Timekeeping RAMs

DS12R885 PRODUCTION

RTCs with Constant-Voltage Trickle Charger

DS1647 Obsolete

Nonvolatile Timekeeping RAM

DS1343 PRODUCTION

Low-Current SPI/3-Wire RTCs

DS1501 PRODUCTION

Y2K-Compliant Watchdog Real-Time Clocks

DS1244 PRODUCTION

256k NV SRAM with Phantom Clock

DS1687 PRODUCTION

3V/5V Real-Time Clock

DS1673 PRODUCTION

Portable System Controller

DS1372 PRODUCTION

I²C, 32-Bit, Binary Counter Clock with 64-Bit ID

DS1306 PRODUCTION

Serial Alarm Real-Time Clock

DS17485 PRODUCTION

3V/5V Real-Time Clocks

DS1646 Obsolete

Nonvolatile Timekeeping RAM

DS1391 PRODUCTION

Low-Voltage SPI/3-Wire RTCs with Trickle Charger

DS1375 PRODUCTION

I²C Digital Input RTC with Alarm

DS1554 PRODUCTION

256k Nonvolatile, Y2K-Compliant Timekeeping RAM

DS12R887 Obsolete

RTCs with Constant-Voltage Trickle Charger

DS1305 PRODUCTION

Serial Alarm Real-Time Clock

DS1340 PRODUCTION

I²C RTC with Trickle Charger

DS1557 PRODUCTION

4Meg, Nonvolatile, Y2K-Compliant Timekeeping RAM

DS1318 PRODUCTION

Parallel-Interface Elapsed Time Counter

DS1670 PRODUCTION

Portable System Controller

DS1390 PRODUCTION

Low-Voltage SPI/3-Wire RTCs with Trickle Charger

DS1747 PRODUCTION

Y2K-Compliant, Nonvolatile Timekeeping RAMs

DS1339B PRODUCTION

Low-Current, I2C, Serial Real-Time Clock for High-ESR Crystals

DS1251 RECOMMENDED FOR NEW DESIGNS

4096K NV SRAM with Phantom Clock

DS17487 PRODUCTION

3V/5V Real-Time Clocks

DS1678 PRODUCTION

Real-Time Event Recorder

DS1388 PRODUCTION

I²C RTC/Supervisor with Trickle Charger and 512 Bytes EEPROM

DS1556 PRODUCTION

1M, Nonvolatile, Y2K-Compliant Timekeeping RAM

DS1683 PRODUCTION

Total-Elapsed-Time and Event Recorder with Alarm

DS1307 PRODUCTION

64 x 8, Serial, I²C Real-Time Clock

DS1393 PRODUCTION

Low-Voltage SPI/3-Wire RTCs with Trickle Charger

DS1339A PRODUCTION

Low-Current, I²C, Serial Real-Time Clock

DS1742 Obsolete

Y2KC Nonvolatile Timekeeping RAM

DS1347 PRODUCTION

Low-Current, SPI-Compatible Real-Time Clock

DS1337 PRODUCTION

I²C Serial Real-Time Clock

DS1643 Obsolete

Nonvolatile Timekeeping RAM

DS1342 PRODUCTION

Low-Current I²C RTCs for High-ESR Crystals

DS1248 PRODUCTION

1024K NV SRAM with Phantom Clock

Product Categories
Latest Media 21
Title
Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project