Considerations on High-Speed Converter PCB Design, Part 4: Plane Coupling

QUESTION:

What are some important PCB layout rules when using a high-speed converter?

RAQ:  Issue 78

Answer:

Part 1 of this series discussed why splitting AGND and DGND is not necessary unless circumstances within the design force you to make that choice. Part 2 discussed the design of the power delivery system (PDS), and how squeezing the power and ground planes together provide added capacitance. Part 3 discussed how wise design of the E-Pad gets the best performance and most heat out of your signal chain design. Part 4 will make light of cross coupling between layers and planes within the PCB.

It is inevitable that some high-speed converter layouts will have a circuit plane overlapping another within the PCB design. In some cases, a sensitive analog plane (power, ground, or signal) might be directly above a noisy digital plane. Most designers wouldn't think that this would matter, as the planes are on different layers. So, here's a simple test:

Choose one of the adjacent layers and inject a signal on that plane. Next, connect the cross-coupled layer to a spectrum analyzer. Can you see how much signal is coupling through to the adjacent layer? Even though they might be separated by 40 mils, adjacent layers still form a capacitor in some sense, and will therefore still couple signal from one plane to another at some frequency.

Let's say a noisy digital plane on one layer has a 1-V signal that switches at a high speed. With 60-dB isolation between the layers, the non-driven layer will "see" 1 mV of coupling from the driven layer. To a 12-bit analog-to-digital converter (ADC) with a 2-V p-p full-scale swing, this is 2 LSBs (least significant bits) of coupling. This may be fine for your particular system, but keep in mind that as you increase the resolution from 12 bits to 14 bits, the sensitivity quadruples, so the error increases to 8 LSBs.

Ignoring cross-plane/cross-layer coupling will probably neither make the system fail nor cripple the design, but be aware, because more coupling exists between two planes than what might be imagined.

Keep this in mind when noise spurs are seen coupling in the frequency spectrum of interest. Sometimes layouts dictate that unintended signals or planes be cross-coupled to a different layer. Remember this when debugging your sensitive systems: the issue may lie one layer below.

Author

Rob Reeder

Rob Reeder

Rob Reeder is a senior system application engineer with Analog Devices in the High Speed Converter and RF Applications Group in Greensboro, North Carolina. He has published numerous articles on converter interfaces, converter testing, and analog signal chain design for a variety of applications. Formerly, Rob was an application engineer for the Aerospace and Defense Group for five years, where he focused on a variety of radar, EW, and instrumentation applications. Previously he was part of the high speed converter product line for nine years. His prior experience also includes test development and analog design engineering for the Multichip Products Group at ADI, where he designed analog signal chain modules for space, military, and high reliability applications for five years. Rob received his M.S.E.E. and B.S.E.E. from Northern Illinois University in DeKalb, Illinois, in 1998 and 1996, respectively. When Rob isn’t writing papers late at night or in the lab hacking up circuits, he enjoys hanging around at the gym, listening to techno music, building furniture out of old pallets, and, most importantly, chilling out with his two boys.