The Zero-Transistor IC, a New Plateau in IC Design

2013年04月01日

Figure 1

   

要約

We can apply a BiCMOS integrated circuit with only resistors and no transistors to solve a difficult design problem. The mythically perfect operational amplifier's gain and temperature coefficient are dependent on external resistor values. Maxim precision resistor arrays are manufactured together on a single die and then automatically trimmed, to ensure close ratio matching. This guarantees that the operational amplifier (op amp) gain and temperature coefficient are predictable and reliable, even with large production volumes.

A similar version of this article appeared in the March 1, 2013 issue of Electronics World magazine.

Introduction

This article explains how a BiCMOS integrated circuit with only resistors and no transistors can solve a difficult design problem. It examines how the mythically "perfect" operational amplifier's gain and temperature coefficient are dependent on external resistor values. It then examines some precision resistor arrays which are manufactured together on a single die and then automatically trimmed to ensure close ratio matching. This process guarantees that the op amp's gain and temperature coefficient are predictable and reliable, even with large production volumes.

The Perfect and Practical Op Amp

A BiCMOS IC without transistors, that's different! Now that we have your attention, we are trying to make a point. Why would anyone want an integrated circuit (IC) without transistors? Would anyone spend good money for a BiCMOS mask set without transistors?

For the answers, we must visit the land of practical operational amplifier (op amp) applications. And while there, we need to remember the old saying "a chain is only as strong as its weakest link." The mythical, perfect, million-dollar op amp has infinite gain and a zero temperature coefficient. In Figure 1, that perfect op amp is configured to provide noninverting amplification of an input signal.

Figure 1. A perfect op amp noninverting amplifier circuit.

Figure 1. A perfect op amp noninverting amplifier circuit.

What controls amplifier gain? More significantly, what controls the gain tolerance and the temperature coefficient? Is it the op amp or the resistors? The op amp will be no better than the resistors. Similarly, it is the resistors that dominate the temperature coefficient. Thus, precision resistor arrays can have an impact on op amp performance. We will use some arrays and op amps from Maxim to provide some as specific examples.

Tolerance in Precision Resistors: Averaging in Manufacturing and What Can Go Awry

Common op amps offer different operating bandwidths (Table 1) and each device can benefit from the precision resistor arrays. The close specifications of the precision resistors are transferred to the amplifier system. Among the transferred specifications are tight gain (as low as 0.035%), and a low temperature gain coefficient (1ppm/°C (typ)). Now the importance of precision resistors is becoming clear—chains do have weak links.

Table 1. Common Op Amps*
Part Description Unity Gain BW (MHz, typ)
MAX9619–MAX9620 Ultra-low power, zero-drift precision op amps in SC70 packages 1.5
MAX9636 3V/5V low-power, low-noise, CMOS, rail-to-rail I/O op amp 1.5
MAX44251 20V, ultra-precision, low-noise op amp 10
MAX9632 36V, precision, low-noise, wide-band amplifier 55
MAX44260 1.8V, 15MHz low-offset, low-power, rail-to-rail I/O op amp 15
MAX9613/MAX9615 Low-power, high-efficiency, single/dual, rail-to-rail I/O op amps 2.8
MAX9912 Dual, 200kHz, 4µA, rail-to-rail I/O op amp 0.2
MAX9916 Dual, 1MHz, 20µA, rail-to-rail I/O op amp in SOT23 1
MAX4036 Single, low IBIAS, 1.4V/800nA, rail-to-rail op amp 0.004
MAX4239 Ultra-low offset/drift op amp (AV ≥ 10) in SOT23 package 6.5
MAX4232 High-output-drive, 10MHz, 10V/µs, rail-to-rail I/O dual op amp 10
MAX4236 Very high precision, 3V/5V, rail-to-rail op amp (unity gain stable) in an 8-pin µMAX® package 1.7
MAX4472 Quad, 1.8V/750nA, rail-to-rail op amp in TSSOP package 0.009
MAX4253 Low-noise/distortion, low-power, rail-to-rail op amp 3
*For the latest information, refer to the device's data sheet.

Let's look at a simple example in which we will use two 10% tolerance resistors. While our prototype may have typical center-value resistors, we know that the production run will eventually encounter a situation with R1 and R2 at opposite ends of the tolerance bands. During the design, we have to consider these worst-case corners to ensure that the final complex system meets specifications. To deal with this, designers should create an error budget that assigns acceptable errors for each stage. By staying within the budget, you can assure specification compliance for the whole system.

One trick is to form each resistor from several larger-value parallel resistors. This uses the normal distribution of a manufacturing process to average the tolerance values, thus increasing the probability of maintaining the proper value. Of course, this is only true if the normal distribution pattern actually exists. This is a dangerous assumption if one does not control the manufacturing process. For example, resistor manufacturer A makes or trims the resistor at one edge instead of at the center value. This could happen as a result of a chemistry error, or perhaps the trimming machine is out of tolerance. Worse, resistor manufacturer B makes the resistors that follow the normal distribution curve; however, they sort or bin the results. Figure 2 illustrates the normal distribution and the sort selection. Note that each of the bins except 1% are really two bins, one for higher than nominal value and a minus bin for parts lower than nominal.

Figure 2. Binning or sorting of manufacturing tolerances.

Figure 2. Binning or sorting of manufacturing tolerances.

The solid (black line) curve in Figure 2 looks good in a perfect world. However, where we live, not much is perfect. As the manufacturing tolerances move, the number of parts in each bin changes. The tolerance could move to the right (illustrated by the green dotted line), resulting in no yield at 1% tolerance. It could be bimodal (illustrated by the gray dashed line) with many 5% and 10% tolerance parts and few 1% and 2% tolerance parts.

More importantly, this method seems to make sure that the 2% tolerance parts are only from minus 1 to minus 2 and plus 1 to plus 2 (no 1% parts). It also appears to remove any 1% and 2% tolerance parts from the 5% bin. We say "seems to" and "appears to," because sales volume and human nature also control the mix. For instance, the plant manager needs to ship 5% tolerance resistors, but he does not have enough to meet the demand this month. He does, however, have an overabundance of 2% tolerance parts. So, this month he throws them into the 5% bin and makes the shipment. Clearly deliberate, human intervention skews the statistics and method, but that plant manager gets his performance bonus. Such is the importance of the human factor.

Then there are other relevant human factors. If an operator is interrupted while unloading the bins, anything can happen. When he (a rhetorical "he" here, as we know that women hold these positions too) returns to working, will he remember to put the parts back in the proper bin? When a few parts spill, the operator does not want to be penalized (or yelled at), so the parts might go back into the most convenient bin. It is human nature and besides, who will ever know?

Then there are human factors when the board is stuffed. The part wanted is 2.52K. The operator is confused—does the correct reel say 2520, 2.533, or 2531? Is the nearest reel the proper one? Alternatively, during rework if some resistors are dropped, will he pick up the correct part, or will he pick up the resistors that he dropped last time? Will the operator admit a mistake or ask for help, taking the risk of some penalty? Human nature says no.

Packaging Resistor Arrays in a Zero-Transistor IC

With so many things to consider, how can a design engineer protect a design from errors? The zero-transistor IC (IC-packaged precision resistor arrays) comes to the rescue. In these integrated arrays, the resistors are very controlled. They have narrow tolerances and, most importantly, the ratio between the two resistors is accurately controlled (after all, it is the ratio that determines the gain). Furthermore, the temperature coefficient is well known and the resistors will track each other, since they are integrated close together on a single die and in a single package.

The resistor arrays are also manufactured together on the same wafer and are typically automatically tested and trimmed together. Yes, test escapes do happen—an operator can dump parts from the bad bin into the good bin. But the places where this can happen are minimized to just one station instead of many. Using automatic test equipment (ATE), it is very common to see a physical lock on the bad bin. Such an operating procedure ensures that the good parts are removed from the test floor and stowed in inventory, before the bad parts are unlocked and discarded.

As the boards are manufactured, the chance of assembly errors is also reduced, since one package now replaces several discrete resistors. It also requires just a single insertion, rather than multiple components being inserted into the PC board.

If the discrete resistors used in Figure 1 are replaced by a pair of MAX5490 precision resistors (Figure 3), the schematic is basically the same. However, the physical co-integration of the resistors provides excellent resistance matching.

Figure 3. The MAX5490 precision resistor pair.

Figure 3. The MAX5490 precision resistor pair.

In fact, resistor arrays often offer a choice of 0.035% (A grade), 0.05% (B grade), and 0.1% (C grade) tolerances. At one part per million, the temperature drift of the devices is extremely low. It is the resistance ratio (effectively gain stability) that is guaranteed to be less than 1ppm/°C (typ) over -55°C to +125°C. The end-to-end resistance of the pair is 100kΩ. Five standard and other custom-resistance ratios from 1:1 to 100:1 are available from tiny 3-pin SOT23 packages. The operating voltage across the resistors is greater than most op amps—up to 80V across the sum of R1 and R2. Additionally, the resistance-ratio long-term stability is typically 0.03% over 2000 hours at 70°C.

The MAX5490 precision-resistor pair allows the use of normal op-amp application circuits. Figure 4, Figure 5, and Figure 6 illustrate the simplest common circuits. To show the typical range of resistor arrays commonly available, Table 2 sums up Maxim's family of arrays. Such arrays can support and simplify system designs, based on instrumentation amplifiers, current-to-voltage converters, filters, adders, level shifters, impedance converters, load isolators, and more.

Table 2. Maxim Resistor Arrays*
Part Description End-to-End Resistance (kΩ) Resistance Tolerance (%) Temp. Coefficient (ppm/°C, typ)
MAX5492 10kΩ, ±2kV ESD precision-matched resistor-divider 10 0.025 35
MAX5491 30kΩ, ±2kV ESD precision-matched resistor-divider 30 0.025 35
MAX5490 100kΩ, ±2kV ESD precision-matched resistor-divider 100 0.025 35
MAX5426 Digitally programmable resistor and switch network for instrumentation amps 15 0.025 35
MAX5431 ±15V digitally programmable precision voltage-divider and switch for programmable gain amplifiers (PGAs) with input bias resistor 57 0.025
MAX5430 Digitally programmable precision voltage-divider and switch for PGAs 15 0.025
MAX5421 Digitally programmable precision voltage-divider and switch for PGAs with input bias resistor 15 0.025
MAX5420 Digitally programmable precision voltage-divider and switch for PGAs 0.025 0.025
*For the latest information, refer to the device's data sheet.

Figure 4. Inverting input op amp.

Figure 4. Inverting input op amp.

Figure 5. Buffered input attenuator.

Figure 5. Buffered input attenuator.

Figure 6. Buffered output attenuator.

Figure 6. Buffered output attenuator.

The data sheet for the MAX5490 tells you to calculate bandwidth by using Equation 1. where C = CP3 and Equation 2.. CP3 is 2pF, so the bandwidth is 3MHz. This assumes that the op amp has sufficient bandwidth to support the resistor bandwidth.

In our example we used a pair of 50kΩ resistors with the expected low currents. However, as the resistance ratio changes, the current levels rise, causing self-heating. Obviously this must be considered when evaluating the temperature coefficient; the data sheet details the needed calculations to minimize this effect.

While the MAX5490 consists of a center-tapped 100kΩ resistor, parts that have other resistor values are available, such as the MAX5491(with a 30kΩ end-to-end resistance) and the MAX5492 (with a 10kΩ end-to-end resistance). Any of these values will be an aide in the design of a summing amplifier.

Summary

Thus, a zero-transistor IC is not such a ridiculous idea after all, especially when it produces resistors with extremely good tolerances. As a practical matter, great amplifiers depend on the tight resistor-pair ratios guaranteed by the MAX5490, MAX5491, and MAX5492.



myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成

この記事に関して

製品

MAX4036
製造中

+1.2Vバッファリファレンス付き、低IBIAS、+1.4V/800nA、レイルトゥレイルオペアンプ

MAX5430
製造中

PGA用、±15Vデジタル設定可能、高精度電圧分周器

MAX5420
製造中

PGA用、デジタル設定可能、高精度分圧器

MAX4488 製造中

SOT23、低ノイズ、低歪み、広帯域、レール・ツー・レールオペアンプ

MAX44251 製造中

20V、超高精度、ローノイズオペアンプ

MAX4239 製造中

超低オフセット/ドリフト、低ノイズ、高精度SOT23アンプ

MAX9620 製造中

シングル/デュアルSC70、ゼロドリフト、高効率、1.5MHzオペアンプ、RRIO内蔵

MAX9632 最終販売

36V、高精度、低ノイズ、高帯域アンプ

MAX9619 製造中

シングル/デュアルSC70、ゼロドリフト、高効率、1.5MHzオペアンプ、RRIO内蔵

MAX4327 製造中

シングル/デュアル/クワッド、低コスト、UCSP/SOT23、低電力、レイルトゥレイルI/Oオペアンプ

MAX9916 製造中

シャットダウン付き、1MHz、20µA、レール・ツー・レールI/Oオペアンプ

MAX4483 製造中

シングル/デュアル/クワッド、低コスト、単一電源、レール・ツー・レールオペアンプ、シャットダウン付

MAX4236 製造中

SOT23、超高精度、3V/5Vレイルトゥレイルオペアンプ

MAX4472 製造中

シングル/デュアル/クワッド、+1.8V/750nA、SC70、レイルトゥレイルオペアンプ

MAX9613 製造中

低電力、高効率、シングル/デュアル、レイルトゥレイルI/Oオペアンプ

MAX44260 製造中

1.8V、15MHz、低オフセット、低電力、レール・ツー・レールI/Oオペアンプ

MAX9636 製造中

3V/5V低電力、低入力バイアス、CMOS、レール・ツー・レールI/Oオペアンプ

MAX4291 製造中

超小型、+1.8V、超低消費電力、レイルトゥレイル入出力オペアンプ

MAX9615 製造中

低電力、高効率、シングル/デュアル、レイルトゥレイルI/Oオペアンプ

MAX9912 製造中

200kHz、4µA、シャットダウン内蔵、レイルトゥレイルI/Oオペアンプ

MAX4253 製造中

UCSP、単一電源、低ノイズ、低歪み、レール・ツー・レールオペアンプ

MAX4128 製造中

シングル/デュアル/クワッド、広帯域、低電力、単一電源、レイルトゥレイル入出力オペアンプ

MAX4232 製造中

シャットダウン付き、高出力ドライブ、10MHz、10V/µs、レール・ツー・レールI/Oオペアンプ、SC70

MAX5421 製造中

PGA用、デジタル設定可能、高精度分圧器

MAX5491 製造中

精度マッチング済み、抵抗分圧器、SOT23

MAX5426 最終販売

プログラマブル計測アンプ用、高精度抵抗ネットワーク

MAX5490 製造中

100kΩ精度マッチング済み抵抗分圧器、SOT23パッケージ

MAX5431 製造中

PGA用、±15Vデジタル設定可能、高精度電圧分周器

MAX5492 製造中

10kΩ精度整合済み抵抗分圧器、SOT23パッケージ

製品カテゴリ
最新メディア 21
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成