AD7794 6チャンネル差動入力、24ビットADC
2011年04月28日
AD7794は6チャンネル差動入力、24ビットのシグマデルタ型AD変換器です。超低ノイズ設計とチョッピング技術による高安定により、最大22ビットの有効ビットを備えた、高性能ADコンバータです。ブリッジタイプの圧力センサーやレンジの広い温度センサーに最適なこのデバイスについて、ご紹介します。
詳細は、AD7794の製品ページをご覧ください。AD7794 6チャンネル差動入力、24ビットADC
2011年04月28日
AD7794は6チャンネル差動入力、24ビットのシグマデルタ型AD変換器です。超低ノイズ設計とチョッピング技術による高安定により、最大22ビットの有効ビットを備えた、高性能ADコンバータです。ブリッジタイプの圧力センサーやレンジの広い温度センサーに最適なこのデバイスについて、ご紹介します。
詳細は、AD7794の製品ページをご覧ください。
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}