Getting Started with Hall-Effect Sensors Using the MAX9921

2022年10月04日

Jesvin explains the hall effect and how hall-effect sensors can be useful in applications that require contactless sensors such as an automatic door opener. He then demonstrates the MAX9921, which is the industry’s first two-wire hall-effect sensor.

Getting Started with Hall-Effect Sensors Using the MAX9921

2022年10月04日
Jesvin explains the hall effect and how hall-effect sensors can be useful in applications that require contactless sensors such as an automatic door opener. He then demonstrates the MAX9921, which is the industry’s first two-wire hall-effect sensor.

Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成