How to Extend I2C Lines Using the DS28E17 1-Wire-to-I2C Master

2022年10月04日

When trying to communicate with I2C over distances greater than two meters, several challenges may arise. Learn a method to extend I2C communication up to 100m using the 1-Wire® protocol and the DS28E17.

How to Extend I2C Lines Using the DS28E17 1-Wire-to-I2C Master

2022年10月04日
When trying to communicate with I2C over distances greater than two meters, several challenges may arise. Learn a method to extend I2C communication up to 100m using the 1-Wire® protocol and the DS28E17.
Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成