Dual IO-Link Master Transceiver: MAX14819 Demo

2022年10月04日

Learn how the IO-Link master transceiver addresses key trends for industrial communications with over 50% lower power dissipation, robust communications in harsh environments, and a scalable, flexible architecture.

See how easy it is to evaluate the MAX14819 using the 8-channel IO-Link master reference design as it communicates with an IO-Link proximity sensor.

Dual IO-Link Master Transceiver: MAX14819 Demo

2022年10月04日

Learn how the IO-Link master transceiver addresses key trends for industrial communications with over 50% lower power dissipation, robust communications in harsh environments, and a scalable, flexible architecture.

See how easy it is to evaluate the MAX14819 using the 8-channel IO-Link master reference design as it communicates with an IO-Link proximity sensor.

Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成