Boston Engineering BF506F Motor Control Demonstration

2011年09月19日

This platform uses a BF506F EZKit for developers to test the power of the BF506F. Features of the platform include: wide DC input range for currents up to 20A and interfaces for motor applications, such as encoders, hall sensors & current feedback.

Visit the BF506 Product Page

Boston Engineering BF506F Motor Control Demonstration

2011年09月19日
This platform uses a BF506F EZKit for developers to test the power of the BF506F. Features of the platform include: wide DC input range for currents up to 20A and interfaces for motor applications, such as encoders, hall sensors & current feedback.
Visit the BF506 Product Page
Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成