Intelligent Linear Motion Control for Fast and Accurate Positioning

2022年12月14日

See our high-speed, high-performance motor control demo showcasing ADI´s latest Trinamic servo controller in hardware and current sense amplifiers in an inverted pendulum application to help our customers achieve better performance and efficiency in their manufacturing processes.

Our robust, accurate, and high bandwidth ADI MagIC+ current sense technology monitors the required current of the application. An inverted pendulum is unstable without control, that is, the pendulum will simply fall over if the cart below the pendulum arm isn't moved to balance it. The objective of the control system is to balance the inverted pendulum by applying a force to the cart that the pendulum is attached to.

This video showcases precise and accurate ADI components and control algorithms with a brushless DC (BLDC) linear motor that will allow the pendulum to remain balanced and not fall over, even when an external force is applied to it. In addition, a contactless AC and DC current clamp meter is demonstrated that uses the ADAF1080 magnetic field sensor. The ADAF1080 enables high bandwidth current measurement in a contactless way without the need for shielding or flux concentrators greatly reducing cost and complexity for our customers.

40% to 50% of overall electric energy is used by e-motors. Using Field Oriented Control (FOC) BLDC Servos instead of DC Motors can allow customers to cut this motor energy consumption by 20% or more. No expert knowledge is needed to realize expert level motor control. Today, there are around 700 million motors in operation. Inefficient motors cause the majority of the pollution, and wasted energy driven by inefficient motors generates pollution unnecessarily.

At ADI, we are creating motor control solutions and components, such as current sense amplifiers (e.g. AD8410A) and servo controllers (e.g. TMC4671), that help our customers achieve better efficiency in their applications. Little efficiency gains that may save consumers millions of dollars each year in power could also help to conserve finite fossil fuel supply and keep pollution out of the environment.

Intelligent Linear Motion Control for Fast and Accurate Positioning

2022年12月14日

See our high-speed, high-performance motor control demo showcasing ADI´s latest Trinamic servo controller in hardware and current sense amplifiers in an inverted pendulum application to help our customers achieve better performance and efficiency in their manufacturing processes.

Our robust, accurate, and high bandwidth ADI MagIC+ current sense technology monitors the required current of the application. An inverted pendulum is unstable without control, that is, the pendulum will simply fall over if the cart below the pendulum arm isn't moved to balance it. The objective of the control system is to balance the inverted pendulum by applying a force to the cart that the pendulum is attached to.

This video showcases precise and accurate ADI components and control algorithms with a brushless DC (BLDC) linear motor that will allow the pendulum to remain balanced and not fall over, even when an external force is applied to it. In addition, a contactless AC and DC current clamp meter is demonstrated that uses the ADAF1080 magnetic field sensor. The ADAF1080 enables high bandwidth current measurement in a contactless way without the need for shielding or flux concentrators greatly reducing cost and complexity for our customers.

40% to 50% of overall electric energy is used by e-motors. Using Field Oriented Control (FOC) BLDC Servos instead of DC Motors can allow customers to cut this motor energy consumption by 20% or more. No expert knowledge is needed to realize expert level motor control. Today, there are around 700 million motors in operation. Inefficient motors cause the majority of the pollution, and wasted energy driven by inefficient motors generates pollution unnecessarily.

At ADI, we are creating motor control solutions and components, such as current sense amplifiers (e.g. AD8410A) and servo controllers (e.g. TMC4671), that help our customers achieve better efficiency in their applications. Little efficiency gains that may save consumers millions of dollars each year in power could also help to conserve finite fossil fuel supply and keep pollution out of the environment.

Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成