10BASE-T1S, Bringing System Advantages and Ready for Production

2023-04-13

The automotive industry is presently going through one of its most revolutionary periods. Car manufacturers need to provide solutions to several significant megatrends such as electrification, autonomy, and the fully connected car in a short period of time. One result of this is the OEMs’ need to radically modify their electrical and electronic architecture to support the new functionality. The industry is moving towards a common new architecture often referred to as a zonal architecture, which determines connectivity by physical location rather than function. One key enabling technology for zonal-based architectures is the new Ethernet standard 10BASE-T1S, which enables optimized connectivity to edge nodes removing the need for protocol translation required today for legacy connectivity technologies such as FlexRay and CAN. In this presentation, we will introduce the 10BASE-T1S technology, its alignment with Zonal architectures and the system advantages that it brings. We will provide insight into the near complete specification activities to ensure smooth rollout of the technology in time for next generation vehicles and discuss the different product offerings including Analog Devices 10BASE-T1S E2B solution, which provides the most optimized edge node connectivity solution available in the market.

10BASE-T1S, Bringing System Advantages and Ready for Production

2023-04-13
The automotive industry is presently going through one of its most revolutionary periods. Car manufacturers need to provide solutions to several significant megatrends such as electrification, autonomy, and the fully connected car in a short period of time. One result of this is the OEMs’ need to radically modify their electrical and electronic architecture to support the new functionality. The industry is moving towards a common new architecture often referred to as a zonal architecture, which determines connectivity by physical location rather than function. One key enabling technology for zonal-based architectures is the new Ethernet standard 10BASE-T1S, which enables optimized connectivity to edge nodes removing the need for protocol translation required today for legacy connectivity technologies such as FlexRay and CAN. In this presentation, we will introduce the 10BASE-T1S technology, its alignment with Zonal architectures and the system advantages that it brings. We will provide insight into the near complete specification activities to ensure smooth rollout of the technology in time for next generation vehicles and discuss the different product offerings including Analog Devices 10BASE-T1S E2B solution, which provides the most optimized edge node connectivity solution available in the market.
Latest Media 12
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目