Evaluation Software (2)
-
ADMxxxx Common Run-Time
This run-time installer is shared between the SuperSequencer, ADM1175-92, and the Hot Swap and Power Monitor tools. Contains driver support for the USB-SMBUS-CABLEZ and USB-SDP-CABLEZ interface connectors.-
Common Run-Time Installer v2.0.0
This file only needs to be downloaded and installed once for all tools that share it. (zip, 406 MB) -
Read Me for ADMxxxx Common Run-Time Installer
(rtf, 11 kB) -
Updating the USB-I2C Dongle Driver
(pdf, 97 kB) -
USB-SMBUS-CABLEZ, USB-5PSMBUS-CABLEZ: USB-to-I2C Interface Dongles
(pdf, 116 kB) Info on updating the USB-SMBUS-CABLEZ Windows device driver.
-
Common Run-Time Installer v2.0.0
-
SuperSequencer Software
Requires the ADMxxxx Common Run-time to be installed in order to provide driver support for the USB-SMBUS-CABLEZ and USB-SDP-CABLEZ interface connectors. If there are previous versions of this software (v4.0.6 or earlier), or the ADM1175-7 & ADM1191-92 software (v3.0.1 or earlier) installed they should be removed prior to installing the common run-time.-
SuperSequencer Configuration Tool - v4.2.1
(zip, 24 MB) Supports Windows XP, Windows Vista, and Windows 7 and is recommended for new installations. -
Read Me for the SuperSequencer Tools v4.2.1
(rtf, 79 kB) -
Read Me for the prog106x command line tool v2.0.1
(txt, 2 kB)
-
SuperSequencer Configuration Tool - v4.2.1