Introduction to the MAX20313-16 500mA to 6A Adjustable Current-Limit Switches

2022年10月04日

This video provides an introduction to the MAX20313–MAX20316 programmable current-limit switches, which feature internal current limiting to prevent damage to host devices due to faulty load conditions.

Introduction to the MAX20313-16 500mA to 6A Adjustable Current-Limit Switches

2022年10月04日
This video provides an introduction to the MAX20313–MAX20316 programmable current-limit switches, which feature internal current limiting to prevent damage to host devices due to faulty load conditions.
Latest Media 12
Title
Subtitle
さらに詳しく
myAnalogに追加

myAnalog のリソース セクション、既存のプロジェクト、または新しいプロジェクトに記事を追加します。

新規プロジェクトを作成