| Наименование |
Тип контента |
Тип файлов |
|
AD5200/AD5201: 256-Position and 33-Position Digital Potentiometers Data Sheet (Rev D, 12/2012) (pdf, 749 kB)
|
Технические описания |
PDF
|
|
AN-686: Implementing an I2C® Reset
(pdf, 44 kB)
|
Статьи по применению |
PDF
|
AN-582: Resolution Enhancements of Digital Potentiometers with Multiple Devices
(pdf, 135 kB)
Digital Potentiometers Can Be Paralleled, Stacked or Cascaded to Optimize Resolution.
|
Статьи по применению |
PDF
|
|
AN-580: 0: Programmable Oscillator Uses Digital Potentiometers
(pdf, 52 kB)
|
Статьи по применению |
PDF
|
AN-214: Ground Rules for High Speed Circuits
(pdf, 356 kB)
Layout and Wiring Are Critical in Video Converter Circuits.
|
Статьи по применению |
PDF
|
|
Choosing the Correct digiPOT for Your Application
(pdf, 431 kB)
|
Руководства по проектированию |
PDF
|
Understanding and Applying Digital Potentiometers
In this webcast our experts will explain the differences between Pots and DigiPots and DACs, and present considerations for successful designs for many applications.
|
Webcasts |
WEBCAST
|
|
Choosing the Correct digiPOT for Your Application
(pdf, 431 kB)
|
Обзор |
PDF
|
|
Is there a power up sequence I should follow?
|
FAQs/RAQs |
HTML
|
|
For dual supply digital potentiometers, if VDD/VSS are +2.5V/-2.5V respectively, can digital inputs be fed from a standard 3.3V CMOS logic component without logic level translation? What are the logic level thresholds when VDD is +2.5V and VSS is -2.5V?
|
FAQs/RAQs |
HTML
|
|
Is there a dependency between the logic level and power consumption?
|
FAQs/RAQs |
HTML
|
|
Is digital potentiometer a real replacement for mechanical potentiometer or are there restrictions regarding voltage potentials?
|
FAQs/RAQs |
HTML
|
|
Are all digital potentiometers limited to |5V|?
|
FAQs/RAQs |
HTML
|
|
Do digital potentiometers handle bipolar and AC operations?
|
FAQs/RAQs |
HTML
|
|
Can I achieve a 15V signal swing when using a 5V digital potentiometer?
|
FAQs/RAQs |
HTML
|
|
For digital potentiometers that do not have nonvolatile memory, what is the state during power up?
|
FAQs/RAQs |
HTML
|
|
Is there a particularly low-power digital potentiometer?
|
FAQs/RAQs |
HTML
|
|
Does the memory allow the device to return to the last stored value without an update from a micro?
|
FAQs/RAQs |
HTML
|
|
Will the data in the EEMEM need to be refreshed after 15 yrs when it is operated at 55°C?
|
FAQs/RAQs |
HTML
|
|
How many write cycles can the EEMEM go through before it fails?
|
FAQs/RAQs |
HTML
|
|
After the specified EEMEM data retention timeout period, can the power be turned off and back on so that the part is considered "refreshed"?
|
FAQs/RAQs |
HTML
|
|
Why are some digital potentiometers' maximum operating temperature only 85°C instead of the standard 125°C?
|
FAQs/RAQs |
HTML
|
|
How good is the resistance matching between Ch1 and Ch2 in the dual digital potentiometer?
|
FAQs/RAQs |
HTML
|
|
How is the resistance matching device to device?
|
FAQs/RAQs |
HTML
|
|
What is the resistance tolerance of the digital potentiometers?
|
FAQs/RAQs |
HTML
|
|
Can I cascade, serialize, or parallel multiple digital potentiometers to get the resistance or resolution I need? My requirement is for a 250 Ω digital potentiometer with approximately 1 Ω/step. I plan to use four 1 kΩ AD8403 in parallel with each set to nominally the same value.
|
FAQs/RAQs |
HTML
|
|
I would like to know how the digital potentiometer is built. How ideal are the wiper switches?
|
FAQs/RAQs |
HTML
|
|
What is the tempco of the digital potentiometer?
|
FAQs/RAQs |
HTML
|
|
What is the maximum current I can force into the digital potentiometer?
|
FAQs/RAQs |
HTML
|
|
Can a digitally controlled variable resistor withstand greater than 20mA?
|
FAQs/RAQs |
HTML
|
|
Can a digipot be used to construct a programmable high current source?
|
FAQs/RAQs |
HTML
|
|
If I use the digital potentiometer in a "dry" circuit (current through wiper < 1 pA), will it behave as a linear resistor in rheostat mode?
|
FAQs/RAQs |
HTML
|
|
Are ADI's digital potentiometers suitable for use in photodetector amplifiers and will they suffer from leakage currents which could affect the gain of the circuit?
|
FAQs/RAQs |
HTML
|
|
Regarding the spec on R-DNL, I am only concerned with relative adjustments. I'm not concerned with the actual value of the resistor in the digipot but need the digipot to be monotonic.
|
FAQs/RAQs |
HTML
|
|
Can I adjust the digital potentiometer for frequencies around 1MHz to 10MHz for adjusting the gain of a video signal?
|
FAQs/RAQs |
HTML
|
|
What is the maximum frequency that can be applied to the digital potentiometer CLK input?
|
FAQs/RAQs |
HTML
|
|
Is there crosstalk between Ch1 and Ch2 of a dual digital potentiometer such that a sine wave applied to Ch1 will occur in Ch2 as well?
|
FAQs/RAQs |
HTML
|
|
If I program Ch 1 from zero to full scale, will I expect Ch 2 to be disturbed?
|
FAQs/RAQs |
HTML
|
|
Digital Feedthrough
|
FAQs/RAQs |
HTML
|
|
How is the THD performance of digital potentiometer?
|
FAQs/RAQs |
HTML
|
|
If I use the digital potentiometer in audio volume control, will I experience zipper noise?
|
FAQs/RAQs |
HTML
|
|
For a digital potentiometer that requires 6-bit word length, what happens if I have 8-bit word length from my PC?
|
FAQs/RAQs |
HTML
|
|
For a digital potentiometer that requires 12-bit word length, how can I control with only 8-bit word length from my micro?
|
FAQs/RAQs |
HTML
|
|
Do you provide any software to control the digital potentiometers?
|
FAQs/RAQs |
HTML
|
|
How do I daisy-chain multiple potentiometers? How does the serial interface work for multiple AD8403's when there are still only two address bits? Are there multiple /CS lines, one for each individual chip?
|
FAQs/RAQs |
HTML
|
|
Can I program two channels of a multi-channel digital potentiometer at the same time?
|
FAQs/RAQs |
HTML
|
|
Can I read back the wiper setting of the digital potentiometers?
|
FAQs/RAQs |
HTML
|
|
Can I read back the contents of the two RDAC registers of AD5242 or AD5282 (dual I2C compatible digital potentiometer)?
|
FAQs/RAQs |
HTML
|
|
Is there a digital potentiometer controlled by a parallel input?
|
FAQs/RAQs |
HTML
|
|
Can digital potentiometers do log taper adjustment?
|
FAQs/RAQs |
HTML
|
|
I'm unsure about how to use pin 13 write protect (/WP), pin 14 preset (/PR), and pin 16 ready (RDY)?
|
FAQs/RAQs |
HTML
|
|
Why Should I replace mechanical potentiometers with digiPOT?
|
FAQs/RAQs |
HTML
|
|
What should I watch out for when I replace mechanical potentiometers with digital potentiometers?
|
FAQs/RAQs |
HTML
|
|
What is the ESD rating of digital potentiometers?
|
FAQs/RAQs |
HTML
|
|
How do I tell the end-to-end RAB resistance value?
|
FAQs/RAQs |
HTML
|
|
What are the common failure modes of digital potentiometers?
|
FAQs/RAQs |
HTML
|
|
Are there any evaluation boards for the digital potentiometers?
|
FAQs/RAQs |
HTML
|
|
Are PB-free digital potentiometers available?
|
FAQs/RAQs |
HTML
|
|
Can I use the new PB-free DigiPOTs in my traditional solder based PCB assembly process?
|
FAQs/RAQs |
HTML
|
|
Programmable 5-30V Power Supply
|
FAQs/RAQs |
HTML
|
|
Programmable LDO with Precision
|
FAQs/RAQs |
HTML
|
|
Manual Push Button LED Driver
|
FAQs/RAQs |
HTML
|
|
Adjustable Voltage Source for Driving LED
|
FAQs/RAQs |
HTML
|
|
Adjustable Current Source for Driving Single LED
|
FAQs/RAQs |
HTML
|
|
Adjustable Current Source for Driving Multiple LEDs
|
FAQs/RAQs |
HTML
|
|
Programmable Bidirectional Current Source
|
FAQs/RAQs |
HTML
|
|
High Power RGB LEDs Driver
|
FAQs/RAQs |
HTML
|
|
Automatic LED Brightness Control
|
FAQs/RAQs |
HTML
|
|
High Voltage DAC
|
FAQs/RAQs |
HTML
|
|
Bipolar DAC with EEPROM
|
FAQs/RAQs |
HTML
|
|
Voltage-to-Current Conversion
|
FAQs/RAQs |
HTML
|
|
Programmable Low Pass Filter
|
FAQs/RAQs |
HTML
|
|
Programmable State-Variable Filter
|
FAQs/RAQs |
HTML
|
|
Programmable Oscillator
|
FAQs/RAQs |
HTML
|
|
Audio Volume Control
|
FAQs/RAQs |
HTML
|
|
Audio Amplifier Volume Control
|
FAQs/RAQs |
HTML
|
|
LCD Panel VCOM Adjustment
|
FAQs/RAQs |
HTML
|
|
Laser Bias and Modulation Current Biasing
|
FAQs/RAQs |
HTML
|
|
Manual Rotary Control
|
FAQs/RAQs |
HTML
|
|
Bipolar Programmable Gain Amplifier
|
FAQs/RAQs |
HTML
|
|
Programmable Current-Sensing Amplifier
|
FAQs/RAQs |
HTML
|
|
6-Bit Controller
|
FAQs/RAQs |
HTML
|
|
Level Shifting Digital Inputs from 3.3V to 5V or Vice Versa
|
FAQs/RAQs |
HTML
|
|
Level Shifting Digital Signals from 0V to +5V to -5V to 0V
|
FAQs/RAQs |
HTML
|
|
Multiple I2C Slave Devices Addressing
|
FAQs/RAQs |
HTML
|
|
Resolution Enhancement
|
FAQs/RAQs |
HTML
|
|
Pseudo Memory Retention
|
FAQs/RAQs |
HTML
|
|
RAQs index
|
Rarely Asked Questions |
HTML
|
|
Словарь терминов
|
Глоссарий |
HTML |