| 快讯名称 | 内容类型 | 文件类型 |
|---|---|---|
| AD7708/AD7718: 16-Bit 8/10-Channel, Low Voltage, Low Power, Sigma Delta ADC Data Sheet (Rev 0, 08/2001) (pdf, 328 kB) | 产品数据手册 | |
|
AN-665: Σ-Δ ADC的通道切换
(pdf, 84 kB)
本应用笔记针对AD7708和AD7718。数据手册详细说明了Σ-Δ ADC的更新速率。 |
应用笔记 | |
|
AN-665: Channel Switching Using Σ-Δ ADCs
(pdf, 84 kB)
This application note refers to the AD7708 and AD7718. Data sheets specify the update rate for Σ-Δ ADCs. |
应用笔记 | |
|
AN-615: 峰峰值分辨率与有效分辨率
(pdf, 244 kB)
本应用笔记说明峰峰值分辨率与有效分辨率的区别。 |
应用笔记 | |
|
AN-615: Peak-to-Peak Resolution Versus Effective Resolution
(pdf, 70 kB)
This application note describes effective resolution and peak-to-peak resolution and highlights the difference between these two specifications. |
应用笔记 | |
|
AN-611: Σ-Δ ADC上的50 Hz/60 Hz干扰抑制
(pdf, 360 kB)
许多工业设置需要抑制50 Hz和60 Hz干扰。本应用笔记介绍如何使用AD7708/AD7718、AD7709、AD7719、AD7782/AD7783 Σ-Δ型ADC实现这些频率的最佳抑制。 |
应用笔记 | |
|
AN-611: 50 Hz/60Hz Rejection on Sigma-Delta ADCs
(pdf, 360 kB)
Rejection of 50 Hz and 60 Hz interference is a requirement in many industrial settings. This Application Note outlines how the AD7708/AD7718,AD7709,AD7719, AD7782/AD7783 Sigma-Delta ADCs are used for optimal rejection of these frequencies. |
应用笔记 | |
|
AN-610: Σ-Δ型ADC上的PGA
(pdf, 152 kB)
AD7708/AD7718、AD7709、AD7719、AD7782/AD7783高分辨率Σ-Δ型ADC全部在Σ-Δ调制器输入端集成了可编程增益放大器(PGA), |
应用笔记 | |
|
AN-610: The PGA on Sigma-Delta ADCs
(pdf, 152 kB)
The AD7708/AD7718,AD7709,AD7719,AD7782/AD7783 high resolution Sigma-Delta ADCs all feature a Programmable Gain Amplifier (PGA)at the input to the Sigma-Delta modulator. This Application Note discusses the use and benefits of this PGA. |
应用笔记 | |
|
AN-609: Σ-Δ ADC上的斩波
(pdf, 232 kB)
斩波是一项用于消除失调电压和其他低频误差的技术。本应用笔记简要介绍在AD7708/AD7718、AD7709和AD7782/AD7783高分辨率Σ-Δ ADC上是如何实现斩波的,及其带来的好处。 |
应用笔记 | |
|
AN-609: Chopping on Sigma-Delta ADCs
(pdf, 232 kB)
Chopping is a technique that can be used to cancel offset voltages and other low frequency errors. This Application Note outlines how chopping is implemented on the AD7708/AD7718,AD7709,AD7719,AD7782/AD7783 high resolution Sigma-Delta ADCs and discusses the resulting benefits it brings. |
应用笔记 | |
|
AN-608: Σ-Δ ADC上的输入缓冲器
(pdf, 260 kB)
ADI公司的AD7708/AD7718、AD7709、AD7719、 AD7782/AD7783高分辨率Σ-Δ ADC在输入端集成了高阻 抗缓冲器。本应用笔记讨论了集成片内缓冲器带来的显著优点和各种系统设计考虑因素。 |
应用笔记 | |
|
AN-608: Input Buffers on Sigma-Delta ADCs
(pdf, 284 kB)
The AD7708/AD7718,AD7709,AD7719,AD7782/AD7783 high resolution Sigma-Delta ADCs feature a high impedance buffer at the input to the ADC. This application note discusses the significant benefits and various system design considerations that result from the integration of on-chip buffers. |
应用笔记 | |
| AN-607: 选择低带宽(<15kSPS)Σ-Δ型ADC (pdf, 127 kB) | 应用笔记 | |
| AN-607: Selecting a Low Bandwidth (<15 kSPS) Sigma-Delta ADC (pdf, 222 kB) | 应用笔记 | |
|
AN-397: 标准线性集成电路的电诱发损坏
(pdf, 498 kB)
最常见起因和防止再发生的相关处理 |
应用笔记 | |
|
AN-397: Electrically Induced Damage to Standard Linear Integrated Circuits:
(pdf, 149 kB)
The Most Common Causes and the Associated Fixes to Prevent Reoccurrence |
应用笔记 | |
|
AN-389: 使用Σ-Δ转换器—第二部分[中文版]
(pdf, 497 kB)
何时及如何使用Σ-Δ转换器:第一部分讨论续篇 |
应用笔记 | |
|
AN-389: Using Sigma-Delta Converters-Part 2
(pdf, 590 kB)
When to Use/How to Use Sigma-Delta ADCs; Continuation of Part 1 Discussion. |
应用笔记 | |
|
AN-388: 使用Σ-Δ转换器—第一部分[中文版]
(pdf, 0)
何时及如何使用Σ-Δ转换器 |
应用笔记 | |
|
AN-388: Using Sigma-Delta Converters-Part 1
(pdf, 590 kB)
When to Use/How to Use Sigma-Delta ADCs |
应用笔记 | |
| AN-311: 如何切实有效地保护CMOS电路不受电源过压影响 (pdf, 217 kB) | 应用笔记 | |
| AN-311: How to Reliably Protect CMOS Circuits Against Power Supply Overvoltaging (pdf, 217 kB) | 应用笔记 | |
|
AN-283: Σ-Δ型ADC和DAC[中文版]
(pdf, 677 kB)
Σ-Δ原理概述:利用Σ-Δ调制器、数字滤波和抽取进行过采样、噪声整形 |
应用笔记 | |
|
AN-283: Sigma-Delta ADCs and DACs
(pdf, 1699 kB)
Overview of Sigma-Delta Concepts: Oversampling, Noise Shaping Using the Sigma-Delta Modulator, Digital Filtering and Decimation. |
应用笔记 | |
| AN-202: IC放大器用户指南:去耦、接地及其他一些要点 (pdf, 0) | 应用笔记 | |
| AN-202: An IC Amplifier User’s Guide to Decoupling, Grounding, and Making Things Go Right for a Change (pdf, 76 kB) | 应用笔记 | |
| MS-2210: Designing Power Supplies for High Speed ADC (pdf, 327 kB) | 技术文章 | |
|
Delta-Sigma Rocks RF, As ADC Designers Jump On Jitter
(Electronic Design, 1/12/06) |
技术文章 | HTML |
| Circuit Suggestions Using Features and Functionality of New Sigma-Delta ADCs | 技术文章 | HTML |
|
Designing and Applying Remote Field Instruments
by Albert O' Grady and Jim Ryan, Analog Devices B.V. ...Good things can come in small packages because of on-chip capabilities (Control Engineering, September 1998) |
技术文章 | HTML |
|
Ask the Applications Engineer-27: What problems am I most likely to run into when instrumenting an industrial system?
(Analog Dialogue, Vol. 33, No. 2, February, 1999) |
《模拟对话》杂志 | HTML |
| Sigma Delta ADCs (< 15 kSPS) | 产品选型指南 | HTML |
| RAQs index | 非常见问题解答 | HTML |
| 术语表 | 专业词汇表 | HTML |
| 快讯名称 | 内容类型 | 文件类型 |
|---|---|---|
|
Σ-Δ型ADC指南
交互式图形工具,显示理想Σ-Δ型ADC的行为。 |
工具与转换 | HTML |
|
Σ-Δ寄存器配置助手
轻松设置Σ-Δ型ADC的配置寄存器。使用下拉菜单确定要载入寄存器的正确十六进制值,并且产生伪代码。 |
Design Calculators | HTML |
| AD7708 IBIS Model | IBIS 模型 | HTML |
原理图符号和PCB封装— Analog Devices offers Symbols & Footprints which are compatible with a large set of today’s CAD systems for broader and easier support.
Recommended Voltage References for the AD7708
Recommended Digital Isolators for the AD7708
Were these recommendations helpful?
样片申请及购买这里所列出的美国报价单仅供预算参考,指美元报价(规定订量的每片美元,美国离岸价),如有修改不再另行通知。由于地区关税、商业税、汇率及手续费原因,国际报价可能不同。对于特殊批量报价,请与您当地的ADI公司办事处或代理商联络。对于评估板和套件的报价是指一个单位价格。