AD9520/22 Configuration Tool
(zip)
This handy tool will automatically calculate divider values based on the user’s input/output frequencies, as well as assist with designing the loop filter based on the user’s parameters. Be sure to install the MATLAB® runtime installer first.
AD9520 Evaluation Software Installer
(zip)
Note: The USB driver requires 32-bit Windows XP (or a 32-bit Windows XP virtual machine).
However, the software can be run in standalone mode on newer versions of Windows.