content here.
content here.

Rarely Asked Questions...

A monthly column, "Rarely Asked Questions: Strange but true stories from the call logs of Analog Devices,"
is published monthly in EDN and Design News.

CAPACITIVE SENSORS: Rugged Enough for the Real World?

Q. I've seen cap sensors used in consumer electronics, but are they rugged enough to function in a harsh industrial environment?

CAPACITIVE SENSORS: Rugged Enough for the Real World?

A.  The answer is an emphatic yes! Capacitive sensors are already used for industrial precision measurement of pressure, proximity, position and liquid levels. Capacitive sensors are rapidly replacing switches, buttons, scroll bars and jog wheels as the preferred choice for human to machine interface in industrial and consumer applications.

Capacitive sensor IC's work essentially by detecting changes in an electric field between a set of pads. The electric field is generated by the capacitive sensor. Changes in the field are caused when an object passes through the field. The electric field fluctuations are proportional to changes in capacitance. A capacitance-to-digital converter (CDC) processes the change in capacitance and provides a digital output, which can then be connected to a microcontroller or other digital interface. Since the sensors have no moving mechanical parts, they are inherently more reliable than their earlier mechanical predecessors.

In rugged industrial applications that require a control device to tolerate sustained exposure to conditions such as wide swings in temperature, humidity, dirt, electrostatic discharge (ESD), accidental spills, or prolonged exposure to moisture, capacitive sensors excel. Capacitive sensors also provide the user with the ability to select the right "tactile feel" for control device in the industrial setting.

The capacitive sensor pads are covered by a thin layer of protective plastic. The pads are therefore impervious to dirt and liquid infiltration. The plastic thickness can vary depending on the application. For these situations the sensor can be tuned to compensate for variations in the plastic thickness. This is especially important in "wet" applications or where the sensor pad may be subjected to frequent exposure to liquids, moisture and cleansing agents. The protective plastic barrier also helps augment the sensors on-chip ESD protection.

In addition to being durable, capacitive sensors can be made to automatically adapt to their local environment. Some of the newer devices feature an Adaptive Environmental Compensation (AEC) algorithm, which continuously monitors the capacitance level of the sensor and compensates for any variations in ambient temperature, humidity and even degradation of the sensors dielectric material over time. The AEC helps ensure accurate and reliable operation no matter what the local environment is.

So, next time your design calls for a switch, button, scroll bar, jog wheel, or the need to make precision measurements, rest assured that there is a capacitive sensor that can handle the task. Capacitive sensors provide a smart and rugged alternative to traditional choices.

Download this article (pdf, 688,128 bytes) back to top

John Ardizzoni is an Application Engineer at Analog Devices in the High Speed Amplifier Group. John joined Analog Devices in 2002, and has over 27 years experience in the electronics industry. John Ardizzoni


For More Information:
Capacitance to Digital Converters Selection Table

Product Links:
Now the Shortest Distance Between a Capacitive Sensor and Digital Code Is a Single Chip: Capacitance-to-Digital Converter (CDC) Technology
Providing an Edge in Capacitive Sensor Applications
Using the AD7142 and a Capacitive Sensor to Develop a Single-Push Digital Shutter Button
AD7143 - Programmable Controller for Capacitance Touch Sensors
AD7142 - Programmable Controller for Capacitance Touch Sensors
AD7747 - 24-Bit Capacitance-to-Digital Converter with Temperature Sensor

Analog Dialogue:
Ask The Application Engineer—35: Capacitance Sensors for Human Interfaces to Electronic Equipment
Providing an Edge in Capacitive Sensor Applications

Online Seminar Library

Analog is everywhere

Useful Analog Devices Links:
Solutions Bulletin Library
Analog Devices Technical Bookstore
Sign up for Analog Devices eNewsletters

Analog Devices Homepage

back to top