Innovation Pushes State-of-the-Art in Voltage References

2017-09-18

Most system designers use voltage references in their circuits. While many will agree that the performance may ultimately be limited by the reference, they are often unclear as to why. With so many reference products available, designers often choose based on a tradeoff between price and precision, using only initial accuracy and TC specs as a measure of precision.

As applications have evolved, so have voltage references. Features such as noise, thermal stability, load and line regulation and size may be just as important as, or more important than, the more obvious precision specifications.

Three new products, the LT6654, LTC6655 and LT6656, have carefully chosen combinations of features and specifications to make them especially compatible with common types of applications.

This presentation gives details as to these features and introduces the products that are best suited for these types of system designs.

Innovation Pushes State-of-the-Art in Voltage References

2017-09-18
Most system designers use voltage references in their circuits. While many will agree that the performance may ultimately be limited by the reference, they are often unclear as to why. With so many reference products available, designers often choose based on a tradeoff between price and precision, using only initial accuracy and TC specs as a measure of precision.

As applications have evolved, so have voltage references. Features such as noise, thermal stability, load and line regulation and size may be just as important as, or more important than, the more obvious precision specifications.

Three new products, the LT6654, LTC6655 and LT6656, have carefully chosen combinations of features and specifications to make them especially compatible with common types of applications.

This presentation gives details as to these features and introduces the products that are best suited for these types of system designs.
Latest Media 12
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目