RAQs
It's easy to drive an EE to drink – but what drives one to poetry?
Q.  My SPICE simulation worked perfectly, but now I've a large production batch which
      doesn't meet its specification?

Circuit Simulation



A.  Analog circuit simulation is one of the most valuable tools that has emerged over the last two decades, and my company offers an impressive array of SPICE models to aid circuit designers. But simulation is not real life. SPICE models rarely emulate all the second- and third order effects which make analog circuit design so challenging.


It is critically important to build, and exhaustively test, hardware versions of your analog designs, not just run interminable simulations.


At high frequency, and with very high precision designs, it is even important to make the prototype as similar to the final production layout as is possible, because parasitic inductance and capacitance from the printed circuit board can have a substantial effect on HF performance and cause big differences between the simulation, the breadboard and the final production version.



 
Designs in their hundreds at Analog
hang in the air,
Ideas from the Valley, ideas from the
timid or bold,
Designs that are pearls and designs that
are rubbish are there,
And there with the rest are designs that
will never be old.
There's circuits from everywhere that
triple Es may reside,
And many to count are the abstract and
many of use,
And many that seem so attractive they
can't be denied,
But few that perform when you build 'em
and turn on the juice.
 
I wish one could know them, I wish there
were tokens to tell
Those fortunate circuits that work when
you turn on the power;
And then one could publish them freely
and not strike a knell
For our firm's reputation for circuit ideas
that inspire.
But now you may stare as you like but
you cannot devise
Infallible ways to ensure that success be
foretold;
They send to the ceiling the smoke of
untimely demise
Designs that will die on their breadboards
and never be old.

(With apologies to A. E. Houseman)
This is a parody of one of the poems (XXIII) in Houseman's "A Shropshire Lad."

Download this article (pdf, 126,976 bytes) back to top

James Bryant Offers Intrigue, Interest and Technological Troubleshooting Ideas... engineer, applications manager, philosopher, humorist, columnist and radio ham (G4CLF), only a man with such an eclectic dossier could make the often drab world of semiconductors come to life with such color and imagination. James Bryant


For More Information:

Analog Breadboarding


Useful Analog Devices Links:

Analog Dialogue

Webcasts from Analog Devices

Sign up for Analog Devices eNewsletters

Analog Devices Homepage

back to top

Send Feedback X
content here.
content here.

Send Feedback

Close