AD-PZSDR2400TDD-EB
Overview
Product Details
The AD-PZSDR2400TDD-EB is a 2.4GHz TDD analog module designed to work with the AD9361, a high performance, highly integrated RF transceiver intended for use in RF applications, such as 3G and 4G base station and test equipment applications, and software defined radios. The AD-PZSDR2400TDD-EB is affectionately dubbed the first 'RF personality card'. It plugs into the ADRV1CRR-FMC carrier card. 35mm U.FL coaxial cables connect the card to the ADRV9361-Z7035 SDR SOM providing access to the transmit and receive inputs of the AD9361. Information on the card, how to use it, the design package that surrounds it, and the software which can make it work, can be found on the wiki page.
The purpose of the AD-PZSDR2400TDD-EB is to provide the user with a path to condition the transmit or receive signals of the AD9361. Selection of TX or RX path is achieved by the 200MHz to 2.7GHz SPDT switch HMC546 controlled by the FPGA and accompanying software. The transmit path consists of a 2.4GHz filter, half watt driver amplifier ADL5324 and 2 watt power amplifier HMC921. The receive path consists of the same 2.4GHz filter as well as a low loss LNA HMC669.
Markets and Technologies
Applicable Parts
Package Contents
- AD-PZSDR2400TDD-EB
- 2 u.FL to u.FL cables
- 4 spacers
- 4 screws
- nuts
Getting Started
To start using the AD-PZSDR2400TDD-EB, you must have the ADRV1CRR-FMC carrier card along with the ADRV9361-Z7035 SDR SOM and some 35mm U.FL coaxial cables. Plug the AD-PZSDR2400TDD-EB onto the carrier, connect the UFL cables between the SOM and the 2400TDD board and you are ready to use the board.
Reference Board
Reference Board: AD-PZSDR2400TDD-EB
- Product Categories:
- RF / IF ICs
- Power Management
- Amplifiers
System Requirements
The AD-PZSDR2400TDD-EB board plugs into the ADRV1CRR-FMC carrier card, so that would be the requirement to be able to operate this board. The software needed is already built in the SD card that we provide with the ADRV9361-Z7035 SDR SOM.
Documentation & Resources
-
AD-PZSDR2400TDD-EB User Guide2/2/2016WIKI