How to Configure a Microcontroller for Deep Sleep Using the MAX32630

2022-10-04

In this video, Mohamed discusses some of the low-power modes available on the MAX32630 microcontroller. After outlining the capabilities and benefits of Deep Sleep mode for his smartwatch application, he demonstrates how to toggle the power mode with the push of a button. For more information on how to use the MAX32630 as a timekeeping circuit, watch the video, "How to Set Up an Ultra-Low Power Real-Time Clock II Using the MAX32630FTHR."

How to Configure a Microcontroller for Deep Sleep Using the MAX32630

2022-10-04

In this video, Mohamed discusses some of the low-power modes available on the MAX32630 microcontroller. After outlining the capabilities and benefits of Deep Sleep mode for his smartwatch application, he demonstrates how to toggle the power mode with the push of a button. For more information on how to use the MAX32630 as a timekeeping circuit, watch the video, "How to Set Up an Ultra-Low Power Real-Time Clock II Using the MAX32630FTHR."

Latest Media 12
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目