How to Use a Flyback Converter to Achieve Isolated Voltage Level Shifting

2022-10-04

Teja explains how to translate a single-ended voltage at the input to a bipolar voltage at the output using an isolated flyback converter. He goes over the importance of isolation in a circuit and the circuit elements that can be used for isolation. He finishes with a demonstration of how to use the MAXREFDES1141 and the MAXREFDES1132 to achieve isolated voltage-level shifting.


How to Use a Flyback Converter to Achieve Isolated Voltage Level Shifting

2022-10-04
Teja explains how to translate a single-ended voltage at the input to a bipolar voltage at the output using an isolated flyback converter. He goes over the importance of isolation in a circuit and the circuit elements that can be used for isolation. He finishes with a demonstration of how to use the MAXREFDES1141 and the MAXREFDES1132 to achieve isolated voltage-level shifting.


Latest Media 12
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目