I2C Quad Buck Regulator Packs Performance, Functionality, Versatility and Adaptability in a 3mm × 3mm QFN

Jan 1 2008

Figure 1

   

Introduction

The LTC3562 is an I2C quadruple step-down regulator composed of four extremely versatile monolithic buck converters. Two 600mA and two 400mA highly adjustable step-down regulators provide a total of 2A of available output current, all packed inside a 3mm × 3mm QFN package. All four regulators are 2.25MHz, constant-frequency, current mode switching buck converters whose output voltages and operating modes can be independently adjusted through I2C control. The 2.7V to 5.5V input voltage range makes it ideally suited for single Li-Ion battery-powered applications requiring multiple independent voltage supply rails.

I2C Programmable Operating Modes

All four LTC3562 step-down regulators have the unique ability to be programmed into four distinct op erating modes to satisfy the various noise/power demands of a variety of applications. These four modes are pulse skipping mode, Burst Mode operation, forced Burst Mode operation, and LDO mode.

Pulse skipping mode allows the regulator to skip pulses at light load currents, providing very low output voltage ripple while maintaining high efficiency. Burst Mode operation and forced Burst Mode operation deliver bursts of current to the buck output and regulate the output voltage through hysteretic control, giving the highest efficiency at low load currents. In LDO mode, the bucks are converted to DC linear regulators and deliver continuous power from the switch pins through the inductor, providing the lowest possible output noise as well as the lowest no-load quiescent current.

I2C Programmable Output Voltages

Another unique feature of the LTC3562 is its ability to adjust the output voltage of each regulator through I2C control. The chip contains two different flavors of output adjustable regulators. The Type A regulators (R600A, R400A) have programmable feedback servo voltages, while the Type B regulators (R600B, R400B) have directly programmable output voltages that do not need external programming resistors.

Table 1. Feature comparison of the LTC3562’s four integrated regulators (two 600mA and two 400mA)
R600A R400A R600B R400B
Type A A B B
Output Current 600mA 400mA 600mA 400mA
I2C Programmable Operating Modes Pulse Skip
Burst
Forced Burst
LDO
Pulse Skip
Burst
Forced Burst
LDO
Pulse Skip
Burst
Forced Burst
LDO
Pulse Skip
Burst
Forced Burst
LDO
Feedback Servo Voltage I2C Programmable
425mV–800mV
25mV steps
(16 settings)
I2C Programmable
425mV–800mV
25mV steps
(16 settings)
600mV (Fixed) 600mV (Fixed)
Output Voltage Adjustable using External Resistors Adjustable using External Resistors I2C Programmable
600mV–3.775V
25mV steps
(128 settings)
I2C Programmable
600mV–3.775V
25mV steps
(128 settings)
RUN Pins Yes Yes No No

The Type A regulators use external feedback resistors to set the output voltage based on a programmable feedback servo voltage. The feedback voltage values can be programmed from 800mV (full scale) down to 425mV in 25mV steps. This results in 16 possible feedback servo voltages, and thus 16 different output voltage settings for the same external programming resistors.

The Type B regulators (R600B, R400B) do not require external programming resistors at all because they are integrated inside the chip. These internal feedback resistors not only save valuable board space, they are also I2C programmable. The values of the internal feedback resistors can be adjusted through I2C control to directly program the regulator output voltages from 0.6V to 3.775V in 25mV increments. That is 128 possible output voltage settings for each Type B regulator.

RUN pins and Default Settings

I2C applications generally have a microprocessor in charge of the I2C communications between the various system blocks. A multi-channel buck converter such as the LTC3562 provides an excellent solution for efficiently stepping down the microprocessor’s core and I/O supply voltages from a higher input supply or battery. At the surface, using an I2C controllable voltage converter to generate the microprocessor’s power supplies seems to pose a bootstrap problem at system start-up. If the microprocessor initially has no power and thus there is no I2C control, what programs the LTC3562’s output to the proper voltage for the patiently waiting microprocessor?

The LTC3562 gets around this start-up issue by providing individual RUN pins for the two Type A regulators. These RUN pins bypass the I2C controls and enable the regulators if I2C is unavailable. When a RUN pin is used, the corresponding Type A regulator is enabled in a default setting, which is 800mV for the feedback voltage and pulse skipping mode for the operating mode. Once I2C becomes available to the system, these default settings can always be modified on the fly through I2C.

Pushbutton Control and Power Sequencing

Figure 1 shows an application circuit that uses the LTC3562 to power the core and I/O supplies of a system microprocessor. The RUN pin of R600A connects to a pushbutton circuit with a pull-up resistor used to power on the system. When the button is pushed, the RUN pin goes low which enables R600A to ramp up the power supply for the microprocessor’s core. The RUN pin of R400A is tied to R600A’s power-on-reset output signal (POR600A). Once R600A reaches regulation, POR600A goes high after a 230ms time delay, which would then enable R400A to power the I/O supply of the microprocessor.

Figure 1. The LTC3562 configured in a quad step-down converter with pushbutton control and power sequencing.

After both the core and I/O supplies are up, the microprocessor could then communicate back to the LTC3562 through I2C to program the part such that it keeps R600A enabled even after the pushbutton stimulus is removed. The microprocessor then can enable regulators R600B and R400B in any mode and program the output voltages to desired levels.

Figure 2. Efficiency of the 2.5V regulator.

Low Power Adaptability

The ability to change the operating modes and output voltages at any time allows the LTC3562 to adapt to the constantly changing demands of many high performance systems. An example of this adaptability would be during lower power standby operation in handheld battery-powered systems. When going into standby mode, the regulators can be programmed into Burst Mode operation or forced Burst Mode operation to maximize power efficiency at light loads. Under no-load conditions, the regulators can also be programmed into LDO mode, which provides the lowest quiescent current (all four regulators in LDO mode only draw a combined 80µA for the entire chip).

To save even more power, the LTC3562 can be programmed to reduce the regulators’ output voltages in Burst Mode operation or forced Burst Mode operation during light load conditions. Since power dissipation is directly proportional to the supply voltage multiplied by the load current, dropping the supply voltage effectively reduces the circuit’s total power dissipation. If the output load is resistive in nature, reducing the supply voltages has an even greater effect, since power dissipation in the load is proportional to the supply voltage squared.

Conclusion

The LTC3562 is a highly flexible I2C quad step-down converter composed of two 600mA and two 400mA buck regulators in a 3mm × 3mm QFN package. The output voltages of the regulators can be switched on the fly using servo control or I2C control. Each regulator can also be switched on the fly into four possible high efficiency or low-noise operating modes. This is a perfect device for high performance applications that require constant control of the power supply. It can also be used to simplify design, build and test cycles, since output voltages can easily be changed without changing components.

About the Authors

Joe Panganiban

Related to this Article

Products

Product Categories

Latest Media 21

Subtitle
Learn More