EMC Testing in Motion Control IC

Jan 31 2020

Abstract

Industrial motion control applications include many sources of noise. EMI can reduce reliability and accuracy in these circuits. Analog has designed an optimized solution for reliable communication and signaling in these harsh environments.

Introduction

EMI can dramatically reduce reliability and affect the performance of motion control systems. Industrial applications need to further be protected against high-voltage, potentially destructive events that can occur on production floors or in harsh environments. Some of these events include electrostatic discharge (ESD) and surge transients.

This application note describes electromagnetic compatibility (EMC) tests, including IEC 61000-4-2 ESD, IEC 61000-4-4 EFT, and IEC 61000-4-5 Surge, done on a high-speed isolated RS-485 data link using the MAX14435 and MAX22445 digital isolators and MAX22500E RS-485 transceiver. The schematic and layout files are available for this solution; however, Analog is not selling assembled boards.

Motion Control Concerns in an Industrial Environment

Digital motion control applications typically include power, a controller, isolation, and a digital interface to connect to a motor or actuator. RS-485 signaling meets the physical layer (PHY) requirements of many commonly used encoder interface standards (e.g., EnDat or SSI) and inherently minimizes many EMI issues associated with communication in motion control applications. As such, RS-485 signals are often used to interface between the controller and downstream devices in motion control applications.

RS-485 transceivers are often optimized for robust communication in difficult environments. However, other low-power digital circuitry may be destroyed by the high-voltage and large switching current signals that may couple-in down the line. Digital and power isolation are often used to further protect sensitive digital circuitry from potentially damaging voltages/signals.

System Overview

The setup includes three major hardware blocks, as seen in Figure 1:

  • Power

    • Power for the digital interface/logic side of the digital isolator
    • Isolated power for the RS-485 transceiver/field-side of the digital isolator interface
  • Isolated digital interface
  • RS-485 line interface

Isolated power for the RS-485 Block Diagram.

Figure 1. Block diagram.

Figure 2 shows a picture of the test board.

Picture of a Motion Control test board.

Figure 2. Analog solution test board.

The test board has three isolated grounds (see Figure 2 in red):

  1. Logic ground
  2. Field ground
  3. Protective earth

Three Analog ICs are used for the power domain (see Figure 2 in brown):

  1. MAX17651 to generate 5V for the logic side
  2. MAX13256 transformer driver
  3. MAX16904 to generate 5V for the field side

Isolation and high-voltage protection are provided by the following devices (see Figure 2 in blue):

  1. MAX14435/MAX22445 isolator
  2. TVS diodes, Semtech® RClamp1224S.TCT
  3. 220pF Y-capacitor
  4. Two 3300pF Y-capacitors in series

Power

Assuming a readily available 24V supply, the Analog solution includes two on-board power supplies for the digital interface.

The MAX17651 low-drop linear regulator generates a 5V supply for the logic side of the on-board digital isolation circuitry.

The MAX13256 H-bridge transformer driver and MAX16904 mini buck converter are used to generate an isolated 5V for the MAX22500E high-speed RS-485 transceiver and the field-side of the digital isolator. The transformer driven by the MAX13256 provides up to 5kVRMS isolation between the 24V source and the isolated/field side of the board. The MAX16904 is used to efficiently step down the 24V voltage to 5V to reduce power dissipation during high-speed communications.

Digital Isolation

Analog 's solution uses a digital isolator to interface between the MAX22500E RS-485 transceiver and the digital signal generator. The digital input (DI) and receiver output (RO) signals of the RS-485 transceiver are routed through the digital isolator to the digital signal generator and analyzer. Both signals include a 50O termination to match the input and output of the signal generators.

Two pin-compatible Analog  digital isolators were tested in this circuit: the MAX14435 (basic isolation) and the MAX22445 (reinforced isolation).

RS-485 Line Interface

The MAX22500E RS-485 transceiver operates with data rates up to 100Mbps and is optimized for high-EMC motion control applications. Integrated preemphasis improves signal integrity at high data rates over long distances. Additionally, the MAX22500E features a 250mV (typ) wide receiver hysteresis to improve noise rejection.

The ground planes under the A and B lines are pulled away to reduce stray capacitance and improve the signal at maximum speed.

Semtech RClamp1224S low-capacitance TVS diodes feature a maximum junction capacitance of 3pF (max, at 1MHz) and protect the transceiver from being destroyed during high-voltage events.

Isolation

The test board features three isolated ground planes to protect the MAX22500E and digital circuitry during high-voltage events: a logic ground, field ground, and protective earth (PE) ground. High-voltage Y-capacitors and high-impedance resistors are used to connect these grounds to provide a return current path for the high-voltage transients and reduce stray switching currents and EMI that may be generated at the isolation boundaries. Analog recommends placing the on-board TVS diodes (RClamp1224S) close to the RS-485 connector and creating a dedicated field-side ground path from the TVS diodes to the 220pF Y-capacitor to direct EFT burst energy to the PE without interfering with the rest of the field-side circuitry including the MAX22500E and the digital isolator.

System Testing

System Setup

Figures 3 and 4 show the test setup for the ESD, surge, and EFT/burst tests. Data was generated by the Tektronix® GB700T signal generator connected to a transmitter (Tx) board at data rates up to 100Mbps with the MAX22500E preemphasis enabled. Data was received by a receiver (Rx) board connected to the Tektronix GB700R signal analyzer for analysis. Although both the Tx and Rx boards are configured for half-duplex communication, data was passed from the Tx board to the Rx board only during testing.

As seen in the figures, cable shields were connected to the PE ground on each board and wide copper tape is used to connect the PE and cable shield to the metal plane.

Motion Control Testing Setup.

Figure 3. Test setup.

Layout of Motion Control Testing Setup.

Figure 4. Test setup; Tx and Rx boards.

A Haefely® ECOMPACT4 compact transient immunity tester was used for surge and EFT/burst testing. A Teseq® CDN 3425 capacitive clamp and CDN 117 data line coupling-decoupling network were used for EFT (burst) and surge tests.

A Teseq NSG 438 ESD simulator was used for ESD testing.

Table 2 shows a complete list of equipment used for testing.

Table 2. Test Equipment
Test Equipment Part Number Used to Test
Power Supply HP E3620A ESD, surge, EFT/burst
PRBS Signal Generator Tektronix GB700T Surge, EFT/burst
PRBS Signal Analyzer Tektronix GB700R Surge, EFT/burst
Oscilloscope Tektronix DPO7254 EFT/burst
Surge/Burst Generator Haefely ECOMPACT4 Surge, EFT/burst
Capacitive Coupling Clamp Teseq CDN 3425 EFT/burst
Coupling-Decoupling Network Teseq CDN 117 Surge
ESD Generator/Simulator Teseq NSG 438 ESD
All tests and measurements were taken at room temperature (TA = +25°C).

Test Results

MAX22500E Transceiver Performance During Normal Operation

The MAX22500E half-duplex RS-485 transceiver is optimized for high-speed (up to 100Mbps) operation over long distances. Integrated preemphasis functionality helps to reduce intersymbol interference (ISI) over long cables and increase signal integrity. Preemphasis reduces ISI by boosting the differential signal amplitude at every transition edge, counteracting the high-frequency attenuation of the cable.

Eye diagrams can be used to evaluate the quality of a transmitted signal. Eye diagram measurements were taken at the Rx board. A Cat6 cable (50m) was used to connect the Tx board and the Rx board, and PRBS data was sent at 100Mbps from the Tx board to the Rx board during testing. Data was measured differentially with 100O termination resistors at both ends of the cable. Measurements were done with preemphasis disabled (Figure 5) and preemphasis enabled (Figure 6).

Eye diagram (VA-VB) at the Rx board, 100Mbps, preemphasis disabled.

Figure 5. Eye diagram (VA-VB) at the Rx board, 100Mbps, preemphasis disabled.

Eye diagram (VA-VB) at the Rx board, 100Mbps, preemphasis enabled.

Figure 6. Eye diagram (VA-VB) at the Rx board, 100Mbps, preemphasis enabled.

As seen in Figure 5 and Figure 6, the eye height is reduced, and jitter is increased when preemphasis is disabled. Jitter of 29% of the bit time was measured when preemphasis was disabled. Enabling preemphasis improved the signal, reducing jitter measurements to 20% of the bit time.

Signal measurements were measured at 100Mbps for cable lengths (Cat6) up to 50m with no errors (with a bit-error rate (BER) < 1E-10).

Contact and Air-Gap ESD per IEC 61000-4-2

Line-to-earth Contact and Air-Gap ESD were tested on both the Tx and Rx boards. These boards were connected with a 20m Cat6 cable, and data was passed from the Tx board to the Rx board at 100Mbps with preemphasis enabled. ESD transients were applied directly to the A and B I/O pins on both Tx and Rx boards, and the ESD ground return was connected to the PE at the Tx board. Figure 7 shows a block diagram of the test circuit used to test the ESD performance of the Analog solution. A BER < 1E-8 was required during the test to consider the result as a pass (performance criterion A). A BER > 1E-8, or device damage or reset during a pulse, was registered as a fail.

Test results are shown in Table 3.

ESD test block diagram.

Figure 7. ESD test block diagram.

Table 3. ESD Test Results
Analog Isolator Used in Testing ±6kV Contact Discharge ±8kV Air-Gap Discharge
MAX14435 Pass Pass
MAX22445 Pass Pass

EFT/Burst per IEC 61000-4-4

Electrical fast transient (EFT), or burst, testing was done using the Haefley high-voltage EFT generator and a large capacitive coupling clamp. The generator is connected directly to the clamp and set to generate high-voltage bursts for a given duration and repetition rate as defined by IEC 61000-4-4. The 20m Cat6 cable used to connect the Tx and Rx board was placed inside the clamp. The clamp was placed nearest the Rx board, with only ~1m of cable between it and the Rx board. Figure 8 shows a block diagram of the test circuit used to test the EFT performance of the Analog solution. Pseudorandom bit sequences (PRBS) at 100Mbps were sent from the Tx board to the Rx board during testing. A BER < 1E-8 was required during the test to consider the result as a pass (performance criterion A). A BER > 1E-8, or device damage or reset during a pulse, was registered as a fail.

Test results for the Analog solution are shown in Table 4.

EFT test block diagram.

Figure 8. EFT test block diagram.

Table 4. EFT Test Results
Analog Isolator Used in Testing ±3kV
MAX14435 Pass
MAX22445 Pass

Surge per IEC 61000-4-5

Line-to-earth surge testing was done using the Haefley high-voltage surge generator and its companion 42?/0.5µF CDN network. The generator outputs were connected directly to the CDN network. The Line+ from the CDN networks was connected to the A and B I/O pins at both the Tx board and the Rx board, and the Line- from the CDN network was connected to the PE at the Tx board. PRBS at 100Mbps was sent from the Tx board to the Rx board during testing.

Figure 9 shows a block diagram of the test circuit used to test the surge performance of the Analog solution. A BER < 1E-8 was required during normal operation to consider the result as a pass, although a BER > 1E-8 was allowed during surges (performance criterion B). Device damage or reset during a pulse was registered as a fail.

Test results for the Analog solution are shown in Table 5.

Surge testing block diagram.

Figure 9. Surge testing block diagram.

Table 5. Surge Test Results
Analog Isolator Used in Testing ±2kV
MAX14435 Pass
MAX22445 Pass

Conclusion

Each IEC 61000-4 standard defines a standard test level for compliance with defined voltage/current levels associated with each test. Analog's high-speed RS-485 communication link circuit, optimized for robust communication in harsh industrial environments, was tested in compliance with the IEC 61000-4-2 (ESD), IEC 61000-4-4 (EFT), and IEC 61000-4-5 (Surge) standards. Table 6 shows the level of protection verified during this testing.

The Analog circuit provides Level 3 protection for ESD and EFT with continued communication during the tests (performance criteria A, as outlined in the IEC standards).

The Analog circuit provides Level 4 protection during surge events. Communication is temporarily lost during a surge event, but the circuit is not damaged and communication resumes when surge event ends (performance criteria A, as outlined in the IEC standards).

Table 6. Electromagnetic Compatibility Immunity
Standard Description Test Results Test Level Performance Criteria
IEC 61000-4-2 Electrostatic Discharge ±6kV Contact Discharge;
±8kV Air Gap Discharge
3 A
IEC 61000-4-4 Electrical Fast Transient/Burst ±3kV inputs/outputs 4 A
IEC 61000-4-5 Surge ±±2kV signal/control ports to earth 3 B

Design Files

While Analog does not sell the Analog solution board, design files (schematic, layout, and BOM) can be downloaded.



Related to this Article

Product Categories

Latest Media 21

Subtitle
Learn More