Abstract
No switch-mode power supply is perfectly accurate. There are different tolerances that influence the precision of the output voltage regulation. This article explains the different sources of inaccuracy and shows how the total tolerance range is established.
Introduction
Switch-mode power supplies have a feedback pin with which an output voltage can be set. This voltage is regulated by the power supply circuit. However, the question arises as to how precisely the voltage is regulated.
Figure 1 shows a switch-mode power supply according to the step-down principle.
An existing, usually unregulated, supply voltage (input voltage) is used to generate an output voltage, which is regulated as accurately as possible.
The accuracy of the output voltage is determined by several influences and tolerances.
DC Tolerance
The DC regulation deviation includes the accuracy of the reference voltage contained in the voltage converter (Figure 1). This has been created by the designer of the integrated circuit in such a way that only minor deviations occur within the supply voltage range, the manufacturing tolerances of the IC, and the operating temperature. The existing tolerance is included in the data sheets of the voltage converter ICs. This value can be specified in different ways. It can be communicated as reference voltage line regulation, as output voltage load regulation, and as regulated feedback voltage. In addition to the accuracy of the pure reference voltage, the latter also includes other IC-specific DC tolerances at the feedback pin.
The DC tolerance also includes the deviation of the resistance values of the resistor divider between the regulated output voltage and the feedback pin (Rfb1 and Rfb2 in Figure 1). These resistors can be purchased with different tolerance ranges. Usually, a resistor has a resistance value close to the maximum specified tolerance. Better resistors, with a smaller tolerance, are detected during manufacturing of these resistors and are typically sold as more accurate resistors.
Output Voltage Ripple
The regulated output voltage always has a certain voltage ripple in a switch-mode power supply. This ripple is determined by the rise and fall of the inductor current of a buck regulator and the value of the output capacitor and its equivalent series resistance (ESR). The voltage ripple can be reduced by a high inductance value of the coil and a large output capacitor with a low ESR, but the output voltage ripple cannot be completely prevented in a switch-mode power supply.
Load Transients
The third influence on the accuracy of the generated voltage is the behavior during load transients. If the load current changes, the voltage generated may deviate upward or downward. The higher the amplitude of the load transient and the faster it occurs, the greater the short-term deviation of the output voltage from the set point.
To keep this influence on the error of the generated voltage as low as possible, the control loop speed must be fast. One tool that optimizes a power converter circuit loop is LTpowerCAD® from Analog Devices.
Figure 2 shows the load transient of the LT8642S. The load current is increased from 100 mA to 5 A within 500 ns and scorched again after 250 μs. The voltage peak is about 27.5 mV and the voltage dip is about 26.4 mV.
The measurement of the load transients was carried out with an LTpowerAnalyzer from Analog Devices. With this hardware, load transients can be measured easily for different current levels and with different transition times.
Figure 3 shows the different available influences on the tolerance of a switch-mode power supply.
Conclusion
When selecting a power supply circuit, it is essential to determine what voltage accuracy is required in an application. This is necessary to select the different components such as the power converter IC and resistor divider for DC accuracy, as well as the coil and output capacitor for the output voltage ripple and the load transient influences. Finally, the control loop of the circuit is optimized to handle load transients as well as possible; for example, with the lowest possible voltage offset.