ADXL367: Nanopower 3-Axis Digital MEMS Accelerometer

The ADXL367 is an ultra low power, 3-axis microelectromechanical systems (MEMS) accelerometer that consumes only 0.89 μA at a 100 Hz output data rate and 180 nA when in motion-triggered wake-up mode. Unlike accelerometers that use power duty cycling to achieve low power consumption, the ADXL367 does not alias input signals by under sampling, but samples the full bandwidth of the sensor at all data rates.​