signals header
Phased array radar against a vibrant sunset sky with mountains.
Phased array radar against a vibrant sunset sky with mountains.

SIGNALS+ 在线快讯订阅

持续关注Signals+,了解有关连接、数字健康、电气化和智能工业的最新见解、信息和想法并加以利用。

点击“订阅”,即表示您同意接收来自Analog Devices, Inc.及其子公司的邮件,并同意我们的隐私政策。设置您的隐私.

谢谢您的订阅,请查看您的邮箱确认邮件并完成注册.

您将实时接收突破性技术如何在全球范围内产生深远影响!

关闭
Head shot of mof Machael Gurr the author of the article
Michael Gurr,

Principal Engineer,
Product Marketing
ADEF & Communications

Analog Devices

作者详情
Michael Gurr
Michael Gurr是ADI公司航空航天和防务事业部的产品线工程师。他于2018年加入ADI公司,先后担任多个RF设计和管理职位。在此之前,他在Raytheon的GaN和GaAs放大器开发部门担任多个职位。他于2013年获得波士顿大学电气工程学士学位,2016年获得东北大学电气工程硕士学位,2021年获得马萨诸塞大学安姆斯特分校工商管理硕士学位。
关闭详情

DEMOCRATIZING PHASED ARRAY: WHY THE FUTURE DEPENDS ON PLATFORMS, NOT JUST PERFORMANCE

October 21, 2026


KEY TAKEAWAYS

  • Phased array deployment speed now matters as much as sensing performance.
  • Ground-up phased array integration forces teams to repeatedly solve the same problems.
  • Modular antenna-to-bits platforms like ADSY2301 turn custom builds into reusable building blocks.
  • Platform architectures will democratize advanced sensing for a broader community of innovators.


Growing demand for connectivity, autonomous systems, satellite communications, and real-time sensing is driving renewed interest in phased array architectures.

For more than half a century, phased arrays have powered some of the world’s most advanced radar, communications, and sensing systems, helping forecast severe weather, connect people and devices, and manage increasingly crowded RF environments. Yet despite their proven capabilities, many organizations still view them as too complex, costly, or specialized to deploy at scale.

This model of exclusivity is increasingly at odds with today’s market demands.

Organizations across industries are under pressure to deploy new capabilities faster, scale them more efficiently, and respond to constantly changing operating environments. As sensing and connectivity become critical to everything from infrastructure and transportation to communications and public safety, the ability to move from concept to deployment quickly is becoming as important as performance itself.

A new generation of modular antenna-to-bits platforms is beginning to emerge. Solutions such as ADI’s ADSY2301 demonstrate how capabilities that once required years of custom integration can increasingly be delivered as reusable building blocks, enabling organizations to focus more on applications and less on infrastructure.

“Just as standardized computing platforms democratized computing, modular phased array and antenna-to-bits architectures are poised to democratize advanced sensing across industries that increasingly depend on real-time awareness.”

A NEW ERA OF SENSING DEMANDS A NEW MODEL

For decades, phased arrays delivered exceptional performance in applications where precision mattered most. But achieving that performance often required significant expertise, custom engineering, and years of development, limiting adoption beyond a relatively small group of organizations.

Today, organizations are being asked to deploy sensing and communications capabilities faster than ever, but they cannot afford to wait years for custom development and deployment. To unlock the full value of phased arrays, the industry must make advanced sensing capabilities faster to deploy and more accessible across commercial and industrial markets.

From responding to severe weather and expanding satellite connectivity to managing crowded spectrum, or supporting critical infrastructure, the value of a system is increasingly tied not only to its performance but also to how quickly it can move from concept to deployment. In today’s world, speed-to-market is not just a “nice to have” but a competitive advantage.

WHAT ARE PHASED ARRAYS AND WHY DO THEY MATTER?

A phased array is a group of antennas that electronically steer radio frequency beams without moving mechanical components. Here are some real-world applications and their impact on humanity.

Technology Capability Outcome
Weather Forecasting Advanced radar sensing Earlier warning of severe storms
Communications Electronically steered antennas More reliable connectivity and broader coverage
Transportation/Collision Avoidance Enhanced situational awareness Improved safety and operational efficiency
Spectrum Management Dynamic resource allocation More efficient use of wireless networks
Threat Detection Multibeam generation Better airspace management

INNOVATION IS SLOWING AT THE INTEGRATION LAYER

Phased array engineers must simultaneously balance performance, power consumption, thermal management, size, cost, manufacturability, and scalability. But improving one attribute can often create trade-offs elsewhere. Higher beamforming performance can increase power requirements. Greater integration may create thermal challenges. Tighter specifications can drive development costs significantly higher.

Also, organizations are often forced to integrate numerous subsystems from the ground up, including RF front ends, beamformers, transceivers, data converters, power management technologies, and signal processing capabilities. While the components themselves may exist, the architectural challenge is substantial. As a result, engineering teams repeatedly solve the same integration problems program after program, extending development cycles and increasing risk.

The industry is approaching a similar inflection point. Just as standardized computing platforms made computing more practical and scalable, the next wave of phased array innovation will depend on simplifying integration and accelerating deployment. As advances in packaging and system-level design pack more capability into smaller, more efficient solutions, managing complexity has become one of the industry’s greatest challenges.

WHY PLATFORM-BASED PHASED ARRAYS MATTER

The future of phased arrays depends on more than advances in individual components. It requires architectures that simplify development, reduce risk, and accelerate deployment. Antenna-to-bits platforms enable engineers to optimize the entire signal chain as a unified system, helping shorten development cycles and create a clearer path from concept to deployment.

Technologies such as digital twin modeling, hybrid beamforming, and scalable manufacturing further streamline development while maintaining performance and controlling costs. Organizations can start small, validate designs quickly, and scale with confidence using a common architectural foundation. The result is a shift from designing individual components to building repeatable platforms that enable faster innovation and broader adoption.

SPECIALIZED TECHNOLOGY TO BROAD IMPACT

As modular, platform-based approaches lower barriers to adoption, advanced sensing capabilities will reach far beyond the traditional RF community. From earlier warning of severe storms to more reliable communications and faster operational decision-making, phased array systems can help industries respond to changing conditions with greater intelligence, agility, and efficiency.

The significance of this transition extends beyond any individual product or application. Platforms such as ADSY2301 offer an early glimpse of what becomes possible when antenna design, RF processing, and digitization are treated as a unified architectural foundation rather than a collection of discrete subsystems. As these approaches mature, advanced sensing capabilities are likely to become accessible to a much broader community of innovators.

Ultimately, no single company can drive this transformation alone. By working together across the technology ecosystem, organizations can make advanced sensing more accessible, helping more industries innovate, adapt, and make better decisions in real time.

 

Two people analyze weather data on a wall of monitors.