How to Set Up Bidirectional DC Powerline Communication Using the MAX20340

2022-10-04

MAX20340 implements a novel variation of bi-directional DC powerline communication interface that is ideal for use in applications where space is limited. Arun will demonstrate how to configure the powerline communication using the MAX20340EVKIT and use it to properly configure a charger.

How to Set Up Bidirectional DC Powerline Communication Using the MAX20340

2022-10-04
MAX20340 implements a novel variation of bi-directional DC powerline communication interface that is ideal for use in applications where space is limited. Arun will demonstrate how to configure the powerline communication using the MAX20340EVKIT and use it to properly configure a charger.
Latest Media 12
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目