Introduction to the MAX41460-64 300-960MHz sub-GHz Transmitter

2022-10-04

This video provides an introduction to the MAX41460 using a SPI programming interface while the MAX41461 thru MAX41464 parts feature an I2C interface as well as preset modes (pin-selectable output frequencies using only one crystal frequency)

Introduction to the MAX41460-64 300-960MHz sub-GHz Transmitter

2022-10-04
This video provides an introduction to the MAX41460 using a SPI programming interface while the MAX41461 thru MAX41464 parts feature an I2C interface as well as preset modes (pin-selectable output frequencies using only one crystal frequency)
Latest Media 12
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目