SIMO Technology Overview using the MAX77650 PMIC
2022年10月04日
Learn how SIMO technology simplifies design of low power systems such as the Smart Sock baby monitor. You’ll see how the MAX77650 PMIC uses the single-inductor/multiple-output (SIMO) power architecture to supply all the rails needed for low-power systems while maintaining high system efficiency in a total solution size under 20mm2. Watch as Gaurav demonstrates how easy it is to go from prototype to working design using the MAX32620FTHR development platform and the MAX44000 proximity sensor.
SIMO Technology Overview using the MAX77650 PMIC
2022年10月04日
Learn how SIMO technology simplifies design of low power systems such as the Smart Sock baby monitor. You’ll see how the MAX77650 PMIC uses the single-inductor/multiple-output (SIMO) power architecture to supply all the rails needed for low-power systems while maintaining high system efficiency in a total solution size under 20mm2. Watch as Gaurav demonstrates how easy it is to go from prototype to working design using the MAX32620FTHR development platform and the MAX44000 proximity sensor.
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}