Abstract
Many of the Company's microcontrollers integrate controllers for LCD displays, which are implemented in hardware. Some microcontrollers like the DS89C450 do not offer this functionality, but one can implement a simple display controller in software. This application note describes how to drive a static LCD panel with 7-segment digits using the DS89C450 ultra-high-speed flash microcontroller.
Overview
Liquid crystal display (LCD) panels are used in a variety of modern electronic equipment like calculators, handheld blood glucose meters, gas station pumps, and television sets. Because of their lower power consumption and easy viewing in direct light, LCDs have replaced older LED displays in many applications. A range of microcontrollers (such as the MAXQ2000) integrate LCD controllers capable of driving LCD panels at up to a ¼-muxed duty cycle. But in some instances, the ideal microcontroller for a particular application may not integrate an LCD controller. For these situations it is possible to implement a display controller in software by using the microcontroller's port pins to drive the display.
This application note describes how to implement a display controller for a simple, static LCD panel with
Example code for this application note is available for download (ASM).
Selecting an LCD Panel
When selecting an LCD panel for an application, take care to match the LCD with a compatible microcontroller or LCD display controller. The following questions should be considered when making this decision.
- What is the operating voltage range for the LCD? Since the DS89C450 is a 5V microcontroller and its port pins operate at 5V levels, we must select a 5V LCD panel. Note that many microcontrollers which integrate LCD controllers use a dedicated supply input (VLCD) to set the voltage range used by that LCD controller.
- What is the LCD's duty cycle? Static LCD panels connect each segment in the display to a dedicated drive line. This means that the number of segment drivers must equal the number of LCD segments to be driven. Multiplexed LCD panels, however, drive more than one LCD segment with each segment drive line (SEG). These panels use multiple common backplane (COM) outputs and drive multiple levels between VLCD and GND on the SEG and COM lines, depending on the duty cycle being used. Because the DS89C450, our example 8051 microcontroller, can only drive its port pin lines to 5V and GND, our example is limited to a static LCD. For additional information on driving a multiplexed LCD, refer to the following documents:
- Application note 3548, "Using an LCD with MAXQ Microcontrollers"
- The MAXQ® Family User Guide: MAXQ2000 Supplement
- How many segment and common drivers are required to operate the LCD panel? When controlling a static LCD panel, one drive line (port pin) is needed for each segment to be driven, plus an additional port pin for the common (COM) backplane line.
Figure 1. Seven-segment LCD display digit.
The LCD-S401C52TR display has a single COM backplane (connected to two pins) and 32 display segments, each connected to a segment drive pin. For this example, we will only use three of the 7-segment digits, which means that the DS89C450 will need to drive 21 SEG lines (seven segments for each of the three digits) and one COM line, thus requiring a total of 22 port pins. When not operating in the expanded memory bus configuration, the DS89C450 provides 24 push-pull port pins. The mircocontroller, therefore, has sufficient I/O capacity for this task. (An additional eight port pins are available on Port 0. However, these pins are open-drain and require additional pullup resistors to be usable as general-purpose I/O).
Hardware Setup
The hardware setup for this example was based on the DS89C450 Evaluation (EV) Kit (Rev B) with the memory interface CPLD (U5) and both external memory chips (U6 and U7) removed. This modification frees a number of additional port pins for use by our application, pins that would otherwise be used to implement the expanded memory bus, specifically Port 0 (all eight lines), Port 2 (all eight lines), Ports 3.6 and 3.7. See Table 1. (Note: Port 0 is not used in this example application.) The DS89C450 includes 64kB of internal code space and 1kB of internal data SRAM, which will be more than sufficient for this example.
The segment and common lines on the LCD-S401C52TR display were connected to port pins on the DS89C450 by using the J4 header adjacent to the prototyping area. The segment lines were connected to the port pins through 1kΩ resistors instead of being connected to the port pins directly. This latter step was done because the DS89C450's port pins have higher drive capacity (strong pulldown for the 0 state and a one-shot, strong pullup followed by a weak pullup for the 1 state) than would normally be used by LCD panel drive lines. Because the COM line has a larger capacitance and requires a stronger driver, it was connected to its port pin directly. This application does not, however, recommend that the segment lines be driven directly by port pins. A problem occurs in that configuration: the capacitive coupling through the LCD display between the segment and common planes tends to pull the COM line away from its intended state as more and more segments turn on. (This problem happens because an active segment will always be the opposite voltage from the common plane.) As a result, segments which should be off, turn partially on. So connecting the port pins through the resistors to reduce their drive strength eliminates this issue.
Table 1. LCD Panel and Port Pin Connections
DS89C450 Port Pin | J4 Header Pin | LCD Pin(s) | LCD Signal | Notes |
P1.0 | 1 | 21 | 4A | Through 1kΩ |
P1.1 | 2 | 20 | 4B | Through 1kΩ |
P1.2 | 3 | 19 | 4C | Through 1kΩ |
P1.3 | 4 | 18 | 4D | Through 1kΩ |
P1.4 | 5 | 17 | 4E | Through 1kΩ |
P1.5 | 6 | 22 | 4F | Through 1kΩ |
P1.6 | 7 | 23 | 4G | Through 1kΩ |
P1.7 | 8 | 1, 40 | COM | Connect directly |
P2.0 | 21 | 25 | 3A | Through 1kΩ |
P2.1 | 22 | 24 | 3B | Through 1kΩ |
P2.2 | 23 | 15 | 3C | Through 1kΩ |
P2.3 | 24 | 14 | 3D | Through 1kΩ |
P2.4 | 25 | 13 | 3E | Through 1kΩ |
P2.5 | 26 | 26 | 3F | Through 1kΩ |
P2.6 | 27 | 27 | 3G | Through 1kΩ |
P3.0 | 10 | 30 | 2A | Through 1kΩ |
P3.1 | 11 | 29 | 2B | Through 1kΩ |
P3.2 | 12 | 11 | 2C | Through 1kΩ |
P3.3 | 13 | 10 | 2D | Through 1kΩ |
P3.4 | 14 | 9 | 2E | Through 1kΩ |
P3.5 | 15 | 31 | 2F | Through 1kΩ |
P3.6 | 16 | 32 | 2G | Through 1kΩ |
There are a few additional items to note about the hardware setup:
- A standard 16.384MHz crystal (inserted at Y1) was used to provide the clock for the DS89C450.
- When running the application, DIP switches SW1.1 and SW4.2 should be ON; all others should be OFF.
- When loading the application (using the MAXQ Microcontroller Tool Kit (MTK) or another development tool), DIP switches SW1.1, SW1.2, SW1.3, SW4.1, and SW4.2 should be ON; all others should be OFF.
- When the LCD display is running, activity from Port 1 will also be seen on the LED bar-graph display, U10. This is normal and, since the LCD display is buffered, does not affect the application.
- P3.0 and P3.1 are also used for the Tx/Rx lines of serial-port 0. Therefore, when the application is loading (using the serial-port bootloader), one or two segments on the LCD can flicker due to activity on these lines. This is normal. When the application is running, DIP switches SW1.2 and SW1.3 should be turned off to disable the serial-port function.
- Any unused segments on the LCD display should be driven explicitly to the OFF state and not allowed to float. This task can be done either by connecting one or more unused segments to a port pin that is driven to the OFF state (the same voltage waveform as COM), or by connecting unused segments to COM directly.
Driving LCD Segments
The default state of LCD segments is OFF (i.e., clear); when no voltage is applied, the segments become transparent and are invisible against the background in the LCD panel. In addition, when the same voltage is applied to both a segment line (SEG) and the common backplane (COM), the segment remains off. The segment will only switch to its ON (i.e., opaque) state when a voltage difference is applied between the SEG pin for that segment and the COM plane. As this voltage passes a particular level, known as the threshold voltage, the segment darkens and finally becomes completely opaque. The threshold voltage, which is a percentage of the specified operating voltage of the LCD panel, varies from one LCD to the next.
The polarity of the voltage differential does not matter for driving the LCD segments. A controller, for example, that drives an LCD with a 3V threshold voltage can switch on segment n either by setting COM to ground and SEGn to 3V, or by setting COM to 3V and SEGn to ground. This fact is important because, if a static DC voltage is left across an LCD segment for a long period of time, the segment can become damaged and will no longer switch properly. To avoid this problem, LCD segments are always driven with alternating waveforms to ensure that the overall DC voltage across each segment is always zero, whether the segment is in the ON or OFF state (Figure 2).
Figure 2. Alternating drive waveforms for static LCD segments.
As Figure 2 shows, the COM pin on a static display is constantly driven by a 50% duty cycle square wave between VLCD (5V for our setup) and GND. Each segment line is then driven by one of two patterns.
- To switch the segment OFF, it should be driven by a waveform identical to the one used to drive the COM pin. This will ensure that the DC voltage across the SEG/COM pair is always zero, which means that the segment will remain off.
- To switch the segment to ON, it should be driven by the inverse of the COM waveform. This means that half the time the segment will be driven by a positive voltage, and by a negative voltage the other half of the time. These two states have the same visual appearance, so the segment appears to be on constantly. Since the average DC value of the voltage difference is zero, no static DC bias remains which could damage the LCD glass.
The main loop for the example application which drives the LCD segments is shown below.
Main: mov IE, #080h ; Disable timer 0 interrupt temporarily mov R2, DigitP1 ; Grab local copies of digit variables mov R3, DigitP2 mov R4, DigitP3 mov IE, #082h ; Re-enable timer 0 interrupt mov A, R2 call getDigit ; Calculate segment pattern for ones digit anl A, #01111111b ; Ensure that COM (P1.7) is driven low mov P1, A mov A, R3 call getDigit ; Calculate segment pattern for tens digit mov P2, A mov A, R4 call getDigit ; Calculate segment pattern for hundreds digit mov P3, A ;;;; Delay loop ;;;; mov R0, #0FFh L1A: mov R1, #0FFh L1B: djnz R1, L1B djnz R0, L1A ;;;;;;;;;;;;;;;;;;;;;; mov A, R2 call getDigit ; Calculate segment pattern for ones digit cpl A ; Inverse of the pattern driven on the first frame half orl A, #10000000b ; Ensure that COM (P1.7) is driven high mov P1, A mov A, R3 call getDigit ; Calculate segment pattern for tens digit cpl A ; Inverse of the pattern driven on the first frame half mov P2, A mov A, R4 call getDigit ; Calculate segment pattern for hundreds digit cpl A ; Inverse of the pattern driven on the first frame half mov P3, A ;;;; Delay loop ;;;; mov R0, #0FFh L2A: mov R1, #0FFh L2B: djnz R1, L2B djnz R0, L2A ;;;;;;;;;;;;;;;;;;;;;; ljmp Main ; Go back for another frame cycle (endless loop)Note that the COM line (connected to P1.7) is always driven with the same waveform: low for the first half of the frame, and high for the second half. For the segment lines, the pattern driven in the first half of the frame is inverted for the second half. Each of the three digits is connected in the same manner to each of the three ports, so that segment A is always connected to Px.0, segment B to Px.1, and so on. This configuration allows the example code to use the getDigit routine to calculate the segment pattern for each of the three LCD panel digits.
;*************************************************************************** ;* ;* getDigit ;* ;* Returns an LCD segment pattern (in Acc) for the decimal digit (0 to 9) ;* input (also in Acc) ;* getDigit: cjne A, #0, getDigit_not0 ; xgfedcba mov A, #00111111b ; Zero ret getDigit_not0: cjne A, #1, getDigit_not1 ; xgfedcba mov A, #00000110b ; One ret getDigit_not1: cjne A, #2, getDigit_not2 ; xgfedcba mov A, #01011011b ; Two ret getDigit_not2: cjne A, #3, getDigit_not3 ; xgfedcba mov A, #01001111b ; Three ret getDigit_not3: cjne A, #4, getDigit_not4 ; xgfedcba mov A, #01100110b ; Four ret getDigit_not4: cjne A, #5, getDigit_not5 ; xgfedcba mov A, #01101101b ; Five ret getDigit_not5: cjne A, #6, getDigit_not6 ; xgfedcba mov A, #01111101b ; Six ret getDigit_not6: cjne A, #7, getDigit_not7 ; xgfedcba mov A, #00000111b ; Seven ret getDigit_not7: cjne A, #8, getDigit_not8 ; xgfedcba mov A, #01111111b ; Eight ret getDigit_not8: cjne A, #9, getDigit_not9 ; xgfedcba mov A, #01101111b ; Nine ret getDigit_not9: mov A, #0 ret
Running the Counter
The pattern displayed on the LCD by the example code is a 3-digit decimal counter, which starts at 000 on power-up and increments to 001, 002, etc., until it reaches 999 and rolls over. Since the main loop of the program drives the LCD segment and common patterns, we must find another method to periodically increment the counter value. One solution is to periodically trigger an interrupt using Timer 0.
mov TMOD, #021h ; Timer 1: 8-bit autoreload from TH1 ; Timer 0: 16-bit mov TCON, #050h ; Enable timers 0 and 1 mov CKMOD, #038h ; Use system clock for all timer inputs mov IE, #082h ; Enable timer 0 interruptEach time the timer interrupt occurs, a delay counter in register memory is decremented. When this delay counter reaches zero, the LCD 3-digit counter value is incremented by one (with each digit rolling over as needed); the delay counter reinitializes to its maximum value. Since Timer 0 is 16 bits in width and since the example code sets the delay counter to 20, the 3-digit counter will increment approximately every
org 000Bh ; Timer 0 interrupt ljmp IntTimer0 ;*************************************************************************** ;* ;* IntTimer0 (INTT0) ;* ;* Timer interrupt service routine ;* IntTimer0: push ACC ; Save off accumulator and R0 push R00 mov R0, Count ; Only increment LCD digits every [CountMax] ; interrupt cycles djnz R0, INTT0_Done inc DigitP1 ; Increment ones digit on display mov A, DigitP1 cjne A, #10, INTT0_Continue ; Check for rollover mov DigitP1, #0 inc DigitP2 ; Increment tens digit on display mov A, DigitP2 cjne A, #10, INTT0_Continue ; Check for rollover mov DigitP2, #0 inc DigitP3 ; Increment hundreds digit on display mov A, DigitP3 cjne A, #10, INTT0_Continue ; Check for rollover mov DigitP3, #0 INTT0_Continue: mov R0, CountMax ; Reset to starting cycle count INTT0_Done: mov Count, R0 ; Update cycle counter pop R00 pop ACC ; Restore accumulator and R0 reti
Conclusion
As with many dedicated digital peripherals on a microcontroller, a static or multiplexed LCD display controller can be implemented in software if necessary. The simplicity of a static display makes this implementation particularly straightforward. The standard, general-purpose I/O functionality of an 8051 microcontroller like the DS89C450 can be used to drive the SEG and COM waveforms on the LCD. Using the high-performance DS89C450 ensures that plenty of processing power remains for the bulk of the application even after the LCD controller is implemented in software.