Quad-Apollo MxFE: A 16 Receive/16 Transmit X-Band Direct Sampling Digital Beamforming Subsystem Reference Design

Jan 18 2026

Figure 1

   

Abstract

This article presents the design and implementation of the Quad-Apollo MxFE™ (mixed-signal front end) X-band digital beamforming platform, an advanced every-element direct-RF-sampling reference architecture developed to demonstrate the full capabilities of Analog Devices’ Apollo MxFE technology. The platform integrates four transceivers with synchronized clocking, deterministic triggering, and phase-coherent timing to enable true digital beamforming across 16 transmit and 16 receive channels at X-band frequencies. A comprehensive signal chain—including low noise RF front end, precision clock generation, multichip synchronization, and power distribution—is implemented to realize a scalable, phase-coherent array capable of wideband operation and multibeam support.

Introduction

The Quad-Apollo MxFE™ (mixed-signal front-end) X-band direct sampling digital beamforming platform (Figure 1) is an advanced, every-element digital, direct RF-sampling solution that serves as a complete reference architecture for next-generation digital beamforming systems. Designed to highlight the capabilities of Analog Devices’ MxFE® technology, the platform integrates all critical subsystems—RF signal conditioning, precision clocking, multichip synchronization, and DC power management—into a unified, high performance environment that supports coherent, scalable signal processing across multiple channels.

Each subarray within this platform comprises 16 receive and 16 transmit channels configured in a uniform linear array, with an element spacing corresponding to half a wavelength at 12 GHz. This geometry enables optimal spatial sampling for X-band operation while supporting full digital beamforming across all elements. The platform demonstrates how multiple AD9084 Apollo MxFE data converters can be seamlessly synchronized and clocked together within one coherent architecture, providing a realistic example of system-level integration for high channel count RF applications.

Beyond its role as a reference design,1 the Quad-Apollo MxFE platform serves as a versatile development and evaluation tool for advanced radar and communications systems. Its architecture supports multiple simultaneous beams, adaptive nulling, and reconfigurable beam patterns, offering the flexibility required for modern phased array radar, electronic warfare, and multimission sensing applications. The system’s deterministic timing framework, broadband front end, and scalable synchronization scheme together illustrate a complete signal chain—from RF input to digital beamformed output—designed to accelerate innovation in high speed, every-element digital array technology.

Figure 1. Quad-Apollo MxFE hardware.
The block diagram in Figure 2 illustrates a single subarray’s transmit and receive RF front-end signal chain, the data converter equipped with hardened digital signal processing features, multichip clocking solution, and 12 VDC power solution. A commercial off-the-shelf FPGA carrier card in combination with open-source low level software drivers and MATLAB® tool boxes enables software control of the system platform.2,3 
Figure 2. Full Quad-Apollo MxFE system block diagram with the ADF4382A.

RF Front End

The RF front end of the Quad-Apollo MxFE system is designed with intentional simplicity and modularity, emphasizing flexibility, performance, and ease of customization for a wide range of applications. As illustrated in figures 3 and 4, the architecture leverages broadband, low complexity signal paths to ensure wide frequency coverage while maintaining high linearity and signal integrity throughout the chain. 

At its core, the design employs 2:1 broadband baluns to interface the high speed ADCs and DACs with the remainder of the analog signal chain. Each transmit-receive channel incorporates a shared, digitally tunable X-band filter (ADMV8913), which provides precise frequency selection and out-of-band rejection. This filter stage includes a board-level bypass path that can be activated through a capacitor rotation mechanism, allowing direct sampling at S-, C-, and Ku-band frequencies. When the filter is bypassed, the system sacrifices the inherent antialiasing benefits provided by the ADMV8913 but gains extended frequency flexibility for broadband or wideband applications where filtering can be handled digitally.

On the receive side, each channel features a modest, yet highly linear, broadband low noise amplifier (LNA) followed by a wideband digital step attenuator (DSA) at the input stage. The DSA enables fine-grained analog gain control across varying signal conditions and is directly controlled via the data converter’s general-purpose input output (GPIO) interface for rapid, deterministic adjustment during system operation. This architecture supports fast reconfiguration, making it particularly suitable for adaptive or real-time beamforming systems.

Receiver linearity was given special emphasis in the design, as intermodulation distortion products tend to be spatially correlated across elements in a fully digital, every-element phased array system. By prioritizing linearity, Quad-Apollo MxFE technology ensures that dynamic range and spectral purity are maintained, even in multichannel coherent configurations.

For applications requiring additional frequency translation, gain stages, or specialized signal conditioning, the platform supports the integration of plug-in personality cards ahead of the front end. This modular extension capability allows system designers to tailor the performance envelope to meet specific end-use requirements, whether optimizing for bandwidth, noise figure, or frequency coverage. By keeping the subarray-level signal chain streamlined and broadband, the Quad-Apollo MxFE system provides a robust yet flexible foundation for scalable, high performance RF system development. 
Figure 3. Receiver signal chain block diagram with the ADMV8913, ADL8100, and ADRF5730.
Figure 4. Transmitter signal chain block diagram with the ADMV8913 and ADL8102.

Clocking Architecture

Clocking plays a pivotal role in modern multiconverter systems, acting as the backbone that enables multichip synchronization, deterministic latency, and coherent signal combining across large, distributed architectures. Precise clock distribution ensures that every data converter, FPGA, and analog front end operates in perfect harmony—an essential requirement for applications such as phased array radar, high channel count instrumentation, and advanced communications systems.

In these systems, synchronization based on the JESD204C standard is achieved through a combination of dedicated clock-generation and clock-distribution blocks, supplemented by a bidirectional subclass 1 synchronizer. This architecture guarantees deterministic latency across all JESD204C channels, allowing system designers to predict and control timing with nanosecond-level precision. Furthermore, the synchronization scheme can be extended beyond a single subsystem, maintaining deterministic latency across multiple subarrays for large-scale implementations.

As illustrated in Figure 5, a single high stability reference clock serves as the foundation for the entire timing network. This reference is distributed through ultralow jitter clock fanout buffers that feed the MxFE devices with exceptionally clean, ultralow phase noise sampling clocks. Each MxFE device employs a dedicated two-wire clock interface that continuously maintains phase and frequency alignment, compensating for drift due to temperature changes or long-term aging effects.

The same master reference also drives a secondary clock generation stage responsible for producing digital clocks for the FPGA fabric and providing precision reference signals to the synchronizer. A 10-channel precision synchronizer forms the heart of the coordination mechanism, delivering bidirectional, low frequency timing signals that align all data converters and the FPGA to a common timing reference. This synchronizer also enables per-channel propagation delay trimming, allowing engineers to fine-tune alignment and phase relationships between channels for optimal performance.

Depending on the overall array architecture, the synchronizer can be deployed in daisy-chain or fanout configurations, ensuring scalable synchronization across multiple subarrays or system partitions. Even when operating at extremely high sample rates—up to 20 GSPS—the clocking infrastructure maintains deterministic alignment, ensuring phase coherence and timing integrity throughout the system. By combining low jitter clocking, hierarchical distribution, and JESD204C subclass 1 synchronization, the entire multiconverter platform achieves a unified, phase-stable timing framework that underpins high speed data acquisition and signal processing performance.

Figure 5. Clocking architecture block diagram.
Table 1. Quad-Apollo MxFE Use Cases
System Reference Clock (MHz)
Sample Clock (GSPS)
ADC Sample Rate (GSPS)  DAC Sample Rate (GSPS) JESD204C Lane Rate (GBPS) Decimation Rate Lane Rate (MSPS) Useable Instantaneous Bandwidth (MHz)
400
12.8
12.8  25.6  13.2   32  400 320 
400
12.8
12.8  25.6  26.4   16 800  640 
400
20
20   20  20.625  16 625   500

Table 1 summarizes three representative operating configurations of the Quad-Apollo MxFE system driven by a 400 MHz reference clock. Together, these configurations illustrate the trade-offs between sampling rate, digital decimation, and data throughput in optimizing bandwidth and interface performance for different system requirements.

Conclusion

System-level validation of the Quad-Apollo MxFE X-band digital beamforming platform confirms coherent operation across all channels, achieving sub-degree phase alignment and sub-picosecond timing accuracy. The demonstrated performance in adaptive beam steering, spatial nulling, and multibeam transmission highlights the platform’s readiness to emulate next-generation radar and electronic warfare architectures.

These results represent an important milestone in realizing scalable, every-element digital beamforming systems. Future articles will explore the deeper technical dimensions of the Quad-Apollo MxFE platform, building on this foundation to uncover the full potential of direct-RF-sampling architectures in enabling the next era of high performance, software-defined arrays.

References

1 ADXBAND16EBZ Prototyping Platform User Guide. Analog Devices Wiki.

2 AMD Virtex™ UltraScale+™ FPGA VCU118 Evaluation Kit. AMD.

3 analogdevicesinc/HighSpeedConverterToolbox: MATLAB Toolbox for ADI High Speed Converter

    Products. GitHub.

About the Authors

Siddhartha Das
Siddhartha Das is a systems applications engineer on the Subsystems and Sensors Team within Analog Devices’ Aerospace, Defense, and Communications Business Unit based in Durham, North Carolina. He earned his B.S. in
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Technology Solutions