Design Note 57: Video Circuits Collection
Introduction
This note shows how to make several different video circuits using high speed op amps. All of these circuits work with composite, RGB and monochrome video. For best results, bypass the power supply pins of these amplifiers with 1μF to 10μF tantalum capacitors in parallel with 0.01μF disc capacitors. It is important to terminate both ends of video cables to preserve frequency response. When properly terminated, the cable looks like a resistive load of 150Ω.

Figure 1. Lots of Inputs Video MUX Cable Driver (LT1227).
Multiplex Amplifiers
Often it is desirable to select one of several signals to send down a cable. Connecting the outputs of several amplifiers together and using the amplifier’s shutdown pin to disable all but one accomplishes this goal. The LT1190, LT1191, LT1192, and LT1193 are shutdown by pulling pin 5 to the negative supply.

Figure 2. Two Input Video MUX Cable Driver (LT1190).
The LT1223 and LT1227 current feedback amplifiers are shutdown by pulling Pin 8 to ground. During normal operation Pin 8 is open and at the positive supply potential. An easy way to interface Pin 8 to logic is with a logic level N-channel FET or a 74C906 (open-drain hex buffer).
| Part Number | Differential | |||
| Load = 1kΩ |
Load = 150Ω |
|||
| Gain | Phase | Gain | Phase | |
| LT1190* |
0.05 | 0.03 | 0.23 | 0.16 |
| LT1191* |
0.03 | 0.01 | 0.09 | 0.07 |
| LT1192** | 0.10 | 0.01 | 0.23 | 0.15 |
| LT1193* | 0.20 | 0.08 | 0.20 | 0.08 |
| LT1194** | 0.20 | 0.08 | 0.20 | 0.08 |
| LT1223 | 0.01 | 0.02 | 0.12 | 0.26 |
| LT1227 | 0.01 | 0.01 | 0.01 | 0.01 |
| LT1228 | 0.01 | 0.01 | 0.04 | 0.10 |
| LT1229 | 0.01 | 0.01 | 0.04 | 0.10 |
| VS = ±15V, AV = 2 *VS = ±8V, AV = 2 **VS = ±8V, AV = 10 |
||||
Loop Through Cable Receivers
Most video instruments require high impedance differential input amplifiers that will not load the cable even when the power is off.

Figure 3. Differential Input Video Loop Through Amplifier Using a Video Difference Amplifier (LT1194).

Figure 4. Electronically Controlled Gain, Video Loop Through Amplifier (LT1228).
DC Restore Circuits
The following circuit restores the black level of a monochrome composite video signal to 0V at the beginning of every horizontal line. This circuit is also used with CCD scanners to set the black level.

Figure 5. Video DC Restore (Clamp) Circuit (LT1228)/
Fader Circuits
Using two LT1228 transconductance amplifiers in front of a current feedback amplifier forms a video fader. The ratio of the set currents into Pin 5 determines the ratio of the inputs at the output.

Figure 6. Video Fader (LT1228, LT1223).