AN-1272: Differences Between the ADE7854A/ADE7858A/ADE7868A/ADE7878A and ADE7854/ADE7858/ADE7868/ADE7878 Products
Introduction
The ADE7854A/ADE7858A/ADE7868A/ADE7878A are enhanced versions of the ADE7854/ADE7858/ADE7868/ADE7878 energy measurement ICs. This application note describes the differences between these products and is recommended for use alongside the ADE7854A/ADE7858A/ADE7868A/ADE7878A data sheet.
The ICs are pin to pin compatible with the following exception regarding Pin 20, REF_GND. In the ADE7854A/ADE7858A/ADE7868A/ADE7878A, it is recommended that REF_GND is tied to ground while in the ADE7854/ADE7858/ADE7868/ADE7878, this pin is a No Connect. Note, however, that there is no degradation of performance even if this pin is left floating in the ADE7854A/ADE7858A/ADE7868A/ADE7878A.
New and Improved Features
ACCMODE Register Settings
Phase B Voltage Calculation for Delta Configuration
For 3-phase, 3-wire delta configuration, Bits[5:4] (CONSEL[1:0] bits) of the ACCMODE register must be set to 01 in the ADE7854/ADE7858/ADE7868/ADE7878. Because Phase B is used as the reference ground in this configuration, Phase B voltage is not measured. Thus, in the enhanced models, Phase B voltage is calculated as the difference between the voltages of Phase A and Phase C, yielding
VB = VA − VC
Thus, the ADE7854A/ADE7858A/ADE7868A/ADE7878A compute BVRMS in 3-phase, 3-wire delta configuration.
Absolute Reactive Energy Mode
An absolute reactive energy mode is made available in the CFx outputs of ADE7854A/ADE7858A/ADE7868A/ADE7878A. When the VARACC, Bits[1:0] in the ACCMODE register are set to 11, though the reactive powers are accumulated in signed mode in the xVARHR registers, the CFx pulses output energy according to an absolute accumulation.
PSM2 Level Changes
The ADE7868A/ADE7878A offer an option to select from eight different threshold levels, one being 587 times lower than the analog full-scale level. This allows the user to set much lower thresholds than in the ADE7868/ADE7878. There is also an optional PSM2 IRQ1 only mode where IRQ0 functionality is disabled. This avoids any glitches in the IRQ0 interrupt from erroneously indicating that a tamper condition has or has not occurred.
By default, IRQ0 and IRQ1 are enabled which results in a larger measurement window than that in the ADE7868/ADE7878. As shown in Table 1, there is a single interrupt mode, which has the same measurement period as in the ADE7868/ADE7878. It is recommended to use the IRQ1 only mode, along with an external timer, for quicker tamper detection.
| Product | IRQ0 and IRQ1 Default Mode | IRQ1 Only Mode |
| ADE7868/ADE7878 | (LPLINE[4:0] + 1)/ 50 sec | Mode not Available. |
| ADE7868A/ADE7878A | (LPLINE[4:0] + 10)/ 50 sec | Measurement period decided by user; external timer can be used. Recommended measurement period: (LPLINE[4:0] +1)/50 sec. |
Calculation of Netural Current RMS from IA, IB, and IC
The ADE7868A and ADE7878A provide the user with the option to compute the sum of the instantaneous phase currents and store it in the NIRMS register, if Bit 0 (the INSEL bit) of the CONFIG_A register is set to 1.
When the INSEL bit is set to 1, the NIRMSOS register does not provide an offset to the NIRMS register. There is also an option to calculate the neutral current rms from the IN channel inputs, such as in the ADE7868/ADE7878, when the INSEL bit is set to 0.
CF Output—Increased Drive Strength
The CF output in the ADE7854A/ADE7858A/ADE7868A/ADE7878A can sink 8 mA, up from 2 mA, on the ADE7854/ADE7858/ADE7868/ADE7878, which makes it easier to drive LEDs and opto couplers.
Low Ripple RMS Measurements
Apart from the regular rms measurements, a separate set of rms measurements can be taken, using the ADE7854A/ADE7858A/ADE7868A/ADE7878A with more averaging. To make these measurements accessible to the user, seven new registers (IARMS_LRIP, VARMS_LRIP, IBRMS_LRIP, VBRMS_LRIP, ICRMS_LRIP, VCRMS_LRIP, and INRMS_LRIP) are provided. These measurements are obtained as a result of averaging 8192 consecutive rms register readings and the registers are updated every 1.024 seconds. The reading settles after 2.048 seconds.
SPI Burst Read Mode
An SPI burst read mode is enabled in the ADE7854A/ADE7858A/ADE7868A/ADE7878A. Registers from Address 0xE50C through Address 0xE51B, that store the instantaneous current, voltage, and power values on each phase, can be read back continuously with just one command.
Once the start address is made available to the ADE7854A/ADE7858A/ADE7868A/ADE7878A, it keeps transmitting the values of successive registers starting at that location, one-by one, until the last register (0xE51B). The user has the option to terminate the operation by bringing the SS line high at any time during this transfer.
Deglitch Filter
An improved deglitch filter is used in the ADE7854A/ADE7858A/ADE7868A/ADE7878A that helps prevent high frequency crystal perturbations from affecting the performance of the product.
Communication Verifiation Registers
Five new registers have been added, LAST_ADDR, LAST_OP, LAST_RWDATA_8, LAST_RWDATA_16, and LAST_RWDATA_32, for communication verification purposes. The LAST_ADDR stores the most recent accessed memory address, LAST_OP stores the recent most performed operation, and the LAST_RWDATA_x registers store the recent most register data corresponding to the last address and operation performed.
Checksum Register
The Checksum (CHECKSUM) register of the ADE7854A/ADE7858A/ADE7868A/ADE7878A includes a CRC calculation done on a much wider set of registers than done with the ADE7854/ADE7858/ADE7868/ADE7878. All the configuration registers are now a part of the CRC calculation. Some registers, such as APHCAL, BPHCAL, CPHCAL, and CONFIG_A, are added to the list, along with the register list that already existed in the CRC calculation of the ADE7854/ADE7858/ADE7868/ADE7878. Also, the DSP data memory RAM registers starting from Address 0x4380 through Address 0x43BE, were added to the list. Though the resultant checksum is still a 32-bit register, the number of bits that enter the LFSR is 2344, in the enhanced model. This provides a more comprehensive check of the default settings, when compared to the ADE7854A/ADE7858A/ADE7868A/ADE7878A. A CRC interrupt is also made available o the user, which flags any change in the Checksum register.
POR Threshold
The POR threshold has been changed from 2.0 V in the ADE7854/ADE7858/ADE7868/ADE7878 to 2.5 V in the ADE7854A/ADE7858A/ADE7868A/ADE7878A. This results in a reduction in the supply voltage operation range for the PSM1 and PSM2 levels of the ADE7868A/ADE7878A. The range for the ADE7868A/ADE7878A is 2.7 V to 3.7 V, instead of 2.4 V to 3.7 V in the ADE7868/ADE7878.
Increased Filtering for Power Computations
An increased filtering option is available to the active and reactive power computations in the ADE7854A/ADE7858A/ADE7868A/ADE7878A. A stronger low-pass filter (LPF) with twice the settling time, and almost twice the ripple attenuation, is enabled when Bit 1 (the LPFSEL bit) of the CONFIG_A register is set to 1.
| LPFSEL Bit | Settling Time | Ripple Attenuation |
| 0 | 650 ms | 65 dB |
| 1 | 1300 ms | 128 dB |
Register Changes and Inclusions
The ADE7854A/ADE7858A/ADE7868A/ADE7878A contain all ADE7854/ADE7858/ADE7868/ADE7878 registers, with modifications to certain registers. Several new registers are also available in the ADE7854A/ADE7858A/ADE7868A/ADE7878A.
Table 3 represents all the new registers that have been included in the ADE7854A/ADE7858A/ADE7868A/ADE7878A, while Table 4 represents the registers that are present in ADE7854/ADE7858/ADE7868/ADE7878 products, but are modified in the ADE7854A/ADE7858A/ADE7868A/ADE7878A.
| Registers Added | Address Location |
| IARMS_LRIP | 0xE530 |
| VARMS_LRIP | 0xE531 |
| IBRMS_LRIP | 0xE532 |
| VBRMS_LRIP | 0xE533 |
| ICRMS_LRIP | 0xE534 |
| VCRMS_LRIP | 0xE535 |
| INRMS_LRIP | 0xE536 |
| CONFIG_A | 0xE740 |
| LAST_OP | 0xE7FD |
| LAST_ADDR | 0xE6FE |
| LAST_RWDATA_8 | 0xE7FC |
| LAST_RWDATA_16 | 0xE6FF |
| LAST_RWDATA_32 | 0xE5FF |
| Registers Modified | Address Location |
| CHECKSUM | 0xE51F |
| ACCMODE | 0xE701 |
| LPOILVL | 0xEC00 |
| CONFIG2 | 0xEC01 |
| STATUS1 | 0xE503 |
| MASK1 | 0xE50B |
Migrating to the Enhanced Product
Moving over from the ADE7854/ADE7858/ADE7868/ADE7878 to the ADE7854A/ADE7858A/ADE7868A/ADE7878A offers multiple advantages. All features available in the ADE7854/ADE7858/ADE7868/ADE7878 are also available for the ADE7854A/ADE7858A/ADE7868A/ADE7878A. Further, there is no need to change the layout or evaluation setup when migrating to the enhanced version of the product. The evaluation board, evaluation software, and firmware codes provided for the ADE7854A/ADE7858A/ADE7868A/ADE7878A, are backward compatible with the ADE7854/ADE7858/ADE7868/ADE7878 family of parts.
Hardware Compatibility
ADE7854A/ADE7858A/ADE7868A/ADE7878A products can be used in the application with the same hardware as the ADE7854/ADE7858/ADE7868/ADE7878 products. No design changes are required. The evaluation board for the ADE7854/ADE7858/ADE7868/ADE7878 products can be used to evaluate the enhanced products as well.
Pin 20, REF_GND
This pin, NC, in the ADE7854/ADE7858/ADE7868/ADE7878, is a ground pin in the ADE7854A/ADE7858A/ADE7868A/ADE7878A. It is recommended to ground this pin externally. This change should not cause any major impact because the recommended layout of ADE7854/ADE7858/ADE7868/ADE7878 recommends grounding the NC pins externally. However, the performance of the A version of the products remains similar to the ADE7854/ADE7858/ADE7868/ADE7878 even when the existing layout has left the pin floating.
Software Compatibilty
The microcontroller code and its protocol, developed for the ADE7854/ADE7858/ADE7868/ADE7878 products, works with the ADE7854A/ADE7858A/ADE7868A/ADE7878A without requiring any modifications to be made with the exception of the changes described in this section.
LPOILVL Register
The default value of the LPOILVL register remains the same, but the default threshold level and measurement period vary. In the ADE7854/ADE7858/ADE7868/ADE7878, the default threshold level is 7/8th of the full scale; in the enhanced version, the default threshold level is 1/587th of full scale. Similarly, as shown in Table 1, the default measurement window in the enhanced product differs from the ADE7854/ADE7858/ADE7868/ADE7878.
Checksum Register
The default values of the Checksum register in the ADE7854A/ADE7858A/ADE7868A/ADE7878A ICs are different from those of the ADE7854/ADE7858/ADE7868/ADE7878 ICs. However, while monitoring the checksum in the application, if the configuration registers are read initially to obtain the default value, and then tracked continuously for changes, then the change in functionality of this register does not cause any problems.
Note that all the configuration registers are now a part of the CRC calculation and thus any change in the value of the registers that have been newly added to the Checksum list are reflected in the value of the Checksum register.
New Functionalities Assigned to Previously Reserved Bits
Some of the reserved bits of the ACCMODE, CONFIG2, STATUS1, and MASK1 registers in the ADE7854/ADE7858/ADE7868/ADE7878 have been assigned new functionalities in the ADE7854A/ADE7858A/ADE7868A/ ADE7878A. The operation remains the same when the default values of these bits are preserved.