Programmable Quad Supervisors Offer Unparalleled Flexibility for Multi-Voltage Monitoring Applications

2002-12-01

Figure 1

   

Introduction

Three new power supply supervisors improve system reliability by offering more accurate reset thresholds than other supervisors on the market. They also save design time, production costs and board space with easy-to-use, flexible interfaces and a low external parts count.

The LTC2900, LTC2901 and LTC2902 quad supervisors can simultaneously monitor four supply voltages with 1.5% threshold accuracy over temperature. Each part offers 16 user-selectable four-voltage combinations from the following: 5V, 3.3V, 3V, 2.5V, 1.8V, 1.5V, +ADJ and –ADJ. A simple external resistor divider performs single-pin programming, eliminating the need to qualify, source and stock different part numbers for different combinations of supply voltages. All three parts are configured for 5% power supply tolerance and the LTC2902 can also be programmed to work with power supplies at 7.5%, 10% and 12.5% tolerance. These new devices require no software, no calibration and no trimming. In some applications, they can be used with no external components, saving additional board space and cost. Available features include manual reset, watchdog functions, selectable supply tolerance and supply margining functions. The reset and watchdog times are also user adjustable via external capacitors.

The LTC2900, LTC2901 and LTC2902 supervisors offer micropower operation, small size, high accuracy and multiple reset output options. The extensive integrated functionality makes these devices easy to design into multi-voltage supervisory applications. Table 1 shows a feature summary for these devices. Figure 1 shows a fixed quad application with push-button reset using the LTC2900-2.

Figure 1. Typical application using the LTC2900-2 for 4-line voltage monitoring.

Table 1. LTC2900, LTC2901 and LTC2902 Feature Summary
Feature LTC2900 LTC2901 LTC2902
Programmable Input Threshold Combinations 16 16 16
Threshold Accuracy 1.5% 1.5% 1.5%
“Open-drain” Reset LTC290x-1
Push-Pull Reset LTC290x-2
Adjustable Reset Time
Buffered Reference
Individual Comparator Outputs
Manual Reset
Independent Adjustable Watchdog Circuitry
Reset Disable
Monitored Supply
Tolerance
Fixed 5% Fixed 5% User Selectable 5%, 7.5%, 10%, 12.5%
Package 10-lead MSOP 16-lead SSOP 16-lead SSOP

Safe Beginnings: Generating the Power-On Reset (POR)

Reliable operation in many systems requires knowledge of when certain power supplies have exceeded minimum thresholds and have remained stable for a specified period of time. One way to provide that knowledge is with a reliable Power-On Reset (POR) signal generated from a highly accurate voltage monitor.

A typical device that requires a reliable POR signal is a microprocessor. The LTC2900, LTC2901 and LTC2902 can prevent a processor from executing instructions until all supply voltages have reached safe thresholds, regardless of the power supply turn-on characteristics. Furthermore, if any supply voltage falls back below a threshold with sufficient duration and magnitude, the reset command is reissued. Once the voltage has returned above the threshold and has remained there for a specified amount of time, the reset line is released.

In order to firmly establish the correct reset logic state, power must get to the reset drive circuitry early in the power-up phase. The LTC2900, LTC2901 and LTC2902 supervisors are powered automatically from the greater of the voltages on the V1 and V2 inputs. With V1 or V2 at 1V or greater, the reset output is specified to be a logic low of 0.3V (max) while sinking 100µA.

Why is Threshold Accuracy Important?

A system voltage margin specification must take three factors into account: power-supply tolerance, IC supply voltage tolerance and supervisor reset threshold accuracy. If a system is to work reliably, none of these can be left out of the design equation. The roles of the power-supply voltage tolerance and the IC supply voltage tolerance are fairly straightforward, but the role of supervisor accuracy in reliable system design is not as obvious. In the simplest terms, diminished accuracy corresponds to a system that must operate reliably over a wider voltage range, complicating the system design; whereas improved accuracy decreases the voltage margin required for reliable system operation, simplifying the system design.

Consider a 5V system with a ±5% power supply tolerance band (see the figure in this sidebar). System ICs powered by this supply must operate reliably within this band (and a little more, as explained below). The bottom of the supply tolerance band, at 4.75V (5V–5%), is the exact voltage at which a perfectly accurate supervisor would generate a reset. Such a perfectly accurate supervisor does not exist—the actual reset threshold may vary over a specified band (±1.5% for the LTC2900, LTC2901 and LTC2902 supervisors).

Improved undervoltage monitor threshold accuracy translates to improved system reliability.

With this variation of reset threshold in mind, the nominal reset threshold of the supervisor is set below the minimum supply voltage; just enough so that the reset threshold band and the power supply tolerance bands do not overlap. If the two bands do overlap, the supervisor could generate a false or nuisance reset when the power supply is actually within its specified tolerance band (say, at 4.8V).

The LTC2900, LTC2901 and LTC2902 have ±1.5% reset threshold accuracy, so 5% thresholds are typically set to 6.5% below the nominal input voltage. For the 5V input, the typical threshold is 4.675V, or 75mV below the ideal threshold of 4.750V. The actual threshold is guaranteed to lie in the band between 4.750V and 4.600V over temperature. The powered system must work reliably down to the low end of the threshold band, or risk malfunction before a reset signal is properly issued. In our 5V example, using the 1.5% accurate supervisor, the system ICs must work down to 4.6V. The same system using a ±2.5% accurate supervisor must operate down to 4.5V, increasing the required system voltage margin, and the probability of system malfunction.

One Chip Covers All Supply Voltages: Single Pin Programming

The LTC2900, LTC2901 and LTC2902 ICs give designers the freedom to specify one chip for all supervisory applications, even though the nominal supply voltages may not be finalized. The desired input voltage combination is selected by placing a simple resistive divider between the reference pin (VREF) and ground (GND) and connecting the tap point to the programming pin (VPG), as shown in Figure 2. The programming process occurs during power-up and is transparent to the user. Table 2 specifies the recommended 1% resistor values for programming the available input combinations. The last column in Table 2 specifies optimum VPG/VREF ratios (±0.01) to be used when programming with a ratiometric DAC.

Figure 2. Programming the voltage monitoring modes (see table 2 for R1and R2 values).

Table 2. Voltage Threshold Programming
Mode V1 (V) V2 (V) V3 (V) V4 (V) R1 (kΩ) R2 (kΩ) VPG/VREF
0 5.0 3.3 ADJ ADJ Open Short 0.000
1 5.0 3.3 ADJ –ADJ 93.1 9.53 0.094
2 3.3 2.5 ADJ ADJ 86.6 16.2 0.156
3 3.3 2.5 ADJ –ADJ 78.7 22.1 0.219
4 3.3 2.5 1.5 ADJ 71.5 28.0 0.281
5 5.0 3.3 2.5 ADJ 66.5 34.8 0.344
6 5.0 3.3 2.5 1.8 59.0 40.2 0.406
7 5.0 3.3 2.5 1.5 53.6 47.5 0.469
8 5.0 3.0 2.5 ADJ 47.5 53.6 0.531
9 5.0 3.0 ADJ ADJ 40.2 59.0 0.594
10 3.3 2.5 1.8 1.5 34.8 66.5 0.656
11 3.3 2.5 1.8 ADJ 28.0 71.5 0.719
12 3.3 2.5 1.8 –ADJ 22.1 78.7 0.781
13 5.0 3.3 1.8 –ADJ 16.2 86.6 0.844
14 5.0 3.3 1.8 ADJ 9.53 93.1 0.906
15 5.0 3.0 1.8 ADJ Short Open 1.000

Monitor Any Positive or Negative Voltage: Configuring the Adjustable Inputs

Voltages not explicitly listed in Table 2 can be monitored using the positive adjustable (ADJ) and negative adjustable (–ADJ) inputs. The positive adjustable threshold available on the V3 or V4 input is set to 0.5V. For the majority of positive adjustable applications, the tap point on an external resistive divider (R3, R4) placed between the positive voltage being sensed and ground is connected to the high impedance input on V3 or V4. Figure 3 demonstrates a generic setup for the positive adjustable application.

Figure 3. Setting the positive adjustable trip point, VTRIP = 0.5V(1 + R3/R4).

The negative adjustable threshold available on the V4 input is tied to ground. In negative adjustable applications, the tap point on an external resistive divider (R3, R4) placed between the negative voltage being sensed and VREF, is connected to the high impedance input on V4. The voltage on the VREF pin (1.210V nominal) provides the necessary and accurate level shift required to operate near ground. The VREF pin can source and sink up to 1mA of current over the full temperature range –40°C to 85°C. Figure 4 shows a generic setup for the negative adjustable application.

Figure 4. Setting the negative adjustable trip point (VTRIP = –VREF(R3/R4).

It is also possible to monitor voltages between ground and +0.5V using the positive adjustable inputs. Similar to the offset technique in the negative adjustable application, tie a resistor from VREF to the V3 or V4 input, and an appropriate resistor to the monitored voltage.

Quality System Design: Consider Threshold Accuracy and Noise Sensitivity

System reliability depends on power supply reset thresholds that remain accurate over temperature and power supply variations (see sidebar). All LTC2900, LTC2901 and LTC2902 supervisor inputs have the same relative threshold accuracy: ±1.5% of the nominal input voltage over temperature (see Figure 5).

Figure 5. Typical threshold accuracy vs temperature (LTC2900, LTC2901 and LTC2902).

In any supervisory application, supply noise riding on the monitored DC voltage can cause spurious resets, particularly when the monitored voltage is already near the reset threshold.

One commonly used, but problematic, solution to this problem is the addition of hysteresis to the input comparator. The amount of hysteresis is usually specified as a percentage of the trip threshold, and typically needs to be added to the advertised accuracy of the part in order to determine the true accuracy on the trip threshold. This technique degrades accuracy, and therefore is not used on the LTC2900, LTC2901 and LTC2902 supervisors.

Instead, two forms of noise filtering are employed to minimize spurious resets while maintaining system accuracy.

The first line of defense used to minimize the effect of noise is a proprietary tailoring of the comparator transient response. Transient events receive a form of electronic integration in the comparator and must be of sufficient magnitude and duration to cause the comparator to switch. Figure 6 illustrates the typical transient duration versus comparator overdrive (as a percentage of the trip threshold VRTx) required to trip the comparators.

Figure 6. Typical transient duration versus overdrive required to trip comparator.

The second filtering method, which is under user control (see next section), is the adjustment of the reset time-out period (tRST) or reset “delay time”. A capacitor (CRT) attached between the CRT pin and ground sets the reset time-out period. When any supply drops below its threshold, the reset line is brought low. The reset time-out counter starts once all inputs are back above threshold. The counter is cleared whenever any input drops back below threshold. A noisy input with frequency components of sufficient magnitude above f = 1/tRST effectively holds the reset line low, preventing oscillatory behavior on the reset line.

Although all four supply monitor comparators have built-in glitch filtering, bypass capacitors on V1 and V2 are recommended because the greater of V1 or V2 is also the VCC for the chip (a 0.1µF ceramic capacitor is satisfactory in most applications). Filter capacitors on the V3 and V4 inputs are allowed and recommended in extremely noisy situations.

User Adjustable Reset Time-Out Period

The reset time-out period (tRST) is adjustable in order to accommodate a variety of applications. The period is adjusted by connecting a capacitor, CRT, between the CRT pin and ground. The value of this capacitor is determined from:

Equation 1

with CRT in Farads and tRST in seconds. Maximum reset timeout is limited by the largest available low-leakage capacitor. The accuracy of the time-out period is affected by capacitor leakage and capacitor tolerance. To maintain timing accuracy, capacitor leakage must be well below the 2µA nominal charging current.

Reset Output Options and Individual Comparator Outputs

The reset output line is available in two styles, open-drain (LTC2900-1, LTC2901-1 and LTC2902-1) and push pull (LTC2900-2, LTC2901-2 and LTC2902-2). The open-drain output actually contains a weak pull-up current source to the V2 input, so an external pull-up resistor is only required when the output needs to pull to a higher voltage and/or when the reset output needs a fast rise time. The open-drain output allows for wired-OR connections and can be useful when more than one signal needs to pull down on the reset line. The non-delayed individual comparator outputs available on the LTC2901 and LTC2902 also have open-drain outputs with identical pull-up characteristics. When externally pulling up to voltages higher than V2, an internal network is automatically enabled to protect the weak pull-up circuitry from reverse currents.

The push-pull reset output has a much stronger active pull-up capability, also to the V2 input, resulting in a faster, low voltage drop pull-up characteristic. Wired-OR connections and/or external pull-ups are not recommended with the push-pull reset output option.

Ensuring Reset Valid for VCC down to 0V (LTC2900-2, LTC2901-2 and LTC2902-2)

Some applications require the reset output (RST) to be valid with VCC down to 0V. The LTC2900-2, LTC2901-2 and LTC2902-2 are designed to handle this requirement with the addition of an external resistor from RST to ground. The resistor will provide a path for stray charge and/or leakage currents, preventing the RST output from floating to undetermined voltages when connected to high impedance (such as CMOS logic inputs). The resistor value should be small enough to provide effective pull-down without excessively loading the active pull-up circuitry. Too large a value may not pull-down well enough. A 100k resistor from RST to ground is satisfactory for most applications.

Manual Reset Feature on the LTC2900

The manual reset or push-button reset pin (PBR) on the LTC2900 is used to issue a forced reset, typically with a normally-open pushbutton switch attached between PBR and ground. The PBR pin is pulled to VCC with an internal current source of 10µA (typical). The switch is debounced through the reset circuitry using the delay provided by the CRT timing capacitor. A logic low on this pin will pull RST low. When the PBR pin returns high, RST will return high after the reset time-out period has elapsed, assuming all four voltage inputs are above their thresholds. The PBR pin may also be driven by a logic signal. The input-high threshold on the PBR pin is 1.6V (max), allowing the pin to be driven by low-voltage logic. Figure 7 demonstrates a supervisory cascade using two LTC2900-2 ICs to monitor 8 voltages. The reset output of the first supervisor is tied to the PBR input of the second which holds the master reset low while the voltages on the first supervisor are below threshold. When all eight voltages are above threshold, the master reset is released after the delay provided by the second reset timing capacitor (CRTB).

Figure 7. Two supervisors cascaded to monitor eight voltages.

Independent Watchdog Features on the LTC2901

The LTC2901 contains independent watchdog circuitry consisting of a watchdog input (WDI), a watchdog output (WDO) and a timing pin (CWT) that allows for a user adjustable watchdog time-out period. An undervoltage condition on any supervisor input causes RST to go low which clears the watchdog timer and brings WDO high. The watchdog timer is started when RST pulls high. Subsequent rising or falling edges received on the WDI pin will clear the watchdog timer. If an edge is not received within the watchdog time-out period, WDO will go low. WDO will remain low and the watchdog timer will remain cleared until another edge is received on the WDI pin or another undervoltage condition occurs.

The watchdog function is typically used to monitor a processor’s activity. Consider a system that is no longer executing the correct code, thereby failing to issue an edge to the WDI pin. If the watchdog output is tied to a non-maskable interrupt (NMI), a watchdog timeout will cause the processor to vector to a new program location, which may enable a variety of recovery actions. For example, a motor could be disabled, an interlock could be engaged, critical data could be written to NVRAM, etc.

The watchdog time-out period (tWD) can be optimized for software execution. A capacitor (CWT) connected between the CWT pin and ground sets the watchdog time-out period. The capacitor value is determined from:

Equation 2

with CWT in Farads and tWD in seconds. Maximum timeout is limited by the largest available low-leakage capacitor. The accuracy of the time-out period is affected by capacitor leakage and capacitor tolerance. To maintain timing accuracy, capacitor leakage must be well below the 2µA nominal charging current.

The watchdog circuit can also be used as a clock or frequency monitor by applying a periodic logic signal to the WDI input. If the input signal is inactive for an amount of time longer than the watchdog time-out period, the WDO line falls, indicating a loss of the periodic input. Figure 8 demonstrates how the LTC2901 can be used to monitor a switching regulator’s activity. In this application, the 3.3V input, 1.8V output and feedback voltage to the LTC1772 regulator are supervised. Furthermore, if the load goes open circuit, the LTC1772 switches into Burst Mode® operation, reducing the duty cycle at the gate of M1. The pulse spacing exceeds the watchdog time-out period, and the watchdog output falls indicating the low-load condition.

Figure 8. Use the LTC2901-2 to monitor the input, output, feedback voltage and low load conditions on a DC/DC controller. In this case, the controller is an LT1772 used in a 3.3V input to 1.8V output application.

Power Supply Margin Testing with the LTC2902

In high reliability system manufacturing and test, it is desirable to verify the correct operation of electrical components at or below the rated power supply tolerance. The LTC2902 is designed to complement such testing in two ways. First, the reset disable pin (RDIS) can be pulled low which forces the RST output high. With RDIS low, moving supply voltages below threshold does not invoke the reset command during margining tests. The individual comparator outputs operate normally with RDIS high or low, allowing for individual supply monitoring.

The second way allows the user to provide more supply headroom by lowering the trip thresholds. Using the digital tolerance programming inputs (T0, T1), the global supply tolerance can be set to 5%, 7.5%, 10%, or 12.5% (Table 3).

Table 3. LTC2902 Tolerance Programming
T0 T1 Tolerance VREF
Low Low 5% 1.210V
Low High 7.5% 1.178V
High Low 10% 1.146V
High High 12.5% 1.113V

When using the positive or negative adjustable inputs in conjunction with tolerance programming, external resistors need only to be sized once, based on a 5% tolerance threshold. Once the external resistor dividers are set using the 5% tolerance thresholds, the thresholds for the other tolerance modes (7.5%, 10%, 12.5%) are automatically correct because the reference voltage (VREF) is scaled accordingly. Figure 9 shows how the LTC2902 can be configured for asymmetric hysteresis, having 5% tolerance when supplies are rising and 12.5% tolerance after all supplies have safely crossed their 5% thresholds.

Figure 9. Quad supply monitor with asymmetric hysteresis.

Conclusion

One part can now satisfy most present and future supervisory needs. The LTC2900, LTC2901 and LTC2902 micropower quad supervisors provide the versatility, accuracy and reliability required in multi-voltage monitoring applications. Input supply combinations are programmable including positive and/or negative adjustable thresholds. The comparators are 1.5% accurate over temperature and feature built-in noise rejection. Reset logic is correct for VCC down to 1V, and is available with open-drain or push-pull outputs. Reset and watchdog times are user adjustable with external capacitors. Power supply margining features include real-time supply tolerance selection and an on-demand reset disable pin.

关于作者

Bob Jurgilewicz
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目

关联至此文章

产品

最新视频 21
Title
Subtitle
了解更多
添加至 myAnalog

将文章添加到 myAnalog 的资源部分、现有项目或新项目。

创建新项目