概览

优势和特点

  • 用于评估的完整ADRV9026无线电卡
    • ADRV9026-HB/PCBZ,适用于2.8GHz至6GHz频段
    • ADRV9026-MB/PCBZ,适用于650MHz至2.8GHz频段
    • ADRV9026-LB/PCBZ,适用于75MHz至1000MHz频段
  • 用于评估的完整ADRV9029无线电卡
    • ADRV9029-HB/PCBZ(集成DPD和CFR),适用于2.8GHz至6GHz频段
    • ADRV9029-MB/PCBZ(集成DPD和CFR),适用于650MHz至2.8GHz频段
  • 4x4宽带RF收发器平台,工作频率范围650MHz至6GHz
  • 独立的电源子卡提供了高效率电源解决方案参考设计
  • 通过FMC连接器连接FPGA母板ADS9-V2EBZ
  • 包括原理图、布局、BOM、API和评估软件

产品详情

ADRV9029和ADRV9026无线电卡设计用于展示ADRV9026(四通道宽带RF收发器)和ADRV9029(集成DPD和CFR的四通道宽带RF收发器)。无线电卡提供一个4x4收发器平台用于器件评估。无线电卡工作所需的全部外设包括一个独立的高效率电源电路板和一个高性能时钟解决方案,它们均已安装在无线电板上。通过FMC连接器将其中一个无线电卡与FPGA主板ADS9-V2EBZ连接,形成ADRV9026和ADRV9029的完整评估平台。ADRV9026评估套件可用于评估ADRV9010的性能。

Radioverse

技术与领域

相关产品

包装内含

  • 一个集成FMC连接器的ADRV9026-HB/PCBZ、ADRV9026-MB/PCBZ、ADRV9026-LB/PCBZ、ADRV9029-HB/PCBZ或ADRV9029-MB/PCBZ无线电卡
  • 一个12V壁式连接器电源电缆

注:该封装不含工作所需的ADS9-V2EBZ母板,此母板必须单独订购。请使用ADS9 EVB套件(TRX)中包含的其中一个16GB Micro SD卡来启动基于Windows的ADRV9026或ADRV9029 GUI。

软件

评估软件

ADRV9026 Released Software SW6.4.0.19
The ADRV9026 software package contains the GUI software, the API source code, the firmware file, and the gain tables. The GUI software enables transceiver testing using the evaluation board and the Windows GUI. The API source code is intended for use in a customer system and can be integrated with the rest of the customer code and compiled for the target system. The firmware file in binary format is used by the ARM® processor on the transceivers. The gain tables include the receiver gain tables and transmitter attenuation table. Note that the files within the zip must be used together. For example, the ARM files from one zip file cannot be used with the API files from another version.
ZIP
2481 M
ADRV9026/ADRV9029 - SDCARD
The ADRV9026-SDCARD included with the evaluation kit was up to date at the time of packaging the kit. If an update is necessary, the user will be prompted to update the image when connecting to the GUI. If the card does not function properly or users would like to create their own SD card, this image file can be downloaded and used to write a new card or overwrite the ADRV9026-SDCARD included with the evaluation kit. To program a card using this image, follow the programming instructions after downloading the image to a local drive. Note that a 16 GB minimum SD card is required when programming a new card.
PDF
584.37 K
ADRV9026/ADRV9029 Release Build Software Release Notes SW6.4.0.19
The SW6.4.0.19 RELEASE build provides updates in the ARM firmware, stream files, API, and GUI software to support ADRV9026/ADRV9029.

设计工具

ZIP
13.85 M
ADRV9026/ADRV9029 Design File Package (Last Updated 10/2021)
The Design File Package includes the eval board schematics, BOM, layout, IBIS, BSDL models, JCOM models, S-parameters Material Declaration, and Symbols and Footprints.

硬件 (1)

开发平台

在线购买

所示报价为单片价格

以上评估板报价仅供人民币结算及大陆购买使用, ADI均提供正规发票,如需美金结算及其他地区购买请直接跳转至英文页面进行购买。