The circuit, shown in Figure 1, is a complete analog front end for digitizing ±10 V industrial level signals with a 16-bit differential input PulSAR® ADC. The circuit provides a high impedance instrumentation amplifier input with high CMR, level shifting, attenuation, and differential conversion, with only two analog components. Because of the high level of integration, the circuit saves printed circuit board space and offers a cost effective solution for a popular industrial application.
Signal levels of up to ±10 V are typical in process control and industrial automation systems. With smaller signal inputs from sensors such as thermocouples and load cells, large commonmode voltage swings are often encountered. This requires a flexible analog input that handles both large and small differential signals with high common-mode rejection and also has a high impedance input.
|
|
Figure 1. High Performance Analog Front for Industrial Process Control (Simplified Schematic: All Connections and Decoupling Not Shown)
|
Attenuation and level shifting are necessary to process industrial level signals with modern low voltage ADCs. In addition, fully differential input ADCs offer the advantages of good common-mode rejection, reduction in second-order distortion products, and simplified dc trim algorithms. Industrial signals, therefore, need further conditioning to properly interface with differential input ADCs.
The circuit in Figure 1 is a complete and highly integrated analog front end industrial level signal conditioner that uses only two active components to drive an AD7687 differential input 16-bit PulSAR ADC: the AD8295 precision in-amp (with two on-chip auxiliary op amps) and the AD8275 level translator/ADC driver. An ADR431 low noise 2.5V XFET® reference supplies the voltage reference for the ADC.
The AD8295 is a precision instrumentation amplifier with two uncommitted on-chip signal processing amplifiers and two precisely matched 20 kΩ resistors in a small 4 mm × 4 mm package.
The AD8275 is a G = 0.2 difference amplifier that can be used to attenuate ±10 V industrial signals, and the attenuated signal can be easily interfaced to a single supply low voltage ADC. The AD8275 performs the attenuation and level shifting function in the circuit, maintaining good CMR without any need for external components.
The AD7687 is a 16-bit, successive approximation ADC that operates from a single power supply between 2.3 V and 5.5 V. It has a differential input for good CMR and also offers the ease of use associated with SAR ADCs.
The circuit is comprised of the AD8295 and AD8275 as the analog front end circuit, an AD7687 ADC with an ADR431 reference, and only a few other external components for decoupling, etc.
Instrumentation Amplifier (Integrated into the
AD8295)
The instrumentation amplifier (IA) integrated into the
AD8295 is set for a gain-of-one as the operating condition.
For applications where higher gain is required, an appropriate
external gain resistor can be added. The power supply of the
AD8295 is ±15 V, which allows for the full ±10 V industrial
input signal level. The reference pin of the in-amp connects to
ground, thereby making the output of the AD8295 ground
referenced.
Difference Amplifier/Attenuator (
AD8275)
The signal at the output of the AD8295 in-amp is single-ended
with a maximum amplitude of ±10 V. This signal must be
attenuated and level shifted to the proper level to drive the
AD7687 ADC. A simple resistive level attenuator stage directly
on the output of AD8295 would not provide a differential output to drive the ADC. The AD8275 (G = 0.2) level translator
is a difference amplifier with matched on-chip precision lasertrimmed
thin film resistors to ensure low gain error, low gain
drift (1 ppm/℃ maximum), and high common-mode rejection
(80 dB). The AD8275 has a wide power supply range from
+3.3 V to +15 V, as well as a large input voltage range from
−12.3 V to +12 V when operating on a single +5 V power supply.
Driving the Differential Input ADC
The circuit in Figure 1 uses a balanced difference amplifier
composed of the AD8275 (U2) and one of the uncommitted op
amps (U1-C) in the AD8295. This op amp (U1-C) is used to
invert the positive output of the AD8275 (thereby providing a
complementary negative output) and drive the REF1 and REF2
pins of the AD8275. The output common-mode voltage of the
differential output (VCOM = 1.25 V) is developed from the
10 kΩ external resistor divider connected to the 2.5 V reference
and is applied to the noninverting input of U1-C. The equations
describing the circuit operation are as follows:
VOUTP + VOUTN = 2 × VCOM
VOUTP = VOUTN + 0.2 × VIN
VOUTP = VCOM + 0.1 × VIN
VOUTN = VCOM − 0.1 × VIN
From the equations, with a ±10 V input voltage, the voltages to the ADC (VOPTP and VOUTN) will each swing between 0.25 V and 2.25 V, 180° out of phase with respect to each other, with a common-mode voltage of 1.25 V. The differential signal, therefore, utilizes 4 V out of the 5 V available differential input range of the ADC.
The ADR431 is a 2.5 V reference in a family of XFET voltage references featuring low noise, high accuracy, and low temperature drift performance. The ADR431 drives the resistor divider and the reference input of the AD7687 ADC. The ADR431output is buffered by the second uncommitted op amp (U1-B) in the AD8295 and drives the power supply (VDD) of the AD7687. A single-pole RC filter composed of two 33 Ω resistors and a 1.5 nF capacitor serves as a 3 MHz cutoff antialiasing and noise reduction filter for the AD7687.
Layout Considerations
The performance of this or any other high speed or high
resolution circuit is highly dependent on proper PCB layout.
This includes, but is not limited to, power supply bypassing,
signal routing, and proper power planes and ground planes. See
Tutorial MT-031, Tutorial MT-101, and the article A Practical
Guide to High-Speed Printed-Circuit-Board Layout for more
detailed information regarding PCB layout.
|
|
Figure 2. FFT with a Kaiser Window (Parameter = 20), 20 kHz Input, 250 kSPS Sampling Rate
|
System Performance
The ac performance was tested at the system level with the
AD7687 sampling at 250 kSPS. Figure 2 shows an FFT test
result with a 5 V p-p 20 kHz input. Figure 3 shows a histogram
of the ADC output with a 10 V dc input.
The results generated from the evaluation software are as follows:
|
|
Figure 3. DC Histogram for a 10 V Input, 15,000 Samples
|
Other pin-compatible differential input 16-bit ADCs in the PulSAR family are available at different sampling rates: AD7684 (100 kSPS), AD7688 (500 kSPS), and AD7693 (500 kSPS).
If 18-bit resolution is needed, the following are also pin-compatible members of the PulSAR family: AD7691 (250 kSPS), AD7690 (400 kSPS), and AD7982 (1 MSPS).
The reference for the ADC can be changed to the ADR430, which is 2.048 V. This makes use of a larger percentage of the input range of the ADC; however, an additional AVDD power supply for the AD7687 is required.
The circuit uses the EVAL-CN0225-SDPZ circuit board and the EVAL-SDP-CB1Z System Demonstration Platform (SDP) evaluation board. The two boards have 120-pin mating connectors, allowing for the quick setup and evaluation of the circuit’s performance. The EVAL-CN0225-SDPZ board contains the circuit to be evaluated, as described in this circuit note, and the SDP evaluation board is used with CN0225 evaluation software to capture the data from the EVAL-CN0225-SDPZ circuit board.
Equipment Needed
Getting Started
Load the evaluation software by placing the CN0225 Evaluation
Software disc in the CD drive of the PC. Then locate the drive
that contains the evaluation software disc and open the Readme
file. Follow the instructions contained in the Readme file for
installing and using the evaluation software.
Functional Block Diagram
Figure 4 shows a functional block diagram of the test setup. The
PDF file “EVAL-CN0225-SDPZ-SCH” has the detailed
schematics for the CN0225 evaluation board. This file is
contained in the CN0225 Design Support Package:
www.analog.com/CN0225-DesignSupport.
|
|
Figure 4. Test Setup Functional Block Diagram
|
Setup
Connect the 120-pin connector on the EVAL-CN0225-SDPZ
circuit board to the connector marked “CONA” on the
EVAL-SDP-CB1Z evaluation (SDP) board. Nylon hardware
should be used to firmly secure the two boards, using the
holes provided at the ends of the 120-pin connectors. After
successfully setting the dc output supply to +15 V, -15 V and
+6 V output, turn the power supply off.
With power to the supply off, connect a +15 V power supply to the pin of J3 marked “+15VA” and a −15 V power supply to the pin of J3 marked “−15VA” and “GND” to the pin of J3 marked “AGND”. Connect +6 V to J2 in the same manner. Turn on the power supply and then connect the USB cable with the SDP board to the USB port on the PC. Note: Do not connect the USB cable to the mini USB connect on the SDP board before turning on the dc power supply for the EVAL-CN0225-SDPZ.
Test
After setting up the power supply and connecting it to the
EVAL-CN0225-SDPZ circuit board, launch the evaluation
software and connect the USB cable from the PC to the USB
mini-connector on the SDP board. The software will be able to
communicate to the SDP board if the Analog Devices System
Development Platform driver is listed in the Device Manager.
Once USB communications are established, the SDP board can be used to send, receive, and capture serial data from the EVAL-CN0225-SDPZ board.
The data in this circuit note was generated using an Agilent 81150A differential signal source
Information regarding the SDP board can be found at www.analog.com/SDP.