AN-1576: Low Jitter Sampling Clock Generator for High Performance ADCs Using the AD9958 500 MSPS DDS or the AD9858 1 GSPS DDS and the AD9515 Clock Distribution IC
Circuit Function and Benefits
This circuit uses a direct digital synthesizer (DDS) with subHertz tuning resolution as a low jitter sampling clock source for high performance analog-to-digital converters (ADCs). The AD9515 clock distribution IC provides positive emitter-coupled logic (PECL) logic levels to the ADC. However, the AD9515 internal divider feature also allows the DDS to run at a higher frequency into the AD9515 front-end, effectively increasing input slew rate. A higher slew rate into the AD9515 input squaring circuit can help reduce broadband jitter in the clock path.
Jitter on the ADC sampling clock produces degradation in the overall signal-to-noise ratio (SNR).
The relationship is given by the following equation:

where:
SNR is the signal-to-noise ratio due solely to clock jitter and does not depend on the resolution of the ADC.
f is the full-scale analog input frequency.
tj is the rms jitter.
The data in this application note supports low jitter that can be attained from a DDS in clocking applications. See the Application Note AN-501 for details on Equation 1 and its use for evaluating the jitter on ADC sampling clocks.
Circuit Description
The circuit configuration in Figure 1 shows a DDS-based clock generator, which consists of DDS followed by a reconstruction filter and an AD9515 clock distribution IC that are used to provide the sampling clock for an ADC. The DDS sampling clock is derived from a Rohde and Schwarz SMA signal generator. The jitter measurement was made by using the clock derived from the DDS and the AD9515 as the sampling clock for the high performance AD6645 14-bit, 80 MSPS/105 MSPS ADC. The analog input signal for the ADC is a filtered 170.3 MHz sine wave derived from a low jitter Wenzel crystal oscillator. Data was taken on the AD9958 (500 MSPS) and the AD9858 (1 GSPS).
By evaluating the contribution of the differential non-linearity (DNL) and thermal noise of the ADC and then applying the DDS-based clock and measuring the ADC SNR, the added jitter that can be attributed to the DDS-based clock can be derived. For details on the measurement setup and the jitter calculations, refer to the Application Note AN-823. Additionally, the Application Note AN-837 is instructive for designing DAC reconstruction filters with optimal stop band performance.
Table 1 shows data for the AD9958 test results. The data confirms that better jitter performance is achieved as the frequency, or slew rate, of the DDS output frequency (fOUT) is increased and the DDS output filter pass band is decreased. Table 2 shows the AD9858 with a 5% band-pass filter, a 225 MHz low-pass filter, and various levels of DDS output power. As expected, lower jitter is achieved as power is increased and the bandwidth is reduced. When using a 5% band-pass filter, the majority of the spurs from the DAC are attenuated. The jitter in this case is much more dependent on noise coupling between the digitalto-analog converter (DAC) output and the limiter input. This dependency is proven by the strong correlation between jitter reduction and increased slew rate. Note that rms jitter values that are consistently <1 ps can be achieved using the AD9858 circuit.
| DDS Sample Rate (MHz) |
DDS Output Frequency (MHz) |
DDS Output Power (dBm) |
DDS Reconstruction Filter |
AD9515 Divider Output Setting |
AD9515 fOUT (MHz) |
Jitter rms (ps) |
| 500 | 38.88 | −3.6 | 200 MHz, low-pass | 1 | 38.88 | 4.1 |
| 500 | 38.88 | −3.6 | 200 MHz, low-pass | 2 | 19.44 | 4.1 |
| 500 | 38.88 | −4.7 | 47 MHz, low-pass | 1 | 38.88 | 2.4 |
| 500 | 38.88 | −4.7 | 47 MHz, low-pass | 2 | 19.44 | 2.4 |
| 500 | 38.88 | −3.3 | 5%, band-pass | 1 | 38.88 | 1.5 |
| 500 | 38.88 | −3.3 | 5%, band-pass | 2 | 19.44 | 1.5 |
| 500 | 77.76 | −3.8 | 200 MHz, low-pass | 1 | 77.76 | 2.5 |
| 500 | 77.76 | −3.8 | 200 MHz, low-pass | 2, 4 | 38.88, 19.44 | 2.5 |
| 500 | 77.76 | −4.9 | 85 MHz, low-pass | 1 | 77.76 | 1.5 |
| 500 | 77.76 | −4.9 | 85 MHz, low-pass | 2, 4 | 38.88, 19.44 | 1.5 |
| 500 | 77.76 | −3.8 | 5%, band-pass | 1 | 77.76 | 1.1 |
| 500 | 77.76 | −3.8 | 5%, band-pass | 2, 4 | 38.88, 19.44 | 1.1 |
| 500 | 155.52 | −5.5 | 200 MHz, low-pass | 2 | 77.76 | 1.5 |
| 500 | 155.52 | −5.5 | 200 MHz, low-pass | 4, 8 | 38.88, 19.44 | 1.5 |
| 500 | 155.52 | −5.6 | 5%, band-pass | 2 | 77.76 | 0.68 |
| 500 | 155.52 | −5.6 | 5%, band-pass | 4, 8 | 38.88, 19.44 | 0.68 |
| DDS Sample Rate (MHz) |
DDS Output Frequency (MHz) |
DDS Output Power (dBm) |
DDS Reconstruction Filter |
AD9515 Divider Output Setting |
AD9515 fOUT (MHz) |
Jitter rms (ps) |
| 1000 | 155.52 | 7.7 | 225 MHz, low-pass | 2 | 77.76 | 0.56 |
| 1000 | 155.52 | 7.7 | 225 MHz, low-pass | 4,8 | 38.88, 19.44 | 0.56 |
| 1000 | 155.52 | 7.7 | 5%, band-pass | 2 | 77.76 | 0.33 |
| 1000 | 155.52 | 7.7 | 5%, band-pass | 4,8 | 38.88, 19.44 | 0.33 |
| 1000 | 155.52 | 2.6 | 225 MHz, low-pass | 2 | 77.76 | 0.63 |
| 1000 | 155.52 | 2.6 | 225 MHz, low-pass | 4,8 | 38.88, 19.44 | 0.63 |
| 1000 | 155.52 | 1.1 | 5%, band-pass | 2 | 77.76 | 0.42 |
| 1000 | 155.52 | 1.1 | 5%, band-pass | 4,8 | 38.88, 19.44 | 0.42 |
| 1000 | 155.52 | −3.2 | 225 MHz, low-pass | 2 | 77.76 | 0.73 |
| 1000 | 155.52 | −3.2 | 225 MHz, low-pass | 4,8 | 38.88, 19.44 | 0.73 |
| 1000 | 155.52 | −4.6 | 5%, band-pass | 2 | 77.76 | 0.64 |
| 1000 | 155.52 | −4.6 | 5%, band-pass | 4,8 | 38.88, 19.44 | 0.64 |
These circuits must be constructed on multilayer printed circuit boards (PCBs) with large area ground planes using proper grounding, layout, and decoupling techniques (see MT-031 Tutorial, Grounding Data Converters and Solving the Mystery of “AGND” and “DGND” and MT-101 Tutorial, Decoupling Techniques) to achieve these performance levels. Consult the evaluation board documentation for the EVAL-AD9958, EVAL-AD9858, EVAL-AD9515, and the EVAL-AD6645 for more guidance.
Common Variations
Analog Devices, Inc., offers a variety of direct digital synthesizers, clock distribution chips, and clock buffers to build a DDS-based clock generator. Refer to the Direct Digital Synthesis page and the Clock & Timing page on the Analog Devices website for more information.