Sigma-Delta Modulators Improve Motion Control Efficiency
Industrial motion control covers a breadth of applications, ranging from inverter-based fan or pump control, to factory automation with more complex ac drive control, to advanced automation applications such as robotics with sophisticated servo control. These systems require sensing and feedback of a number of variables, such as motor winding current or voltage, dc link current or voltage, rotor position, and speed. The selection of variables and the required measurement precision depend on the end application demands, the system architecture, target system cost, or system complexity. There are other considerations, such as value add features like condition monitoring. With motors reportedly consuming 40% of worldwide electric power, international regulations have increased the focus on system efficiency across the entire range of industrial motion applications (see Figure 1).

Figure 1. Industrial drive application spectrum.
Current and voltage sensing techniques in various motor control signal chain topologies vary according to motor power rating, system performance requirements, and end application. In this context, motor control signal chain implementations differ by sensor choice, galvanic isolation requirements, ADC choice, system integration, and system power/ground partitioning. While isolation requirements usually have a significant influence on the resulting circuit topology and architecture, this article will focus on improving current sensing measurements (as one contributing element) to realize a more efficient motor control system.
I and V Measurement
A generic motor control signal chain is shown in Figure 2. Signal conditioning to realize a high fidelity measurement is not trivial. Phase current sensing is particularly challenging, as this node is connected to the same circuit node as the gate driver output within the heart of the inverter block and therefore experiences the same demands, in terms of isolation voltages and handling switching transients.

Figure 2. Generic motor control signal chain.
The most commonly used current sensors in motor control are shunt resistors, Hall effect sensors (HES), and current transformers (CTs). While shunt resistors don’t provide isolation and incur losses, they are the most linear of all the sensors, the lowest cost, and suitable for both ac and dc measurements. The signal level reductions needed to limit shunt power losses typically limit shunt applications to 50 A or less. CTs and HESes provide inherent isolation, allowing them to serve high current systems, but they are higher cost and result in a less accurate solution than what can be achieved with a shunt resistor, either due to poorer initial accuracy or worse accuracy over temperature. Apart from the sensor type, there are several motor current measurement nodes to choose from (as shown in Figure 3) with direct in-phase winding measurement being the ideal and used in the highest performance systems.

Figure 3. Isolated and nonisolated motor current feedback.
There are many topologies to sense motor current with many factors to consider, such as cost, power, and performance levels, but a key objective for most system designers is to improve efficiency within their cost targets.
From HES to Shunt Resistors
Shunt resistors coupled with isolated Σ-Δ (sigma-delta) modulators provide the highest quality current feedback (where the current level is low enough). There is a significant trend for system designers to migrate from HESes to shunt resistors, with an additional trend to move to the isolated modulator vs. an isolated amplifier approach. Quite often, system designers replacing HESes with shunt resistors opt for an isolated amplifier and continue using the ADC previously used in the HES-based design. In that case, the performance will be limited by the isolated amplifier regardless of the analog-to-digital performance.
Replacing the isolated amplifier and ADC with an isolated Σ-Δ modulator will eliminate the performance bottleneck and greatly improve the design—typically taking it from a 9-bit to 10-bit quality feedback to a 12-bit level. Analog overcurrent protection circuitry (OCP) can also potentially be eliminated, as the digital filter required to process the Σ-Δ modulator output can also be configured to implement a fast OCP loop.
Available Σ-Δ modulators may have a differential input range of ±250 mV, with ±320 mV full scale used for OCP, which is well suited to resistive shunt measurements. The analog input is continuously sampled by the analog modulator and the input information is contained in the digital output stream with a data rate up to 20 MHz. The original information can be reconstructed with an appropriate digital filter. As conversion performance can be traded off vs. bandwidth or filter group delay, a coarser, faster filter can provide fast response OCP in the order of 2 µs, ideally suited to IGBT protection.
Reduce Shunt Resistor Sizes
From a signal measurement standpoint, there are some key challenges associated with the shunt resistor selection, as there is a trade-off between sensitivity and power dissipation. Nonlinearity due to self heating effects can also be a challenge using higher value resistors. Designers are faced with making trade-offs, and further exacerbating this is a common need to select a shunt size that will service many models and motors at different current levels. Maintaining dynamic range is a challenge in the face of peak currents that can be several times the rated current of the motor and the need to reliably capture both.
In the face of these challenges, system designers are looking for superior Σ-Δ modulators with wider dynamic range or improved signal-to-noise-and-distortion ratio (SINAD). Isolated Σ-Δ modulator offerings to date have provided 16-bit resolution with up to 12-bit effective number of bits (ENOB) guaranteed performance.
High Performance Isolated Σ-Δ Modulator
A higher performance isolated Σ-Δ modulator would support several needs in industrial motor control designs and improve power efficiency of motor drives through shunt resistor size reduction. One industry example is the AD7403 modulator from Analog Devices (see Figure 4). It is the next-generation product to the AD7401A, providing much wider dynamic range at the same external clock rate of 20 MHz. It allows more flexible shunt size selection and allows for shunt resistor usage in place of HESes at higher current levels. The chip’s ENOB is typically 14.2 bits. Dynamic response can also be improved through reduced measurement latency. The device also features an isolation scheme with a higher continuous working voltage (VIORM) than the previous generation, which can contribute to higher system efficiency via higher dc bus voltages and lower currents.

Figure 4. The AD7403 a high performance, second-order Σ-Δ modulator
System Solutions with the ADSP-CM40x Mixed-Signal Control Processor
As noted, the implementation of a Σ-Δ modulator requires a digital filter. This is traditionally implemented with an FPGA or ASIC. The advent of the ADSP-CM408F mixed-signal control processor from Analog Devices will alleviate that design problem as it includes hardware sinc filters to which the modulators can directly connect. This is likely to lead to an increased rate of adoption of the resistive shunt and Σ-Δ modulator technique.
About the Authors
{{modalTitle}}
{{modalDescription}}
{{dropdownTitle}}
- {{defaultSelectedText}} {{#each projectNames}}
- {{name}} {{/each}} {{#if newProjectText}}
-
{{newProjectText}}
{{/if}}
{{newProjectTitle}}
{{projectNameErrorText}}