Display Different LED Sequences Using the MAXQ2000 Microcontroller with the MAX6970 LED Driver

Feb 21 2023

Overview

The MAX6970 is an 8-port, 36V constant-current LED driver that uses a 4-wire serial interface. Using this application note, the MAX6970 can be used with the MAXQ2000 16-bit RISC microcontroller to create a variety of simple LED sequences with the touch of a button.

Hardware Setup

The circuit discussed in this application note utilizes the MAX6970EVKIT and the MAXQ2000-KIT. The MAX6970 evaluation (EV) kit schematic is shown in Figure 1. A MAXQ2000 EV kit board is included in the MAX6970 EV kit design. However for this application, it will be detached from the on-board MAXQ2000, since the MAXQ2000 EV kit has pushbutton features that would otherwise be used to control the LED sequences.

Figure 1. MAX6970EVKIT schematic

Figure 1. MAX6970EVKIT schematic

Related to this Article

Products

Resources

Latest Media 21

Subtitle
Learn More