signals header
Large cellular base station tower with multiple antennas against a city skyline, representing 5G network deployment.
Large cellular base station tower with multiple antennas against a city skyline, representing 5G network deployment.
 

SIGNALS+ NEWSLETTER SUBSCRIPTION

Stay updated and leverage Signals+ latest insights, information and ideas on Connectivity, Digital Health, Electrification, and Smart Industry.

By clicking “Subscribe”, you consent to receive marketing communications from Analog Devices, Inc. and its subsidiaries and agree to our Privacy Policy. Unsubscribe any time in your Privacy Settings.

Thank you for subscribing to ADI Signals+. A confirmation email has been sent to your inbox.

You'll soon receive timely updates on all the breakthrough technologies impacting human lives across the globe. Enjoy!

Close

Navigating the Rising Complexity of 5G and 6G Radio Design

February 10, 2026

The race toward 6G is accelerating. However, it also brings a challenge that could hinder or slow progress: the increasing complexity of radio design. Today, mobile operators are under pressure to deliver faster, more flexible networks while reducing costs and energy consumption. Shared infrastructure and expanding band requirements are reshaping the industry, demanding radios that can do more with less.

Panoramic city skyline at dusk with illuminated buildings and digital network lines representing wireless connectivity.

How can vendors and operators simplify design, accelerate deployment, and secure the future of mobile networks in an era where increased complexity is the new normal?

Why Complexity Is Exploding

The progression from 5G into the 6G era isn’t just about speed—it’s about the increasing need for more capable radio unit designs. Today, operators manage a growing number of frequency bands across sub-6 GHz and beyond. They’re deploying radios for macro sites, small cells, and distributed antenna systems (DAS), often in shared environments where multiple operators use the same hardware. This trend toward shared infrastructure improves efficiency but introduces additional complexity in radio design by combining multiple bands into a single radio unit.

Traditionally, building a new radio could take 18 to 24 months. With the proliferation of additional bands and configurations, these timelines are stretching even further. For vendors, this means higher development costs and longer time to market. For operators, it means slower rollouts and delayed revenue. Complexity is increasingly a bottleneck—and the industry needs a viable solution.

Meeting the Challenge for the Next Generation of Radios

Operators and vendors must rethink radio design to meet the needs of tomorrow’s 6G world. The requirements include:

  • Simpler Design: Integration hurdles have historically slowed development. Simplifying these processes is essential.
  • Faster Build Cycles: Time to market is critical as competition intensifies, and operators prepare to refresh their networks.
  • Flexibility and Programmability: Radios must support multiple bands, configurations, and applications without requiring new hardware for every variant.
  • Universal Radios: A single small-signal platform should serve diverse applications—from macro sites to DAS—reducing the need for multiple core radio designs.
  • Energy Efficiency: Lower power consumption is no longer optional; it’s a mandate for sustainability and cost control.
  • Security Built-In: Zero-trust environments and secure boot are industry standards that must be met.
  • Market Diversity and O-RAN: Open architectures are key to expanding the vendor ecosystem and fostering innovation.
  • Future-Proofing: As 6G approaches, radios must be ready for even more complex requirements, including AI-driven features and advanced network awareness.

Collaboration and Innovation Are Key

Meeting these needs requires more than just small or incremental improvements. It calls for collaboration between operators, vendors, and semiconductor leaders. Open RAN demonstrates that the industry is shifting toward increased flexibility and market diversity. By adhering to standard interfaces across the network, O-RAN enables operators to source radios from a broader ecosystem, expanding the diversity of radio units available for their networks.

For many companies with 5G, the partnership has advanced to a multi-operator RAN (MORAN) model—sharing infrastructure while maintaining separate spectrum for each operator. This approach delivers impressive results: two companies report 30% to 35% lower capital expenditures and 25% to 30% lower operating costs compared to building standalone networks. Most importantly, it enables 5G coverage for more than 75% of the population—accelerating access to next-generation connectivity.1 2

Innovation at the component level is equally important. Features like AI-driven digital pre-distortion (DPD) and passive intermodulation (PIM) cancellation are helping radios deliver better performance across multiple bands. But these features can add complexity and increase energy consumption—unless they are integrated intelligently.

Samana: Integration That Simplifies

Analog Devices ADRV906x radioverse system-on-chip shown from top and bottom, used for advanced wireless communications.
Figure 1: ADRV906x RU Titan reference design.

Analog Devices, Inc. (ADI) Samana chip illustrates how integration can address complexity without sacrificing capability. By combining the transceiver, digital front-end processing functions, and network connectivity into a single device, Samana eliminates the need for an FPGA—an incremental processor that typically consumes 30 W to 40 W. This integration not only reduces power and cost but also eases the design by simplifying the board layout and network integration while removing timing challenges that often slow development.

Beyond integration, Samana addresses the market challenges by incorporating features such as Zero Trust and MACSec for security, and enhanced power savings to address operators’ OPEX, cost, and simplicity, and reducing customers’ time to market. Although not the only viable option on the market, Samana exemplifies the innovation the industry needs: solutions that reduce complexity while expanding flexibility and scalability.

Preparing for 6G

As the industry advances toward 6G, complexity will continue to increase. Multi-band, multi-operator radios will become the norm, and AI-driven features will be essential for optimizing performance and network capacity. At the same time, sustainability goals will demand lower energy footprints, and security requirements will only tighten.

Vendors and operators must find ways to do more with less—creating radios that are easier to design, quicker to produce, and simpler to adopt. It involves leveraging architectures that offer flexibility without more complexity. It also emphasizes prioritizing energy efficiency and security from the outset to help create a more sustainable planet.

Simplicity: The Ultimate Advantage

Reducing complexity while adding flexibility is a strategic imperative for the mobile industry. Simplifying the design process accelerates deployment, lowers costs, and enables further innovation. Flexible, programmable radios enable operators to adapt quickly to changing spectrum and service requirements. Together, these capabilities will define success in the 5G-to-6G era.

Cellular communication tower overlooking a modern city, symbolizing mobile network infrastructure.

Solutions like ADI’s Samana highlight what’s possible when integration meets innovation. However, the future of mobile networks also depends on collaboration, creativity, and an uncompromising focus on simplicity. In an industry where complexity is the new normal, simplicity may be the ultimate competitive advantage.

References

1 “Managed Service Model for a MORAN Shared Network.” Omnitele.
2 “Operators View Cost Saving and Coverage as the Two Main Drivers for Network Sharing.” Analysys Mason, May 2023.