Common-Mode Transient Immunity

Feb 3 2020

Figure 1

   

Common‐Mode Transient Immunity (CMTI) is one of three key characteristics associated with isolators such as iCoupler digital isolators as well as optocouplers. The other key characteristics are isolation rating and working voltage. This article discusses how ADI measures CMTI for our transformer‐based iCoupler digital isolators and shows comparisons to competing digital isolators based on capacitors.

CMTI is important because high‐slew‐rate (high‐frequency) transients can corrupt data transmission across the isolation barrier. Understanding and measuring the susceptibility to these transients is critical. The capacitance across the barrier (i.e., between the isolated ground planes) provides the path for these fast transients to cross the isolation barrier and corrupt the output waveform.

Figure (1) shows a typical setup for performing the CMTI test of a 4‐channel digital isolator. During CMTI testing, a pulsed transient is applied across the isolated ground planes and the outputs of the device are monitored for data disruptions. The key characteristic of this transient is its slew rate. In the case shown in Figure 1, a transient pulse is applied to the ground on the left‐hand side of the isolation barrier while the outputs of the DUT on the right hand side of the barrier are monitored. The CMTI test is performed for both positive and negative transients and is also done with the inputs of the DUT tied both HIGH and LOW.

Figure 1 : Typical CMTI Setup of a 4‐Channel Digital Isolator.

Transformer‐Based Isolation vs. Capacitor‐Based Isolation

The ADuM1402, 4‐channel digital isolator from ADI relies on a transformer based isolation method and uses on‐chip, air‐core transformers to provide the isolation barrier. The primary and secondary coils are separated by a thick polyimide layer that provides thousands of volts of isolation. Through inductive coupling and a changing magnetic field between the two coils of the transformer, data is transmitted across the isolation barrier.

An alternative to transformer‐based isolation employs capacitors for both isolation and data transmission across the isolation barrier. The dielectric material between the capacitor plates acts as the galvanic isolation barrier. Similar to the transformer case, capacitive coupling uses a changing electric field to transmit information across the isolation barrier.

In our testing, we have demonstrated that transformer‐based isolation has inherent advantages over capacitor‐based isolation with respect to CMTI. As the following table demonstrates, transformer isolation is less sensitive to CMTI.

Test Transient Polarity Output State Transformer Pass Level Capacitive Pass Level Transformer Fail Level Capacitive Fail Level
CMH Positive High 100 kV/μs 9 kV/μs > 100 kV/μs 10 kV/μs
CML Positive Low 100 kV/μs 100 kV/μs > 100 kV/μs > 100 kV/μs
CMH Negative High 100 kV/μs 18 kV/μs > 100 kV/μs 20 kV/μs
CML Negative Low 100 kV/μs 100 kV/μs > 100 kV/μs > 100 kV/μs
(All testing performed @ VBATT = VDD2 = 4.50V, +25C)

The CMH test parameter is the maximum common‐mode voltage slew rate that can be sustained while still maintaining VOUT > 0.8*VDD2. CML is the maximum common‐mode voltage slew rate that can be sustained while still maintaining VOUT < 0.8V.

Figure 2 shows a positive going common‐mode transient of 10 kV/μs and its adverse effect on the capacitive‐based digital isolator when the output state is High (CMH). Whereas, Figure 3 shows the ADuM1402 is immune to positive common‐mode transients as high as 100 kV/μs.

Positive Transients

Figure 2 : Capacitive‐based isolator CMH ~10 kV/μs.

Figure 3 : ADuM1402, CMH ~100 kV/μs, VOA, VOB.

As is the case for positive going transients, Figure 4 indicates that a capacitive‐based digital isolator is also susceptible to negative going common‐mode transients when the output state is High (CMH). However, Figure 5 shows the ADuM1402 is immune to negative common‐mode transients as high as 100 kV/μs. iCoupler data sheets often specify a guaranteed CMTI level much lower than 100 kV/μs, typically guaranteed to be at least 25 kV/μs; however, this is to ensure that rating over all process and operating conditions.

Negative Transients

Figure 4 : Capacitive‐based isolator CMH ~20 kV/μs.

Figure 5 : ADuM1402, CMH ~100 kV/μs, VOA, VOB.

Conclusion

Based on the measurements above, it can be seen that capacitor‐based digital isolators may be more susceptible to common‐mode transients when their output state is High (CMH). However, in the case when the output state is Low (CML), capacitive‐based digital isolators can provide CMTI comparable to that of inductive‐based digital isolators. The advantage of inductive coupling is that it provides high common‐mode impedance to the noise and low differential impedance to the signal. However, unlike the transformer‐based isolator, in the capacitor‐based isolator there is no differential signal and the noise and the signal share the same transmission path. Therefore, this requires that the signal frequencies be well above the expected frequency of the noise so that the barrier capacitance presents low impedance to the signal and high impedance to the noise.

Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project

Related to this Article

Industry Solutions
Product Categories

Latest Media 21

Subtitle
Learn More
Add to myAnalog

Add article to the Resources section of myAnalog, to an existing project or to a new project.

Create New Project