ADI DRIVES CES
ADI DRIVES CES
ADI is Transforming the Daily Commute
Connected, sustainable, immersive. Our daily commutes are quickly evolving from simple transportation. Now they are sanctuaries in which to relax and opportunities to improve the efficiency and safety of our drives.
Dynamic lighting that combines style and safety.
The dazzling effects of dynamic lighting are complex and require an increasing number of LEDs to be individually controlled. ADI’s matrix managers and LED drivers deliver compact and efficient designs to power the next generation of automotive exterior lighting solutions. Now connected with ADI’s leading 10BASE-T1S E2B Ethernet technology supporting the transition to Zonal based architectures.
Automotive LED Driver Technology
ADI’s LED driver technology focuses on incorporating the state of the art in switching technology, LED dimming, safety, and features to reduce cost and ease design constraints.
Automotive Ethernet Connectivity with 10BASE-T1S E2B
See how ADI’s E2B 10BASE-T1S technology enables Ethernet connectivity all the way to the edge node as part of an automotive zonal architecture.
An intelligent view of automotive safety.
ADI technology enables highly efficient, compact, ultrathin, power management solutions to improve the connectivity of classic automotive cameras. This smart technology is a huge step forward in active safety and driver experience.
Making every person a happy passenger.
ADI powered breakthroughs in GMSL technology enables vehicle manufacturers to deploy Level 3 autonomous driving. By connecting high-resolution camera, radar, and lidar sensors, we set a new standard in safety for the future of transportation.
Drive away distractions.
Drive toward safety.
A robust Driver Monitoring System (DMS) requires proper illumination. This solution combines the strength of Seeing Machines' algorithm with the power of ADI's infrared driver to provide an overall safer driving experience.
Driving the displays of the future.
ADI-powered GMSL enables pillar to pillar displays over a single wire, empowering systems to fulfill all the resolution and safety requirements needed to drive displays that will lead us into the future.
Bridging the gap between high contrast and low power in automotive display.
ADI’s local-dimming LED driver and high-bandwidth serial link technology are contributing to making automotive travel safer, more power efficient, and immersive.
Teaching our vehicles to truly listen.
ADI LISTN™ embedded voice signal processing can focus on a particular passengers’ voice, in the presence of music, conversation, or road noise, to successfully and safely carry out every verbal command.
Voice and Acoustic Signal Processing
With a matured IP equipped on millions of cars on the road, this dependable software solution is easy to integrate and tune, and thus gets you to market faster.
A2B® Audio Bus: An Easier, Simpler Solution for Audio Designs
A better design experience. A more dynamic automotive experience. ADI's A2B®
Scalable, robust, and mature EV solution for a sustainable future.
ADI's battery management systems (BMS) with both wired and robust wireless (wBMS) connectivity options, along with the support of a growing network of ecosystem partners, ensure that EV manufacturers can respond to the industry’s demands, reduce risk, and shorten the time to bring products to market.
Powering the "me" drive, with E-Drive.
The emergence of the new SiC power switch changes the way energy conversion systems are designed. More efficient, smaller, and designed to the highest level of safety, ADI technology integrated into SiC-based systems delivers on the promise of changing the way we drive, forever.
Charging experiences that never leave you stranded.
Range anxiety is one of the biggest challenges facing EV adoption, so the rollout of a safe, easy, and reliably accessible charging experience is crucial. ADI technology fits both AC & DC systems at your home, on the commute, or at the workplace.