In-System Programming Using I2C Bootloader Commands
Abstract
This application note describes I2C bootloader commands supported by optical microcontrollers. The bootloader commands are executed from functions in the utility ROM (UROM). The application note specifies the I2C master and I2C slave command response protocol, which interacts with the I2C slave to execute the bootloader commands. It also describes various methods of in-system programming (ISP) using the I2C slave bootloader commands.
Introduction
The DS4830 has a program segment known as utility ROM (UROM), which provides various system utility functions. This allows in-system programming (ISP) using the I2C slave interface. The DS4830 reset vector is located in the utility ROM at address 8000h. Following each power-on reset (POR), the DS4830 automatically starts execution from the utility ROM, which allows the ROM code to perform any necessary system support functions.
The utility ROM provides the following utility functions.
- Reset vector
- Bootstrap function for system initialization
- In-circuit debug
- ISP using JTAG or I2C slave interface
In-System Programming Using the I2C Bootloader
The DS4830 has a special bit, I2C_SPE, which does not change on I2C soft reset or external reset. This bit is used to identify the I2C bootloader function. The I2C_SPE bit is not writable in the application program; this bit can be written through UROM code only. The DS4830 has the dedicated slave address 34h, which is always visible on the active I2C slave interface and cannot be disabled without disabling the I2C slave interface. Slave address 34h is used to communicate directly with the UROM code. When the slave address 34h receives the Enter I2C Bootloader command, it sets the I2C_SPE bit. On reset, the UROM code checks the I2C_SPE bit. If I2C_SPE is clear, code execution jumps to the flash location 0000h in the application program. Otherwise, execution remains in UROM to execute utility functions. For more information, see the In-System Programming section in the user guide 5484, “DS4830 Optical Microcontroller User’s Guide.”
| Family | Command | Command Description | Password Protected |
| 0 | 00h | No Operation | N |
| 01h | Exit Loader. With this command, the bootloader exits, clears the JTAG_SPE and I2C_SPE bits, and performs an internal reset. | N | |
| 02h | Master Erase. This command erases (sets to FFFFh) the words in the program flash memory, writes (sets to 0000h) all words in the data SRAM, and clears the password lock bit. | N | |
| 03h | Password Match. This command matches the 32-byte password value to that in program memory to clear the password lock bit. | N | |
| 04h | Get Status. This command monitors the bootloader Status Flags and Status Code. | N | |
| 05h | Get Supported commands | N | |
| 06h | Get Code Size | N | |
| 07h | Get Data Size | N | |
| 08h | Get Loader Version | N | |
| 09h | Get Utility ROM Version | N | |
| 0Dh | ID Banner command | N | |
| 1 | 10h | Load Code. This command programs data into the program flash memory. | Y |
| 11h | Load Data. This command programs data into the SRAM. | Y | |
| 2 | 20h | Dump Code. This command reads data from the program flash memory. | Y |
| 21h | Dump Data. This command reads data from the SRAM. | Y | |
| 3 | 30h | CRC Code. This command calculates the CRC of the program flash memory. | Y |
| 31h | CRC Data. This command calculates the CRC of the SRAM. | Y | |
| 4 | 40h | Verify Code. This command verifies that the data written in the program flash memory matches the input data with this command. | Y |
| 41h | Verify Data. This command verifies that the data written in the SRAM matches the input data with this command. | Y | |
| 5 | 50h | Load and Verify Code. This command programs data into the program flash memory and verifies the data immediately after each word. | Y |
| 51h | Load and Verify Data. This command programs data into the SRAM and verifies the data immediately after each word. | Y | |
| E | E0h | Code (Flash) Page Erase | Y |
The utility ROM provides the following functions for ISP using the I2C slave interface.
- Enter I2C bootloader
- Poll 3Eh
- Master Erase command
- Flash programming commands
- Load and Verify Code command (50h)
- Load Code command (10h) and Verify Code command (40h) (alternate method)
- Load Code command (10h) and Dump Code command (20h) (alternate method)
- Get Status command
- Exit Bootloader command
See Figure 1 for ISP.

Figure 1. Flowchart of flash ISP.
See Figure 2 for the colors used to differentiate the I2C master sequence/response, the bootloader command, and the bootloader (I2C slave) response.

Figure 2. I2C master-slave communication color indicators for the bootloader commands.
- Enter I2C Bootloader
- Set the I2C_SPE bit by sending command F0h as shown below.
- Reset the device by either using the I2C reset command BBh (with slave address 34h) or by toggling the %-overbar_pre%RST%-overbar_post% pin.
- Poll 3Eh
- Master Erase
- Send the I2C sequence for Master Erase. Note: This clears the password lock bit on successful Master Erase execution, which unlocks flash for flash programming commands (e.g., Load and Verify Code, Load, Verify, Dump).
- Wait 24ms (the typical time for Master Erase).
- Poll for 3Eh.
- Read the Get Status command and check the status byte for Master Erase Failed (i.e., status value 08).
- Flash Programming
- Load Code (10h)
- Load and Verify Code (50h)
- Load and Verify Code command (50h)
- Load Code command (10h) and Verify Code command (40h)
- Load Code command (10h) and Dump Code command (20h)
- Load and Verify Code (50h)
- Load Code (10h)
- Verify Code (40h)
- Dump Code (20h)
The DS4830 has the dedicated slave address 34h, which is always visible on the DS4830 active I2C slave interface. This slave address is used to enter bootloader mode from the application. To enter bootloader mode, the I2C communication sequence should be as follows.
| I2C Start | Slave Addr 34h + W | ACK | Cmd F0h |
ACK | I2C Stop |
| I2C Start | Slave Addr 34h + W | ACK | Cmd BBh |
ACK | I2C Stop |
The UROM acknowledges the execution of commands by sending 3Eh after the execution of every command. This polling for 3Eh at the end of every command execution is required for the correct functioning of the UROM functions.
Polling 3Eh for I2C bootloader ReadThe I2C Read command operation can be terminated by reading an additional byte. The additional byte should be 3Eh. For example, the Get Status command provides two bytes of status. To terminate this command, the I2C master should read three bytes and send NACK to the last byte. See Figure 3 for the I2C bootloader Read operation.

Figure 3. I2C bootloader Read operation.
The completion of the execution of the UROM I2C Write command operation can be identified by polling 3Eh after the I2C Write operation. See Figure 4 for 3Eh polling after the Write command operation. The Exit Bootloader command is an exception that does not require 3Eh.

Figure 4. I2C bootloader Write operation.
Either of the following two sequences can be used to poll for 3Eh after a Write command operation.
Method 1In this method, the I2C master starts reading data from slave address 36h. It compares received data with 3Eh. If the data does not match, then it sends ACK. If the data matches, it sends NACK and completes the communication by issuing Stop.
| I2C Start | Slave Addr 36 + R | ACK | Read 3Eh? ‘No’ |
ACK | Read 3Eh? ‘Yes’ |
NACK | I2C Stop |
In this method, the I2C sequence involves reading only one data byte for every sequence. The I2C master compares the received data with 3Eh. If the data matches, it stops polling for the 3Eh.
| I2C Start | Slave Addr 36 + R | ACK | Read Data | NACK | I2C Stop |
The Master Erase command erases all flash pages simultaneously. The steps to execute this command are shown below.
| I2C Start | Slave Addr 36h + W | ACK | Cmd 02h |
ACK | I2C Stop |
The UROM provides two commands to program data into the flash memory.
The Load Code command writes input data to the flash memory. The Load and Verify Code command writes input data to the flash memory and verifies the data by reading back from the flash memory after writing. This command takes a longer time to execute. However, the user can save significant time by using the Load and Verify Code command in place of using the Load Code and Verify Code commands separately.
To program and verify the flash memory, the user can use one of the following methods.
The UROM functions are executed with the following commands. These commands are used for flash programming in the three methods above.
Each command is explained below.
Load and Verify Code
This command writes data into the flash memory and verifies it by reading data from the flash memory.
The steps to implement this command are listed below.
- Send the following I2C sequence for flash programming with the Load and Verify Code command.
- Poll for 3Eh.
- Read the Get Status command and check the status byte for Verify Failed (i.e., status value 05).
| I2C Start | Slave Addr 36h + W | ACK | Cmd 50h |
ACK | Length N |
ACK | AddL | ACK | AddH | ACK |
| Byte 1 | ACK | Byte 2 | ACK | ….. | ….. | Byte n | ACK | I2C Stop |
Load Code
The Load Code command (10h) writes n number of bytes to the flash memory, starting from the input address. This command requires a number of bytes to write (in one bytes) and the starting address. The starting address is given in two bytes: AddH and AddL. The bootloader function calculates the address as (AddH * 256 + AddL). The one byte data length limits the total number of bytes transferred in a single sequence to 255 bytes for this command. To verify the written data, the user can use the Verify Code command or the Dump Code command. The steps to implement the Load Code command are listed below.
- Use the Master Erase command or the Flash Page Erase command. Note: The Flash Page Erase command requires password unlock. See the Miscellaneous I2C Commands section for details.
- Send the following I2C sequence for flash programming with the Load Code command.
- Poll for 3Eh.
- Read the Get Status command for any error.
| I2C Start | Slave Addr 36h + W | ACK | Cmd 10h |
ACK | Length N |
ACK | AddL | ACK | AddH | ACK |
| Byte 1 | ACK | Byte 2 | ACK | ….. | ….. | Byte n | ACK | I2C Stop |
Verify Code
The Verify Code command compares the data written to the flash with the given data. If the data does not match, it sets the Verify Failed bit in the status code byte [bit 5]. The steps to implement the Verify Code command are listed below.
- Unlock the password. (This is not required if the Master Erase command executed successfully.)
- Send the following I2C sequence for flash programming with the Verify Code command.
- Poll for 3Eh.
- Read the Get Status command and check the status byte for Verify Failed (i.e., status value 05).
| I2C Start | Slave Addr 36h + W | ACK | Cmd 40h |
ACK | Length N |
ACK | AddL | ACK | AddH | ACK |
| Byte 1 | ACK | Byte 2 | ACK | ….. | ….. | Byte n | ACK | I2C Stop |
Dump Code
The Dump Code command reads the data from the flash memory and compares it to the data written. This command requires the starting address (sent in two bytes) and a number of bytes to read (in two bytes). The command sends out the flash data from the given address. The steps to implement the Dump Code command are listed below.
- Unlock the password. (This is not required if the Master Erase command executed successfully and the Load Code operation executed.)
- Send the following I2C sequence for the Dump Code with the starting address AddL:AddH and the number of bytes LengthL:LengthH (n = LengthH * 256 + LengthL).
- Send restart and read n bytes of data with ACK.
- Read 3Eh with NACK and issue Stop.
| I2C Start | Slave Addr 36h + W | ACK | Cmd 20h |
ACK |
| 02 | ACK | AddL | ACK | AddH | ACK | LengthL | ACK | LengthH | ACK |
| I2C Restart | Slave Addr 36h + R | ACK | Read Byte1 | ACK | … | … | Read Byte n |
ACK | 3Eh (n+1) |
NACK | I2C Stop |
Get Status
The UROM provides the Get Status command, which returns flags and status code from the executed command. The I2C sequence for the Get Status command is shown below.
| I2C Start | Slave Addr 36h + W | ACK | Cmd 04h |
ACK |
| I2C Restart | Slave Addr 36h + R | ACK | Read Flags | ACK | Read Status Code |
ACK | Read 3Eh |
NACK | I2C Stop |
Exit Bootloader
This command clears the I2C_SPE bit, which is set by the Enter I2C Bootloader command, and generates an internal reset. Note: After receiving the Exit Bootloader command (01h), the I2C bootloader waits for approximately 32µs and then generates an internal reset.
| I2C Start | Slave Addr 36 h + W | ACK | Cmd 01h |
ACK | I2C Stop |
Miscellaneous I2C Commands
Password Unlock
The DS4830 has a 32-byte password in program memory at byte address 0020h through 003Fh. To access the password-protected commands, the user has to provide the same password using the Password Unlock command as shown below. Except for family 0 commands, all bootloader commands are password protected.
The sequence to unlock the password is as follows.
- Send the following I2C sequence for Password Unlock.
- Poll for 3Eh.
- Read the Get Status command and check bit 3 No Password Match of the status code byte.
| I2C Start | Slave Addr 36h + W | ACK | Cmd 03h |
ACK | PW0 | ACK | PW1 | ACK | ….. | ACK | PW31 | ACK | I2C Stop |
Calculate CRC-16 of memory (code or data)
The UROM provides a function to calculate the CRC-16 of either program memory (code) or data memory (SRAM). The steps to calculate CRC-16 are as follows.
- Send the following I2C sequence to calculate the CRC-16. The CRC-16 values are two bytes prior to 3E.
- Wait for a delay of approximately (LengthL + LengthH *256) * 45µs.
- Send the following I2C sequence to read three bytes (two bytes CRC and the last byte 3E).
Note: The UROM takes approximately 45µs/byte to calculate the CRC-16.
| I2C Start | Slave Addr 36h + W | ACK | Cmd 30h |
ACK | 02h | ACK | AddL | ACK | AddH | ACK |
| LengthL | ACK | LengthH | ACK | I2C Stop |
| I2C Restart | Slave Addr + R | ACK | Data Out CRCL |
ACK | Data Out CRCH |
ACK | 3E | NACK | I2C Stop |
Two-byte Read commands
The Read commands with two bytes of data (Table 2) use the following format to read bytes and complete the execution.
| Command Name | Command | LSB | MSB |
| Get Status | 04h | Flags | Status |
| Get Code Size (flash) | 06h | Size–lower byte | Size–higher byte |
| Get Data Size (SRAM) | 07h | Size–lower byte | Size–higher byte |
| Get Loader Version | 08h | Lower version number | Higher version number |
| Get Utility ROM Version | 09h | Lower version number | Higher version number |
| I2C Start | Slave Addr 36h + W | ACK | Command | ACK |
| I2C Restart | Slave Addr 36h + R | ACK | Read LSB | ACK | Read MSB |
ACK | Read 3Eh |
NACK | I2C Stop |
Get device specific banner (0Dh command)
The ID Banner command can be used to differentiate various MAXQ MCUs. The I2C sequence for the ID Banner command is shown below.
| I2C Start | Slave Addr 36h + W | ACK | Cmd 0Dh |
ACK |
| I2C Restart | Slave Addr 36h + R | ACK | Read Byte1 |
ACK | … | … | Read Byte n |
ACK | 3E (n+1) Byte |
NACK | I2C Stop |
The n value for the DS4830 is 31 and the ID Banner is “DS4830 Loader 1.01 03-09-2010 \0” in ASCII.
Code (Flash) Page Erase command
The DS4830 flash memory is divided into pages. Each page size is 512 bytes (256 words). In total, there are 128 pages in the flash memory. Each page can be erased individually using the I2C bootloader command. The steps to implement the Code (Flash) Page Erase command are shown below.
- Unlock the password (if locked).
- Send the following I2C sequence for the Flash Page Erase command.
- Wait 24ms (the typical time for Code (Flash) Page Erase).
- Poll for 3Eh.
| I2C Start | Slave Addr 36h + W | ACK | Cmd E0h |
ACK | 00h | ACK | Page Num |
ACK | 00h | ACK | I2C Stop |
Additional Resources
Pseudocode for the I2C master (ZIP, 8kB)
Notes
- The I2C communication clock frequency should not be more than 100kHz for reliable operation.
- Bootloader commands greater than 0Fh are password protected.